Structure containing state of the image file processed.
Public Attributes#
uint8_t
Image contents.
uint8_t
Parser instructions.
bool
Flag to indicate parsing has completed.
bool
Flag to indicate the image file has been validated.
uint32_t
Version number of main bootloader extracted from image file.
Information about the application.
uint32_t
Size of the bootloader upgrade contained in the image file.
Public Attribute Documentation#
imageVerified#
bool ImageProperties_t::imageVerified
Flag to indicate the image file has been validated.
bootloaderVersion#
uint32_t ImageProperties_t::bootloaderVersion
Version number of main bootloader extracted from image file.
bootloaderUpgradeSize#
uint32_t ImageProperties_t::bootloaderUpgradeSize
Size of the bootloader upgrade contained in the image file.