ACMP_VBConfig_TypeDef Struct ReferenceEMLIB > ACMP

VB Configuration structure. This structure is used to configure the VB voltage input source and its dividers.

Definition at line 801 of file em_acmp.h.

#include <em_acmp.h>

Data Fields

uint32_t div0
 
uint32_t div1
 
ACMP_VBInput_TypeDef input
 

Field Documentation

uint32_t ACMP_VBConfig_TypeDef::div0

A divider for VB voltage input source when ACMP output is 0. This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.

VB divided = VB input * (div0 + 1) / 64

Definition at line 811 of file em_acmp.h.

Referenced by ACMP_VBSetup().

uint32_t ACMP_VBConfig_TypeDef::div1

A divider for VB voltage input source when ACMP output is 1. This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.

VB divided = VB input * (div1 + 1) / 64

Definition at line 820 of file em_acmp.h.

Referenced by ACMP_VBSetup().

ACMP_VBInput_TypeDef ACMP_VBConfig_TypeDef::input

VB Voltage input source

Definition at line 802 of file em_acmp.h.

Referenced by ACMP_VBSetup().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/em_acmp.h