PCNT_Init_TypeDef Struct ReferenceEMLIB > PCNT
Initialization structure.
Definition at line 169
of file em_pcnt.h
.
#include <
em_pcnt.h
>
Data Fields | |
PCNT_CntEvent_TypeDef | auxCntEvent |
PCNT_CntEvent_TypeDef | cntEvent |
bool | countDown |
uint32_t | counter |
bool | filter |
bool | hyst |
PCNT_Mode_TypeDef | mode |
bool | negEdge |
PCNT_PRSSel_TypeDef | s0PRS |
bool | s1CntDir |
PCNT_PRSSel_TypeDef | s1PRS |
uint32_t | top |
Field Documentation
PCNT_CntEvent_TypeDef PCNT_Init_TypeDef::auxCntEvent |
Selects whether the auxiliary counter responds to up-count events, down-count events, both, or none.
Definition at line 215
of file em_pcnt.h
.
Referenced by PCNT_Init().
PCNT_CntEvent_TypeDef PCNT_Init_TypeDef::cntEvent |
Selects whether the regular counter responds to up-count events, down-count events, both, or none.
Definition at line 211
of file em_pcnt.h
.
Referenced by PCNT_Init().
bool PCNT_Init_TypeDef::countDown |
Counting direction, only applicable for pcntModeOvsSingle and pcntModeExtSingle modes.
Definition at line 193
of file em_pcnt.h
.
Referenced by PCNT_Init().
uint32_t PCNT_Init_TypeDef::counter |
Initial counter value (refer to reference manual for max value allowed). Only used for pcntModeOvsSingle (and possibly pcntModeDisable) modes. If using pcntModeExtSingle or pcntModeExtQuad modes, counter value is reset to HW reset value.
Definition at line 177
of file em_pcnt.h
.
Referenced by PCNT_Init().
bool PCNT_Init_TypeDef::filter |
Enable filter, only available in #pcntModeOvs* modes.
Definition at line 196
of file em_pcnt.h
.
Referenced by PCNT_Init().
bool PCNT_Init_TypeDef::hyst |
Set to true to enable hysteresis. When enabled, PCNT will always overflow and underflow to TOP/2.
Definition at line 201
of file em_pcnt.h
.
Referenced by PCNT_Init().
PCNT_Mode_TypeDef PCNT_Init_TypeDef::mode |
bool PCNT_Init_TypeDef::negEdge |
Polarity of incoming edge.
- pcntModeExtSingle mode - if false, positive edges are counted, otherwise negative edges.
- pcntModeExtQuad mode - if true, counting direction is inverted.
Definition at line 189
of file em_pcnt.h
.
Referenced by PCNT_Init().
PCNT_PRSSel_TypeDef PCNT_Init_TypeDef::s0PRS |
Select PRS channel as input to S0IN in PCNTx_INPUT register.
Definition at line 218
of file em_pcnt.h
.
Referenced by PCNT_Init().
bool PCNT_Init_TypeDef::s1CntDir |
Set to true to enable S1 to determine the direction of counting in OVSSINGLE or EXTCLKSINGLE modes.
When S1 is high, the count direction is given by CNTDIR, and when S1 is low, the count direction is the opposite.
Definition at line 207
of file em_pcnt.h
.
Referenced by PCNT_Init().
PCNT_PRSSel_TypeDef PCNT_Init_TypeDef::s1PRS |
Select PRS channel as input to S1IN in PCNTx_INPUT register.
Definition at line 221
of file em_pcnt.h
.
Referenced by PCNT_Init().
uint32_t PCNT_Init_TypeDef::top |
Initial top value (refer to reference manual for max value allowed). Only used for pcntModeOvsSingle (and possibly pcntModeDisable) modes. If using pcntModeExtSingle or pcntModeExtQuad modes, top value is reset to HW reset value.
Definition at line 183
of file em_pcnt.h
.
Referenced by PCNT_Init().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_pcnt.h