NorFlashKit Drivers
         Data Structures | 
       |
| struct | NORFLASH_Info_TypeDef | 
| 
         NORFLASH device information struct.
          | 
       |
         Enumerations | 
       |
| enum | 
         
          NORFLASH_Status_TypeDef
         
         {
          NORFLASH_STATUS_OK = 0, NORFLASH_NONUNIFORM_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6, NORFLASH_STATUS_OK = 0, NORFLASH_UNSUPPORTED_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6 }  | 
       
| 
         NORFLASH status enumerator.
          | 
       |
| enum | 
         
          NORFLASH_Status_TypeDef
         
         {
          NORFLASH_STATUS_OK = 0, NORFLASH_NONUNIFORM_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6, NORFLASH_STATUS_OK = 0, NORFLASH_UNSUPPORTED_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6 }  | 
       
| 
         NORFLASH status enumerator.
          | 
       |
         Functions | 
       |
| bool | NORFLASH_AddressValid (uint32_t addr) | 
| 
         Check if an address is valid for the flash device.
          | 
       |
| NORFLASH_Info_TypeDef * | NORFLASH_DeviceInfo (void) | 
| 
         Return a pointer to a
         
          NORFLASH_Info_TypeDef
         
         , which contain vital flash device information.
          | 
       |
| int | NORFLASH_EraseDevice (void) | 
| 
         Erase entire flash device.
          | 
       |
| int | NORFLASH_EraseSector (uint32_t addr) | 
| 
         Erase a sector in the flash device.
          | 
       |
| uint32_t | NORFLASH_getDeviceID (void) | 
| 
         Get flash device ID.
          | 
       |
| uint32_t | NORFLASH_getDeviceSize (void) | 
| 
         Get flash device size.
          | 
       |
| uint32_t | NORFLASH_getSectorRegionCount (void) | 
| 
         Get flash sector region count.
          | 
       |
| uint32_t | NORFLASH_getVendorID (void) | 
| 
         Get manufacturer ID.
          | 
       |
| int | NORFLASH_Init (void) | 
| 
         Initialize the NORFLASH module.
          | 
       |
| int | NORFLASH_Program (uint32_t addr, uint8_t *data, uint32_t count) | 
| 
         Program the flash device.
          | 
       |
| int | NORFLASH_ProgramByte (uint32_t addr, uint8_t data) | 
| 
         Program a single byte in the flash device.
          | 
       |
| int | NORFLASH_ProgramWord16 (uint32_t addr, uint16_t data) | 
| 
         Program a word (16bit) in the flash device.
          | 
       |
| int | NORFLASH_ProgramWord32 (uint32_t addr, uint32_t data) | 
| 
         Program a word (32bit) in the flash device.
          | 
       |
Enumeration Type Documentation
NORFLASH status enumerator.
        Definition at line
        
         38
        
        of file
        
         norflash.h
        
        .
       
NORFLASH status enumerator.
        Definition at line
        
         38
        
        of file
        
         norflash_s29gl.h
        
        .
       
Function Documentation
| bool NORFLASH_AddressValid | ( | uint32_t | 
           
            addr
           
           | 
          ) | 
Check if an address is valid for the flash device.
- Parameters
 - 
         
[in] addrThe address value to check.  
- Returns
 - True if address value is valid, false otherwise.
 
        Definition at line
        
         48
        
        of file
        
         norflash.c
        
        .
       
References NORFLASH_Info_TypeDef::baseAddress , NORFLASH_Info_TypeDef::deviceSize , and NORFLASH_STATUS_OK .
Referenced by NORFLASH_EraseSector() , NORFLASH_Program() , and NORFLASH_ProgramWord16() .
| NORFLASH_Info_TypeDef * NORFLASH_DeviceInfo | ( | void | 
           
           
           | 
          ) | 
Return a pointer to a NORFLASH_Info_TypeDef , which contain vital flash device information.
- Returns
 - NULL if unable to initialize the flash if no prior call to NORFLASH_Init() has been made. Pointer to a NORFLASH_Info_TypeDef on success.
 
        Definition at line
        
         74
        
        of file
        
         norflash.c
        
        .
       
References NORFLASH_STATUS_OK .
| int NORFLASH_EraseDevice | ( | void | 
           
           
           | 
          ) | 
Erase entire flash device.
- Returns
 - NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
 
        Definition at line
        
         93
        
        of file
        
         norflash.c
        
        .
       
References NORFLASH_Info_TypeDef::baseAddress , and NORFLASH_STATUS_OK .
| int NORFLASH_EraseSector | ( | uint32_t | 
           
            addr
           
           | 
          ) | 
Erase a sector in the flash device.
- Parameters
 - 
         
[in] addrAddress of the sector to erase.  
- Returns
 - NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
 
        Definition at line
        
         126
        
        of file
        
         norflash.c
        
        .
       
References NORFLASH_AddressValid() , NORFLASH_INVALID_ADDRESS , NORFLASH_STATUS_OK , and NORFLASH_Info_TypeDef::sectorSize .
| uint32_t NORFLASH_getDeviceID | ( | void | 
           
           
           | 
          ) | 
Get flash device ID.
- Returns
 - Flash device ID
 
        Definition at line
        
         409
        
        of file
        
         norflash_s29gl.c
        
        .
       
| uint32_t NORFLASH_getDeviceSize | ( | void | 
           
           
           | 
          ) | 
Get flash device size.
- Returns
 - Flash device size
 
        Definition at line
        
         427
        
        of file
        
         norflash_s29gl.c
        
        .
       
| uint32_t NORFLASH_getSectorRegionCount | ( | void | 
           
           
           | 
          ) | 
Get flash sector region count.
- Returns
 - Flash sector region
 
        Definition at line
        
         439
        
        of file
        
         norflash_s29gl.c
        
        .
       
| uint32_t NORFLASH_getVendorID | ( | void | 
           
           
           | 
          ) | 
Get manufacturer ID.
- Returns
 - Manufacturer ID
 
        Definition at line
        
         397
        
        of file
        
         norflash_s29gl.c
        
        .
       
| int NORFLASH_Init | ( | void | 
           
           
           | 
          ) | 
Initialize the NORFLASH module.
- Note
 - This function should be called before any other NORFLASH_xxx() functions are used.
 
- Returns
 - NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
 
        Definition at line
        
         169
        
        of file
        
         norflash.c
        
        .
       
| int NORFLASH_Program | ( | uint32_t | 
           
            addr,
           
           | 
         
| uint8_t * | 
           
            data,
           
           | 
         ||
| uint32_t | 
           
            count
           
           | 
         ||
| ) | 
Program the flash device.
- Note
 - It is assumed that the area to be programmed is erased.
 
- Parameters
 - 
         
[in] addrThe first address in the flash to be programmed. [in] dataPointer to the data to be programmed. [in] countNumber of bytes to be programmed.  
- Returns
 - NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
 
        Definition at line
        
         194
        
        of file
        
         norflash.c
        
        .
       
References NORFLASH_AddressValid() , NORFLASH_INVALID_ADDRESS , NORFLASH_ProgramByte() , NORFLASH_ProgramWord16() , NORFLASH_STATUS_OK , NORFLASH_Info_TypeDef::sectorSize , and SL_MIN .
| int NORFLASH_ProgramByte | ( | uint32_t | 
           
            addr,
           
           | 
         
| uint8_t | 
           
            data
           
           | 
         ||
| ) | 
Program a single byte in the flash device.
- Note
 - It is assumed that the area to be programmed is erased.
 
- Parameters
 - 
         
[in] addrThe address to be programmed. [in] dataThe byte value to be programmed.  
- Returns
 - NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
 
        Definition at line
        
         282
        
        of file
        
         norflash.c
        
        .
       
References NORFLASH_ProgramWord16() .
Referenced by NORFLASH_Program() .
| int NORFLASH_ProgramWord16 | ( | uint32_t | 
           
            addr,
           
           | 
         
| uint16_t | 
           
            data
           
           | 
         ||
| ) | 
Program a word (16bit) in the flash device.
- Note
 - It is assumed that the area to be programmed is erased.
 
- Parameters
 - 
         
[in] addrThe address to be programmed. [in] dataThe word value to be programmed.  
- Returns
 - NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
 
        Definition at line
        
         313
        
        of file
        
         norflash.c
        
        .
       
References NORFLASH_AddressValid() , NORFLASH_INVALID_ADDRESS , NORFLASH_MISALIGNED_ADDRESS , and NORFLASH_STATUS_OK .
Referenced by NORFLASH_Program() , NORFLASH_ProgramByte() , and NORFLASH_ProgramWord32() .
| int NORFLASH_ProgramWord32 | ( | uint32_t | 
           
            addr,
           
           | 
         
| uint32_t | 
           
            data
           
           | 
         ||
| ) | 
Program a word (32bit) in the flash device.
- Note
 - It is assumed that the area to be programmed is erased.
 
- Parameters
 - 
         
[in] addrThe address to be programmed. [in] dataThe word value to be programmed.  
- Returns
 - NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
 
        Definition at line
        
         360
        
        of file
        
         norflash.c
        
        .
       
References NORFLASH_MISALIGNED_ADDRESS , NORFLASH_ProgramWord16() , and NORFLASH_STATUS_OK .