RTCC_Init_TypeDef Struct ReferenceEMLIB > RTCC
RTCC initialization structure.
       Definition at line
       
        215
       
       of file
       
        em_rtcc.h
       
       .
      
      
       #include <
       
     
        em_rtcc.h
       
       >
      
         Data Fields | 
       |
| RTCC_CntMode_TypeDef | cntMode | 
| bool | cntWrapOnCCV1 | 
| bool | debugRun | 
| bool | disLeapYearCorr | 
| bool | enable | 
| bool | enaOSCFailDetect | 
| bool | precntWrapOnCCV0 | 
| RTCC_CntPresc_TypeDef | presc | 
| RTCC_PrescMode_TypeDef | prescMode | 
Field Documentation
| RTCC_CntMode_TypeDef RTCC_Init_TypeDef::cntMode | 
Select operational mode of the counter.
        Definition at line
        
         248
        
        of file
        
         em_rtcc.h
        
        .
       
Referenced by RTCC_Init() .
| bool RTCC_Init_TypeDef::cntWrapOnCCV1 | 
Enable/disable counter wrap on ch. 1 CCV value.
        Definition at line
        
         226
        
        of file
        
         em_rtcc.h
        
        .
       
Referenced by RTCC_Init() .
| bool RTCC_Init_TypeDef::debugRun | 
Enable/disable timer counting during debug halt.
        Definition at line
        
         220
        
        of file
        
         em_rtcc.h
        
        .
       
Referenced by RTCC_Init() .
| bool RTCC_Init_TypeDef::disLeapYearCorr | 
Disable leap year correction for calendar mode. When this parameter is set to false, February has 29 days if (year % 4 == 0). If set to true, February always has 28 days.
        Definition at line
        
         255
        
        of file
        
         em_rtcc.h
        
        .
       
Referenced by RTCC_Init() .
| bool RTCC_Init_TypeDef::enable | 
Enable/disable counting when initialization is completed.
        Definition at line
        
         217
        
        of file
        
         em_rtcc.h
        
        .
       
Referenced by RTCC_Init() .
| bool RTCC_Init_TypeDef::enaOSCFailDetect | 
Enable/disable the check that sets OSCFFAIL interrupt flag if no LFCLK-RTCC ticks are detected within one ULFRCO cycles.
        Definition at line
        
         243
        
        of file
        
         em_rtcc.h
        
        .
       
Referenced by RTCC_Init() .
| bool RTCC_Init_TypeDef::precntWrapOnCCV0 | 
Enable/disable pre-counter wrap on ch. 0 CCV value.
        Definition at line
        
         223
        
        of file
        
         em_rtcc.h
        
        .
       
Referenced by RTCC_Init() .
| RTCC_CntPresc_TypeDef RTCC_Init_TypeDef::presc | 
Counter prescaler.
        Definition at line
        
         229
        
        of file
        
         em_rtcc.h
        
        .
       
Referenced by RTCC_Init() , and RTCDRV_Init() .
| RTCC_PrescMode_TypeDef RTCC_Init_TypeDef::prescMode | 
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_rtcc.h