NorFlashKit Drivers
Data Structures |
|
| struct | NORFLASH_Info_TypeDef |
|
NORFLASH device information struct.
|
|
Enumerations |
|
| enum |
NORFLASH_Status_TypeDef
{
NORFLASH_STATUS_OK = 0, NORFLASH_NONUNIFORM_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6, NORFLASH_STATUS_OK = 0, NORFLASH_UNSUPPORTED_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6 } |
|
NORFLASH status enumerator.
|
|
| enum |
NORFLASH_Status_TypeDef
{
NORFLASH_STATUS_OK = 0, NORFLASH_NONUNIFORM_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6, NORFLASH_STATUS_OK = 0, NORFLASH_UNSUPPORTED_GEOMETRY = -1, NORFLASH_NOT_CFI_DEVICE = -2, NORFLASH_WRITE_FAILURE = -3, NORFLASH_WRITE_TIMEOUT = -4, NORFLASH_INVALID_ADDRESS = -5, NORFLASH_MISALIGNED_ADDRESS = -6 } |
|
NORFLASH status enumerator.
|
|
Functions |
|
| bool | NORFLASH_AddressValid (uint32_t addr) |
|
Check if an address is valid for the flash device.
|
|
| NORFLASH_Info_TypeDef * | NORFLASH_DeviceInfo (void) |
|
Return a pointer to a
NORFLASH_Info_TypeDef
, which contain vital flash device information.
|
|
| int | NORFLASH_EraseDevice (void) |
|
Erase entire flash device.
|
|
| int | NORFLASH_EraseSector (uint32_t addr) |
|
Erase a sector in the flash device.
|
|
| uint32_t | NORFLASH_getDeviceID (void) |
|
Get flash device ID.
|
|
| uint32_t | NORFLASH_getDeviceSize (void) |
|
Get flash device size.
|
|
| uint32_t | NORFLASH_getSectorRegionCount (void) |
|
Get flash sector region count.
|
|
| uint32_t | NORFLASH_getVendorID (void) |
|
Get manufacturer ID.
|
|
| int | NORFLASH_Init (void) |
|
Initialize the NORFLASH module.
|
|
| int | NORFLASH_Program (uint32_t addr, uint8_t *data, uint32_t count) |
|
Program the flash device.
|
|
| int | NORFLASH_ProgramByte (uint32_t addr, uint8_t data) |
|
Program a single byte in the flash device.
|
|
| int | NORFLASH_ProgramWord16 (uint32_t addr, uint16_t data) |
|
Program a word (16bit) in the flash device.
|
|
| int | NORFLASH_ProgramWord32 (uint32_t addr, uint32_t data) |
|
Program a word (32bit) in the flash device.
|
|
Enumeration Type Documentation
NORFLASH status enumerator.
Definition at line
38
of file
norflash.h
.
NORFLASH status enumerator.
Definition at line
38
of file
norflash_s29gl.h
.
Function Documentation
| bool NORFLASH_AddressValid | ( | uint32_t |
addr
|
) |
Check if an address is valid for the flash device.
- Parameters
-
[in] addrThe address value to check.
- Returns
- True if address value is valid, false otherwise.
Definition at line
48
of file
norflash.c
.
References NORFLASH_Info_TypeDef::baseAddress , NORFLASH_Info_TypeDef::deviceSize , and NORFLASH_STATUS_OK .
Referenced by NORFLASH_EraseSector() , NORFLASH_Program() , and NORFLASH_ProgramWord16() .
| NORFLASH_Info_TypeDef * NORFLASH_DeviceInfo | ( | void |
|
) |
Return a pointer to a NORFLASH_Info_TypeDef , which contain vital flash device information.
- Returns
- NULL if unable to initialize the flash if no prior call to NORFLASH_Init() has been made. Pointer to a NORFLASH_Info_TypeDef on success.
Definition at line
74
of file
norflash.c
.
References NORFLASH_STATUS_OK .
| int NORFLASH_EraseDevice | ( | void |
|
) |
Erase entire flash device.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line
93
of file
norflash.c
.
References NORFLASH_Info_TypeDef::baseAddress , and NORFLASH_STATUS_OK .
| int NORFLASH_EraseSector | ( | uint32_t |
addr
|
) |
Erase a sector in the flash device.
- Parameters
-
[in] addrAddress of the sector to erase.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line
126
of file
norflash.c
.
References NORFLASH_AddressValid() , NORFLASH_INVALID_ADDRESS , NORFLASH_STATUS_OK , and NORFLASH_Info_TypeDef::sectorSize .
| uint32_t NORFLASH_getDeviceID | ( | void |
|
) |
Get flash device ID.
- Returns
- Flash device ID
Definition at line
409
of file
norflash_s29gl.c
.
| uint32_t NORFLASH_getDeviceSize | ( | void |
|
) |
Get flash device size.
- Returns
- Flash device size
Definition at line
427
of file
norflash_s29gl.c
.
| uint32_t NORFLASH_getSectorRegionCount | ( | void |
|
) |
Get flash sector region count.
- Returns
- Flash sector region
Definition at line
439
of file
norflash_s29gl.c
.
| uint32_t NORFLASH_getVendorID | ( | void |
|
) |
Get manufacturer ID.
- Returns
- Manufacturer ID
Definition at line
397
of file
norflash_s29gl.c
.
| int NORFLASH_Init | ( | void |
|
) |
Initialize the NORFLASH module.
- Note
- This function should be called before any other NORFLASH_xxx() functions are used.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line
169
of file
norflash.c
.
| int NORFLASH_Program | ( | uint32_t |
addr,
|
| uint8_t * |
data,
|
||
| uint32_t |
count
|
||
| ) |
Program the flash device.
- Note
- It is assumed that the area to be programmed is erased.
- Parameters
-
[in] addrThe first address in the flash to be programmed. [in] dataPointer to the data to be programmed. [in] countNumber of bytes to be programmed.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line
194
of file
norflash.c
.
References NORFLASH_AddressValid() , NORFLASH_INVALID_ADDRESS , NORFLASH_ProgramByte() , NORFLASH_ProgramWord16() , NORFLASH_STATUS_OK , NORFLASH_Info_TypeDef::sectorSize , and SL_MIN .
| int NORFLASH_ProgramByte | ( | uint32_t |
addr,
|
| uint8_t |
data
|
||
| ) |
Program a single byte in the flash device.
- Note
- It is assumed that the area to be programmed is erased.
- Parameters
-
[in] addrThe address to be programmed. [in] dataThe byte value to be programmed.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line
282
of file
norflash.c
.
References NORFLASH_ProgramWord16() .
Referenced by NORFLASH_Program() .
| int NORFLASH_ProgramWord16 | ( | uint32_t |
addr,
|
| uint16_t |
data
|
||
| ) |
Program a word (16bit) in the flash device.
- Note
- It is assumed that the area to be programmed is erased.
- Parameters
-
[in] addrThe address to be programmed. [in] dataThe word value to be programmed.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line
313
of file
norflash.c
.
References NORFLASH_AddressValid() , NORFLASH_INVALID_ADDRESS , NORFLASH_MISALIGNED_ADDRESS , and NORFLASH_STATUS_OK .
Referenced by NORFLASH_Program() , NORFLASH_ProgramByte() , and NORFLASH_ProgramWord32() .
| int NORFLASH_ProgramWord32 | ( | uint32_t |
addr,
|
| uint32_t |
data
|
||
| ) |
Program a word (32bit) in the flash device.
- Note
- It is assumed that the area to be programmed is erased.
- Parameters
-
[in] addrThe address to be programmed. [in] dataThe word value to be programmed.
- Returns
- NORFLASH_STATUS_OK on success, an error code enumerated in NORFLASH_Status_TypeDef on failure.
Definition at line
360
of file
norflash.c
.
References NORFLASH_MISALIGNED_ADDRESS , NORFLASH_ProgramWord16() , and NORFLASH_STATUS_OK .