LESENSE_TimeCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
LESENSE timing control descriptor structure.
Definition at line
547
of file
em_lesense.h
.
#include <
em_lesense.h
>
Data Fields |
|
bool | delayAuxStartup |
uint8_t | startDelay |
Field Documentation
bool LESENSE_TimeCtrlDesc_TypeDef::delayAuxStartup |
Set to true do delay startup of AUXHFRCO until the system enters excite phase. This will reduce the time AUXHFRCO is enabled and reduce power usage.
Definition at line
556
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
uint8_t LESENSE_TimeCtrlDesc_TypeDef::startDelay |
Set number of LFACLK cycles to delay sensor interaction on each channel. Valid range: 0-3 (2 bit).
Definition at line
550
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_lesense.h