RMUEMLIB
Detailed Description
Reset Management Unit (RMU) Peripheral API.
This module contains functions to control the RMU peripheral of Silicon Labs 32-bit MCUs and SoCs. RMU ensures correct reset operation and is responsible for connecting the different reset sources to the reset lines of the MCU or SoC.
Macros |
|
| #define | RMU_LockupResetDisable (A) RMU_ResetControl ( rmuResetLockUp , A) |
Enumerations |
|
| enum |
RMU_Reset_TypeDef
{
rmuResetBU = _RMU_CTRL_BURSTEN_MASK, rmuResetLockUp = _RMU_CTRL_LOCKUPRDIS_MASK } |
| enum |
RMU_ResetMode_TypeDef
{
rmuResetModeClear = 0, rmuResetModeSet = 1 } |
Functions |
|
| void | RMU_ResetCauseClear (void) |
|
Clear the reset cause register.
|
|
| uint32_t | RMU_ResetCauseGet (void) |
|
Get the cause of the last reset.
|
|
| void | RMU_ResetControl ( RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode) |
|
Disable/enable reset for various peripherals and signal sources.
|
|
Macro Definition Documentation
| #define RMU_LockupResetDisable | ( |
A
|
) | RMU_ResetControl ( rmuResetLockUp , A) |
RMU_LockupResetDisable kept for backwards compatibility.
Definition at line
132
of file
em_rmu.h
.
Enumeration Type Documentation
| enum RMU_Reset_TypeDef |
RMU reset modes.
Definition at line
60
of file
em_rmu.h
.
Function Documentation
| void RMU_ResetCauseClear | ( | void |
|
) |
Clear the reset cause register.
This function clears all the reset cause bits of the RSTCAUSE register. The reset cause bits must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseGet() .
Definition at line
274
of file
em_rmu.c
.
References BUS_RegBitWrite() , EMU_Lock() , and EMU_Unlock() .
Referenced by SLEEP_Init() .
| uint32_t RMU_ResetCauseGet | ( | void |
|
) |
Get the cause of the last reset.
To be useful, the reset cause must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseClear() . This function call will return the main cause for reset, which can be a bit mask (several causes) and clear away "noise".
- Returns
- A reset cause mask. See the reference manual for a description of the reset cause mask.
Definition at line
317
of file
em_rmu.c
.
Referenced by SLEEP_Init() .
| void RMU_ResetControl | ( | RMU_Reset_TypeDef |
reset,
|
| RMU_ResetMode_TypeDef |
mode
|
||
| ) |
Disable/enable reset for various peripherals and signal sources.
- Parameters
-
[in] resetReset types to enable/disable.s [in] modeReset mode.
Definition at line
246
of file
em_rmu.c
.
References BUS_RegBitWrite() , and SL_CTZ() .