DAC_InitChannel_TypeDef Struct ReferenceEMLIB > DAC
DAC channel initialization structure.
Definition at line
185
of file
em_dac.h
.
#include <
em_dac.h
>
Data Fields |
|
| bool | enable |
| bool | prsEnable |
| DAC_PRSSEL_TypeDef | prsSel |
| bool | refreshEnable |
Field Documentation
| bool DAC_InitChannel_TypeDef::enable |
| bool DAC_InitChannel_TypeDef::prsEnable |
Peripheral reflex system trigger enable. If false, channel is triggered by writing to CHnDATA.
Definition at line
193
of file
em_dac.h
.
Referenced by DAC_InitChannel() .
| DAC_PRSSEL_TypeDef DAC_InitChannel_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if
prsEnable
is enabled.
Definition at line
206
of file
em_dac.h
.
Referenced by DAC_InitChannel() .
| bool DAC_InitChannel_TypeDef::refreshEnable |
Enable/disable automatic refresh of channel. Refresh interval must be defined in common control initialization, see DAC_Init() for more information.
Definition at line
200
of file
em_dac.h
.
Referenced by DAC_InitChannel() .
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_dac.h