Utility FunctionsBSP > Thunderboard Sense BSP
Detailed Description
Utility functions.
Macros | |
#define | UTIL_SUPPLY_TYPE_AA 2 |
#define | UTIL_SUPPLY_TYPE_AAA 3 |
#define | UTIL_SUPPLY_TYPE_CR2032 4 |
#define | UTIL_SUPPLY_TYPE_UNKNOWN 0 |
#define | UTIL_SUPPLY_TYPE_USB 1 |
Functions | |
static void | adcDeInit (void) |
De-initializes the A/D converter. | |
static void | adcInit (void) |
Initializes the A/D converter. | |
static uint16_t | getAdcSample (void) |
Initiates an A/D conversion and reads the sample when done. | |
static float | measureSupplyIR (uint8_t loadSetting) |
Measures the unladed and loaded supply voltage and calculates the intermal resistance of the connected supply. The load is provided by the heater element built in the Si7021. | |
static float | measureSupplyVoltage (unsigned int avg) |
Measures the supply voltage by averaging multiple readings. | |
static void | rtcCb (RTCDRV_TimerID_t id, void *user) |
RTC callback function, called when the timer expired. | |
void | SysTick_Handler (void) |
Interrupt Service Routine for system tick counter. | |
void | UTIL_delay (uint32_t ms) |
Delays number of msTick Systicks (1 ms) | |
uint32_t | UTIL_init (void) |
Sets up the SysTick timer for 1ms interrupts and initializes and starts the RTC timer. | |
bool | UTIL_isLowPower (void) |
Checks if the current power supply has low power capability. | |
void | UTIL_shutdown (void) |
Enter lowest power shutdown mode, EM4S. | |
void | UTIL_sleep (uint32_t ms) |
Delays number of milliseconds in sleep mode (EM2) using the RTC. | |
uint32_t | UTIL_sleepInit (void) |
Sets up the RTC timer used for sleep functions. | |
void | UTIL_supplyGetCharacteristics (uint8_t *type, float *voltage, float *ir) |
Retrieves the supply characteristic variables. | |
uint8_t | UTIL_supplyGetType (void) |
Returns the type of the power supply. | |
void | UTIL_supplyProbe (void) |
Probes the connected supply and determines its type. The results are stored in global variables. | |
uint32_t | UTIL_waitForEvent (uint32_t timeout) |
Delays number of milliseconds in sleep mode (EM2) using the RTC but but returns if an event wakes up the MCU. | |
Macro Definition Documentation
#define UTIL_SUPPLY_TYPE_AA 2 |
The board powered from AA batteries
Definition at line 36
of file util.h
.
#define UTIL_SUPPLY_TYPE_AAA 3 |
The board powered from AAA batteries
Definition at line 37
of file util.h
.
Referenced by UTIL_supplyProbe().
#define UTIL_SUPPLY_TYPE_CR2032 4 |
The board powered from a CR2032 battery
Definition at line 38
of file util.h
.
Referenced by UTIL_isLowPower(), and UTIL_supplyProbe().
#define UTIL_SUPPLY_TYPE_UNKNOWN 0 |
Unknown power supply type
Definition at line 34
of file util.h
.
Referenced by UTIL_isLowPower(), and UTIL_supplyProbe().
#define UTIL_SUPPLY_TYPE_USB 1 |
The board powered from the USB connector
Definition at line 35
of file util.h
.
Referenced by UTIL_supplyProbe().
Function Documentation
|
static |
De-initializes the A/D converter.
- Returns
- None
Definition at line 93
of file util_supply.c
.
References PRS_SourceAsyncSignalSet().
Referenced by measureSupplyVoltage().
|
static |
Initializes the A/D converter.
- Returns
- None
Definition at line 59
of file util_supply.c
.
References ADC_InitSingle_TypeDef::acqTime, ADC_Init(), ADC_INIT_DEFAULT, ADC_InitSingle(), ADC_INITSINGLE_DEFAULT, ADC_PrescaleCalc(), ADC_TimebaseCalc(), adcAcqTime16, adcPRSSELCh4, adcRef5VDIFF, CMU_ClockEnable(), cmuClock_ADC0, cmuClock_PRS, ADC_Init_TypeDef::prescale, ADC_InitSingle_TypeDef::prsEnable, ADC_InitSingle_TypeDef::prsSel, ADC_InitSingle_TypeDef::reference, and ADC_Init_TypeDef::timebase.
Referenced by measureSupplyVoltage(), and MIC_init().
|
static |
Initiates an A/D conversion and reads the sample when done.
- Returns
- The output of the A/D conversion
Definition at line 108
of file util_supply.c
.
References ADC_DataSingleGet(), ADC_IntGet(), ADC_Start(), and adcStartSingle.
Referenced by measureSupplyVoltage().
|
static |
Measures the unladed and loaded supply voltage and calculates the intermal resistance of the connected supply. The load is provided by the heater element built in the Si7021.
- Parameters
-
[in] loadSetting
Heater current setting of the Si7021
- Returns
- The measured internal resistance of the connected supply
Definition at line 161
of file util_supply.c
.
References measureSupplyVoltage(), SI7021_CMD_WRITE_HEATER_CTRL, SI7021_CMD_WRITE_USER_REG1, SI7021_cmdWrite(), and UTIL_delay().
Referenced by UTIL_supplyProbe().
|
static |
Measures the supply voltage by averaging multiple readings.
- Parameters
-
[in] avg
Number of measurements to average
- Returns
- The measured voltage
Definition at line 127
of file util_supply.c
.
References adcDeInit(), adcInit(), and getAdcSample().
Referenced by measureSupplyIR(), and UTIL_supplyProbe().
|
static |
RTC callback function, called when the timer expired.
- Parameters
-
[in] id
The id of the timer [in] user
Extra parameter for user application (not used)
- Returns
- None
Definition at line 129
of file util_sleep.c
.
Referenced by UTIL_sleep(), and UTIL_waitForEvent().
void SysTick_Handler | ( | void |
| ) |
Interrupt Service Routine for system tick counter.
- Returns
- None
Definition at line 69
of file util.c
.
void UTIL_delay | ( | uint32_t | ms | ) |
Delays number of msTick Systicks (1 ms)
- Parameters
-
[in] ms
Number of ticks (ms) to delay
- Returns
- None
Definition at line 86
of file util.c
.
References EMU_EnterEM1().
Referenced by BAP_init(), BOARD_flashDeepPowerDown(), BOARD_gasSensorWake(), BOARD_init(), CCS811_init(), HALL_init(), ICM20648_accelGyroCalibrate(), ICM20648_gyroCalibrate(), ICM20648_init(), ICM20648_lowPowerModeEnter(), ICM20648_reset(), ICM20648_wakeOnMotionITEnable(), IMU_config(), measureSupplyIR(), SI1133_init(), SI1133_measureLuxUvi(), SI1133_reset(), SI7021_init(), and SI7021_measure().
uint32_t UTIL_init | ( | void |
| ) |
Sets up the SysTick timer for 1ms interrupts and initializes and starts the RTC timer.
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line 50
of file util.c
.
References CMU_ClockFreqGet(), and cmuClock_CORE.
bool UTIL_isLowPower | ( | void |
| ) |
Checks if the current power supply has low power capability.
- Returns
- True if the supply is low power type, false otherwise
Definition at line 281
of file util_supply.c
.
References UTIL_SUPPLY_TYPE_CR2032, and UTIL_SUPPLY_TYPE_UNKNOWN.
void UTIL_shutdown | ( | void |
| ) |
Enter lowest power shutdown mode, EM4S.
- Returns
- None
Definition at line 105
of file util.c
.
References EMU_EM4Init(), EMU_EM4INIT_DEFAULT, EMU_EnterEM4(), GPIO_EM4EnablePinWakeup(), GPIO_PinModeSet(), and gpioModeInputPullFilter.
void UTIL_sleep | ( | uint32_t | ms | ) |
Delays number of milliseconds in sleep mode (EM2) using the RTC.
- Parameters
-
ms
Number of milliseconds to sleep
- Returns
- None
Definition at line 76
of file util_sleep.c
.
References EMU_EnterEM2(), rtcCb(), RTCDRV_StartTimer(), and rtcdrvTimerTypeOneshot.
uint32_t UTIL_sleepInit | ( | void |
| ) |
Sets up the RTC timer used for sleep functions.
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line 51
of file util_sleep.c
.
References ECODE_EMDRV_RTCDRV_OK, RTCDRV_AllocateTimer(), and RTCDRV_Init().
void UTIL_supplyGetCharacteristics | ( | uint8_t * | type, |
float * | voltage, |
||
float * | ir |
||
) |
Retrieves the supply characteristic variables.
- Parameters
-
[in] type
Supply type [in] voltage
Loaded supply voltage [in] ir
Internal resistance of the supply
- Returns
- None
Definition at line 253
of file util_supply.c
.
uint8_t UTIL_supplyGetType | ( | void |
| ) |
Returns the type of the power supply.
- Returns
- The type of the supply
Definition at line 269
of file util_supply.c
.
void UTIL_supplyProbe | ( | void |
| ) |
Probes the connected supply and determines its type. The results are stored in global variables.
- Returns
- None
Definition at line 208
of file util_supply.c
.
References measureSupplyIR(), measureSupplyVoltage(), SI7021_deInit(), SI7021_init(), UTIL_SUPPLY_TYPE_AAA, UTIL_SUPPLY_TYPE_CR2032, UTIL_SUPPLY_TYPE_UNKNOWN, and UTIL_SUPPLY_TYPE_USB.
uint32_t UTIL_waitForEvent | ( | uint32_t | timeout | ) |
Delays number of milliseconds in sleep mode (EM2) using the RTC but but returns if an event wakes up the MCU.
- Parameters
-
timeout
Timeout, the maximum number of milliseconds to sleep
- Returns
- The number of milliseconds remained from the timeout
Definition at line 98
of file util_sleep.c
.
References EMU_EnterEM2(), rtcCb(), RTCDRV_StartTimer(), RTCDRV_TimeRemaining(), and rtcdrvTimerTypeOneshot.