SMU_PrivilegedAccess_TypeDef Struct ReferenceEMLIB > SMU

SMU peripheral privileged access enablers.

Definition at line 485 of file em_smu.h .

#include < em_smu.h >

Data Fields

bool privilegedACMP0 : 1
bool privilegedACMP1 : 1
bool privilegedADC0 : 1
bool privilegedCMU : 1
bool privilegedCRYOTIMER : 1
bool privilegedCRYPTO : 1
bool privilegedEMU : 1
bool privilegedFPUEH : 1
bool privilegedGPCRC : 1
bool privilegedGPIO : 1
bool privilegedI2C0 : 1
bool privilegedIDAC0 : 1
bool privilegedLDMA : 1
bool privilegedLESENSE : 1
bool privilegedLETIMER0 : 1
bool privilegedLEUART : 1
bool privilegedMSC : 1
bool privilegedPCNT0 : 1
bool privilegedPRS : 1
bool privilegedReserved0 : 1
bool privilegedReserved1 : 1
bool privilegedReserved2 : 1
bool privilegedReserved3 : 1
bool privilegedReserved4 : 1
bool privilegedReserved5 : 1
bool privilegedReserved6 : 1
bool privilegedReserved7 : 1
bool privilegedReserved8 : 1
bool privilegedReserved9 : 1
bool privilegedRMU : 1
bool privilegedRTCC : 1
bool privilegedSMU : 1
bool privilegedTIMER0 : 1
bool privilegedTIMER1 : 1
bool privilegedTRNG0 : 1
bool privilegedUSART0 : 1
bool privilegedUSART1 : 1
bool privilegedVDAC0 : 1
bool privilegedWDOG0 : 1
bool privilegedWDOG1 : 1
bool privilegedWTIMER0 : 1

Field Documentation

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP0

Privileged access enabler for ACMP0.

Definition at line 584 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP1

Privileged access enabler for ACMP1.

Definition at line 585 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedADC0

Privileged access enabler for ADC0.

Definition at line 586 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedCMU

Privileged access enabler for CMU.

Definition at line 589 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYOTIMER

Privileged access enabler for CRYOTIMER.

Definition at line 591 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYPTO

Privileged access enabler for CRYPTO.

Definition at line 592 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedEMU

Privileged access enabler for EMU.

Definition at line 595 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedFPUEH

Privileged access enabler for FPUEH.

Definition at line 596 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedGPCRC

Privileged access enabler for GPCRC.

Definition at line 598 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedGPIO

Privileged access enabler for GPIO.

Definition at line 599 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C0

Privileged access enabler for I2C0.

Definition at line 600 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedIDAC0

Privileged access enabler for IDAC0.

Definition at line 601 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedLDMA

Privileged access enabler for LDMA.

Definition at line 603 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedLESENSE

Privileged access enabler for LESENSE.

Definition at line 604 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedLETIMER0

Privileged access enabler for LETIMER0.

Definition at line 605 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedLEUART

Privileged access enabler for LEUART0.

Definition at line 606 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedMSC

Privileged access enabler for MSC.

Definition at line 602 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedPCNT0

Privileged access enabler for PCNT0.

Definition at line 608 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedPRS

Privileged access enabler for PRS.

Definition at line 594 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved0

Reserved privileged access enabler.

Definition at line 587 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved1

Reserved privileged access enabler.

Definition at line 588 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved2

Reserved privileged access enabler.

Definition at line 590 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved3

Reserved privileged access enabler.

Definition at line 597 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved4

Reserved privileged access enabler.

Definition at line 607 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved5

Reserved privileged access enabler.

Definition at line 609 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved6

Reserved privileged access enabler.

Definition at line 610 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved7

Reserved privileged access enabler.

Definition at line 611 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved8

Reserved privileged access enabler.

Definition at line 612 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved9

Reserved privileged access enabler.

Definition at line 617 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedRMU

Privileged access enabler for RMU.

Definition at line 613 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedRTCC

Privileged access enabler for RTCC.

Definition at line 614 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedSMU

Privileged access enabler for SMU.

Definition at line 615 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER0

Privileged access enabler for TIMER0.

Definition at line 618 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER1

Privileged access enabler for TIMER1.

Definition at line 619 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedTRNG0

Privileged access enabler for TRNG0.

Definition at line 620 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART0

Privileged access enabler for USART0.

Definition at line 621 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART1

Privileged access enabler for USART1.

Definition at line 622 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedVDAC0

Privileged access enabler for VDAC0.

Definition at line 593 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG0

Privileged access enabler for WDOG0.

Definition at line 623 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG1

Privileged access enabler for WDOG1.

Definition at line 624 of file em_smu.h .

bool SMU_PrivilegedAccess_TypeDef::privilegedWTIMER0

Privileged access enabler for WTIMER0.

Definition at line 625 of file em_smu.h .


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/emlib/inc/ em_smu.h