SLEEPTIMEREMDRV
Detailed Description
Low frequency timer utilities.
Utilities (timer, delays and time keeping).
Data Structures |
|
| struct | sl_sleeptimer_timer_handle |
| struct | time_date |
|
Time and Date structure.
|
|
Macros |
|
| #define | ECODE_EMDRV_SLEEPTIMER_OK ( ECODE_OK ) |
|
A successful return value.
|
|
| #define | ECODE_EMDRV_SLEEPTIMER_PARAM_ERROR ( ECODE_EMDRV_SLEEPTIMER_BASE | 0x00000001) |
|
An illegal input parameter.
|
|
| #define | ECODE_EMDRV_SLEEPTIMER_TIMER_NOT_RUNNING ( ECODE_EMDRV_SLEEPTIMER_BASE | 0x00000002) |
|
A timer is not running.
|
|
| #define | SLEEPTIMER_ENUM (name) typedef uint8_t name; enum name##_enum |
Typedefs |
|
| typedef struct time_date | sl_sleeptimer_date_t |
|
Time and Date structure.
|
|
| typedef int32_t | sl_sleeptimer_time_zone_offset_t |
|
Time zone offset from UTC(second).
|
|
| typedef void(* | sl_sleeptimer_timer_callback_t ) ( sl_sleeptimer_timer_handle_t *handle, void *data) |
| typedef struct sl_sleeptimer_timer_handle | sl_sleeptimer_timer_handle_t |
| typedef uint32_t | sl_sleeptimer_timestamp_t |
|
Timestamp, wall clock time in seconds.
|
|
Typedef Documentation
| typedef void(* sl_sleeptimer_timer_callback_t) ( sl_sleeptimer_timer_handle_t *handle, void *data) |
Typedef for the user supplied callback function which is called when a timer expires.
- Parameters
-
handleThe timer handle. dataAn extra parameter for the user application.
Definition at line
64
of file
sleeptimer.h
.
Function Documentation
| void sl_sleeptimer_delay_millisecond | ( | uint16_t |
time_ms
|
) |
Active delay.
- Parameters
-
time_msDelay duration in milliseconds.
Definition at line
684
of file
sleeptimer.c
.
References ECODE_EMDRV_SLEEPTIMER_OK , sl_sleeptimer_ms_to_tick() , and sl_sleeptimer_start_timer() .
| uint32_t sl_sleeptimer_get_tick_count | ( | void |
|
) |
Gets current 32 bits global tick count.
- Returns
- Current tick count.
Gets current 32 bits tick count.
Definition at line
301
of file
sleeptimer.c
.
| uint64_t sl_sleeptimer_get_tick_count64 | ( | void |
|
) |
Gets current 64 bits global tick count.
- Returns
- Current tick count.
Gets current 64 bits tick count.
Definition at line
309
of file
sleeptimer.c
.
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , and CORE_EXIT_ATOMIC .
| uint32_t sl_sleeptimer_get_timer_frequency | ( | void |
|
) |
Get timer frequency.
- Returns
- 0 if successful. Error code otherwise.
Get timer frequency.
Definition at line
324
of file
sleeptimer.c
.
| Ecode_t sl_sleeptimer_get_timer_time_remaining | ( | sl_sleeptimer_timer_handle_t * |
handle,
|
| uint32_t * |
time
|
||
| ) |
Gets remaining time until timer expires.
- Parameters
-
handlePointer to handle to timer. timeTime left in timer ticks.
- Returns
- 0 if successful. Error code otherwise.
Gets a 32 bits timer's time remaining.
Definition at line
259
of file
sleeptimer.c
.
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , sl_sleeptimer_timer_handle::delta , ECODE_EMDRV_SLEEPTIMER_OK , ECODE_EMDRV_SLEEPTIMER_PARAM_ERROR , ECODE_EMDRV_SLEEPTIMER_TIMER_NOT_RUNNING , and sl_sleeptimer_timer_handle::next .
| Ecode_t sl_sleeptimer_init | ( | void |
|
) |
Initializes the Sleeptimer.
- Returns
- 0 if successful. Error code otherwise.
Initializes sleep timer.
Definition at line
126
of file
sleeptimer.c
.
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , and ECODE_EMDRV_SLEEPTIMER_OK .
| Ecode_t sl_sleeptimer_is_timer_running | ( | sl_sleeptimer_timer_handle_t * |
handle,
|
| bool * |
running
|
||
| ) |
Gets the status of a timer.
- Parameters
-
handlePointer to handle to timer. runningPointer to the status of the timer.
- Returns
- 0 if successful. Error code otherwise.
Gets the status of a timer.
Definition at line
232
of file
sleeptimer.c
.
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , ECODE_EMDRV_SLEEPTIMER_OK , ECODE_EMDRV_SLEEPTIMER_PARAM_ERROR , and sl_sleeptimer_timer_handle::next .
| Ecode_t sl_sleeptimer_ms32_to_tick | ( | uint32_t |
time_ms,
|
| uint32_t * |
tick
|
||
| ) |
Converts 32-bits milliseconds in ticks.
- Parameters
-
time_msNumber of milliseconds. tickPointer to the converted tick number.
- Returns
- 0 if successful. Error code otherwise.
- Note
- The result is "rounded" to the superior tick number. If possible the sl_sleeptimer_ms_to_tick() function should be used. The millisecond 32-bits range is not fully supported, depending on the timer frequency. The function will return an error if the converted number of ticks would overflow.
Definition at line
713
of file
sleeptimer.c
.
References ECODE_EMDRV_SLEEPTIMER_OK , and ECODE_EMDRV_SLEEPTIMER_PARAM_ERROR .
| uint32_t sl_sleeptimer_ms_to_tick | ( | uint16_t |
time_ms
|
) |
Converts milliseconds in ticks.
- Parameters
-
time_msNumber of milliseconds.
- Returns
- Corresponding ticks number.
- Note
- The result is "rounded" to the superior tick number. This function is light and cannot fail so it should be privilegied to perform a millisecond to tick conversion.
Definition at line
705
of file
sleeptimer.c
.
Referenced by sl_sleeptimer_delay_millisecond() .
| Ecode_t sl_sleeptimer_start_periodic_timer | ( | sl_sleeptimer_timer_handle_t * |
handle,
|
| uint32_t |
timeout,
|
||
| sl_sleeptimer_timer_callback_t |
callback,
|
||
| void * |
callback_data,
|
||
| uint8_t |
priority
|
||
| ) |
Starts a 32 bits periodic timer.
- Parameters
-
handlePointer to handle to timer. timeoutTimer periodic timeout, in timer ticks. callbackCallback function that will be called when initial/periodic timeout expires. callbackDataPointer to user data that will be passed to callback. priorityPriority of callback. Useful in case multiple timer expire at the same time. 0 = highest priority.
- Returns
- 0 if successful. Error code otherwise.
Starts a 32 bits periodic timer.
Definition at line
175
of file
sleeptimer.c
.
References ECODE_EMDRV_SLEEPTIMER_PARAM_ERROR .
| Ecode_t sl_sleeptimer_start_timer | ( | sl_sleeptimer_timer_handle_t * |
handle,
|
| uint32_t |
timeout,
|
||
| sl_sleeptimer_timer_callback_t |
callback,
|
||
| void * |
callback_data,
|
||
| uint8_t |
priority
|
||
| ) |
Starts a 32 bits timer.
- Parameters
-
handlePointer to handle to timer. timeoutTimer timeout, in timer ticks. callbackCallback function that will be called when initial/periodic timeout expires. callbackDataPointer to user data that will be passed to callback. priorityPriority of callback. Useful in case multiple timer expire at the same time. 0 = highest priority.
- Returns
- 0 if successful. Error code otherwise.
Starts a 32 bits timer.
Definition at line
154
of file
sleeptimer.c
.
References ECODE_EMDRV_SLEEPTIMER_PARAM_ERROR .
Referenced by sl_sleeptimer_delay_millisecond() .
| Ecode_t sl_sleeptimer_stop_timer | ( | sl_sleeptimer_timer_handle_t * |
handle
|
) |
Stops a timer.
- Parameters
-
handlePointer to handle to timer.
- Returns
Stops a 32 bits timer.
Definition at line
196
of file
sleeptimer.c
.
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , ECODE_EMDRV_SLEEPTIMER_OK , and ECODE_EMDRV_SLEEPTIMER_PARAM_ERROR .
| Ecode_t sl_sleeptimer_tick64_to_ms | ( | uint64_t |
tick,
|
| uint64_t * |
ms
|
||
| ) |
Converts 64-bit ticks in milliseconds.
- Parameters
-
tickNumber of tick. msPointer to the converted milliseconds number.
- Returns
- 0 if successful. Error code otherwise.
- Note
- The result is rounded to the inferior millisecond.
Definition at line
739
of file
sleeptimer.c
.
References ECODE_EMDRV_SLEEPTIMER_OK , and ECODE_EMDRV_SLEEPTIMER_PARAM_ERROR .
| uint32_t sl_sleeptimer_tick_to_ms | ( | uint32_t |
tick
|
) |
Converts ticks in milliseconds.
- Parameters
-
tickNumber of tick.
- Returns
- Corresponding milliseconds number.
- Note
- The result is rounded to the inferior millisecond.
Definition at line
727
of file
sleeptimer.c
.