LESENSE_CH_TypeDef Struct ReferenceDevicesDevices > | LESENSE
LESENSE_CH LESENSE CH Register
.
       Definition at line
       
        46
       
       of file
       
        efr32fg12p_lesense_ch.h
       
       .
      
      
       #include <
       
     
        efr32fg12p_lesense_ch.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | EVAL | 
| __IOM uint32_t | INTERACT | 
| uint32_t | RESERVED0 [1U] | 
| __IOM uint32_t | TIMING | 
Field Documentation
| __IOM uint32_t LESENSE_CH_TypeDef::EVAL | 
Scan Configuration
        Definition at line
        
         49
        
        of file
        
         efr32fg12p_lesense_ch.h
        
        .
       
Referenced by LESENSE_ChannelSlidingWindow() , and LESENSE_ChannelStepDetection() .
| __IOM uint32_t LESENSE_CH_TypeDef::INTERACT | 
Scan Configuration
        Definition at line
        
         48
        
        of file
        
         efr32fg12p_lesense_ch.h
        
        .
       
| uint32_t LESENSE_CH_TypeDef::RESERVED0[1U] | 
Reserved future
        Definition at line
        
         50
        
        of file
        
         efr32fg12p_lesense_ch.h
        
        .
       
| __IOM uint32_t LESENSE_CH_TypeDef::TIMING | 
Scan Configuration
        Definition at line
        
         47
        
        of file
        
         efr32fg12p_lesense_ch.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/platform/Device/SiliconLabs/EFR32FG12P/Include/
       efr32fg12p_lesense_ch.h