ARING_TypeDef Struct ReferenceKit Drivers > SegmentLcd

Defines segment COM and BIT fields for A-wheel (suited for Anim)

Definition at line 107 of file segmentlcd.c.

Data Fields

uint8_t bit [8]
 
uint8_t com [8]
 

Field Documentation

uint8_t ARING_TypeDef::bit[8]

LCD bit number

Definition at line 109 of file segmentlcd.c.

uint8_t ARING_TypeDef::com[8]

LCD COM line (for multiplexing)

Definition at line 108 of file segmentlcd.c.


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/hardware/kit/common/drivers/segmentlcd.c