USART_InitAsync_TypeDef Struct ReferenceEMLIB > USART
Asynchronous mode initialization structure.
Definition at line 282
of file em_usart.h
.
#include <
em_usart.h
>
Data Fields | |
bool | autoCsEnable |
uint8_t | autoCsHold |
uint8_t | autoCsSetup |
uint32_t | baudrate |
USART_Databits_TypeDef | databits |
USART_Enable_TypeDef | enable |
USART_HwFlowControl_TypeDef | hwFlowControl |
bool | mvdis |
USART_OVS_TypeDef | oversampling |
USART_Parity_TypeDef | parity |
USART_PRS_Channel_t | prsRxCh |
bool | prsRxEnable |
uint32_t | refFreq |
USART_Stopbits_TypeDef | stopbits |
Field Documentation
bool USART_InitAsync_TypeDef::autoCsEnable |
uint8_t USART_InitAsync_TypeDef::autoCsHold |
Auto CS hold time in baud cycles.
Definition at line 324
of file em_usart.h
.
Referenced by USART_InitAsync().
uint8_t USART_InitAsync_TypeDef::autoCsSetup |
Auto CS setup time in baud cycles.
Definition at line 327
of file em_usart.h
.
Referenced by USART_InitAsync().
uint32_t USART_InitAsync_TypeDef::baudrate |
Desired baud rate.
Definition at line 293
of file em_usart.h
.
Referenced by UARTDRV_InitUart(), and USART_InitAsync().
USART_Databits_TypeDef USART_InitAsync_TypeDef::databits |
Number of data bits in frame. Notice that UART modules only support 8 or 9 data bits.
Definition at line 300
of file em_usart.h
.
Referenced by UARTDRV_InitUart(), and USART_InitAsync().
USART_Enable_TypeDef USART_InitAsync_TypeDef::enable |
Specifies whether TX and/or RX is enabled when initialization is completed.
Definition at line 284
of file em_usart.h
.
Referenced by RETARGET_SerialInit(), UARTDRV_InitUart(), and USART_InitAsync().
USART_HwFlowControl_TypeDef USART_InitAsync_TypeDef::hwFlowControl |
Hardware flow control mode.
Definition at line 330
of file em_usart.h
.
Referenced by USART_InitAsync().
bool USART_InitAsync_TypeDef::mvdis |
Majority Vote Disable for 16x, 8x and 6x oversampling modes.
Definition at line 310
of file em_usart.h
.
Referenced by UARTDRV_InitUart(), and USART_InitAsync().
USART_OVS_TypeDef USART_InitAsync_TypeDef::oversampling |
Oversampling used.
Definition at line 296
of file em_usart.h
.
Referenced by UARTDRV_InitUart(), and USART_InitAsync().
USART_Parity_TypeDef USART_InitAsync_TypeDef::parity |
Parity mode to use.
Definition at line 303
of file em_usart.h
.
Referenced by UARTDRV_InitUart(), and USART_InitAsync().
USART_PRS_Channel_t USART_InitAsync_TypeDef::prsRxCh |
Select PRS channel for USART Rx. (Only valid if prsRxEnable is true).
Definition at line 316
of file em_usart.h
.
Referenced by USART_InitAsync().
bool USART_InitAsync_TypeDef::prsRxEnable |
Enable USART Rx via PRS.
Definition at line 313
of file em_usart.h
.
Referenced by USART_InitAsync().
uint32_t USART_InitAsync_TypeDef::refFreq |
USART/UART reference clock assumed when configuring baud rate setup. Set to 0 to use the currently configured reference clock.
Definition at line 290
of file em_usart.h
.
Referenced by USART_InitAsync().
USART_Stopbits_TypeDef USART_InitAsync_TypeDef::stopbits |
Number of stop bits to use.
Definition at line 306
of file em_usart.h
.
Referenced by UARTDRV_InitUart(), and USART_InitAsync().
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_usart.h