RTCC
Detailed Description
Real Time Counter (RTCC) Peripheral API.
This module contains functions to control the RTCC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTCC ensures timekeeping in low energy modes. The RTCC also includes a BCD calendar mode for easy time and date keeping.
Data Structures | |
struct | RTCC_CCChConf_TypeDef |
struct | RTCC_Init_TypeDef |
Macros | |
#define | RTCC_CH_INIT_CAPTURE_DEFAULT |
#define | RTCC_CH_INIT_COMPARE_DEFAULT |
#define | RTCC_CH_VALID(ch) ((unsigned)(ch) < RTCC_CC_NUM) |
#define | RTCC_INIT_DEFAULT |
#define | rtccPRSCh0 0U |
#define | rtccPRSCh1 1U |
#define | rtccPRSCh10 10U |
#define | rtccPRSCh11 11U |
#define | rtccPRSCh2 2U |
#define | rtccPRSCh3 3U |
#define | rtccPRSCh4 4U |
#define | rtccPRSCh5 5U |
#define | rtccPRSCh6 6U |
#define | rtccPRSCh7 7U |
#define | rtccPRSCh8 8U |
#define | rtccPRSCh9 9U |
Typedefs | |
typedef uint8_t | RTCC_PRSSel_TypeDef |
Enumerations | |
enum | RTCC_CapComChMode_TypeDef { rtccCapComChModeOff = _RTCC_CC_CTRL_MODE_OFF, rtccCapComChModeCapture = _RTCC_CC_CTRL_MODE_INPUTCAPTURE, rtccCapComChModeCompare = _RTCC_CC_CTRL_MODE_OUTPUTCOMPARE } |
enum | RTCC_CntPresc_TypeDef { rtccCntPresc_1 = _RTCC_CFG_CNTPRESC_DIV1, rtccCntPresc_2 = _RTCC_CFG_CNTPRESC_DIV2, rtccCntPresc_4 = _RTCC_CFG_CNTPRESC_DIV4, rtccCntPresc_8 = _RTCC_CFG_CNTPRESC_DIV8, rtccCntPresc_16 = _RTCC_CFG_CNTPRESC_DIV16, rtccCntPresc_32 = _RTCC_CFG_CNTPRESC_DIV32, rtccCntPresc_64 = _RTCC_CFG_CNTPRESC_DIV64, rtccCntPresc_128 = _RTCC_CFG_CNTPRESC_DIV128, rtccCntPresc_256 = _RTCC_CFG_CNTPRESC_DIV256, rtccCntPresc_512 = _RTCC_CFG_CNTPRESC_DIV512, rtccCntPresc_1024 = _RTCC_CFG_CNTPRESC_DIV1024, rtccCntPresc_2048 = _RTCC_CFG_CNTPRESC_DIV2048, rtccCntPresc_4096 = _RTCC_CFG_CNTPRESC_DIV4096, rtccCntPresc_8192 = _RTCC_CFG_CNTPRESC_DIV8192, rtccCntPresc_16384 = _RTCC_CFG_CNTPRESC_DIV16384, rtccCntPresc_32768 = _RTCC_CFG_CNTPRESC_DIV32768 } |
enum | RTCC_CompBase_TypeDef { rtccCompBaseCnt = _RTCC_CC_CTRL_COMPBASE_CNT, rtccCompBasePreCnt = _RTCC_CC_CTRL_COMPBASE_PRECNT } |
enum | RTCC_CompMatchOutAction_TypeDef { rtccCompMatchOutActionPulse = _RTCC_CC_CTRL_CMOA_PULSE, rtccCompMatchOutActionToggle = _RTCC_CC_CTRL_CMOA_TOGGLE, rtccCompMatchOutActionClear = _RTCC_CC_CTRL_CMOA_CLEAR, rtccCompMatchOutActionSet = _RTCC_CC_CTRL_CMOA_SET } |
enum | RTCC_InEdgeSel_TypeDef { rtccInEdgeRising = _RTCC_CC_CTRL_ICEDGE_RISING, rtccInEdgeFalling = _RTCC_CC_CTRL_ICEDGE_FALLING, rtccInEdgeBoth = _RTCC_CC_CTRL_ICEDGE_BOTH, rtccInEdgeNone = _RTCC_CC_CTRL_ICEDGE_NONE } |
enum | RTCC_PrescMode_TypeDef { rtccCntTickPresc = _RTCC_CFG_CNTTICK_PRESC, rtccCntTickCCV0Match = _RTCC_CFG_CNTTICK_CCV0MATCH } |
Functions | |
__STATIC_INLINE uint32_t | RTCC_ChannelCaptureValueGet (int ch) |
Get RTCC input capture register value for selected channel. | |
__STATIC_INLINE uint32_t | RTCC_ChannelCCVGet (int ch) |
Get RTCC capture/compare register value for selected channel. For parts with separate capture compare value registers, this function returns the compare value. | |
__STATIC_INLINE void | RTCC_ChannelCCVSet (int ch, uint32_t value) |
Set RTCC capture/compare register value for selected channel. For parts with separate capture compare value registers, this function sets the compare value. | |
__STATIC_INLINE uint32_t | RTCC_ChannelCompareValueGet (int ch) |
Get RTCC compare register value for selected channel. | |
__STATIC_INLINE void | RTCC_ChannelCompareValueSet (int ch, uint32_t value) |
Set RTCC compare register value for selected channel. | |
void | RTCC_ChannelInit (int ch, RTCC_CCChConf_TypeDef const *confPtr) |
Configure the selected capture/compare channel of the RTCC. | |
__STATIC_INLINE uint32_t | RTCC_CombinedCounterGet (void) |
Get combined CNT/PRECNT register content. | |
__STATIC_INLINE uint32_t | RTCC_CounterGet (void) |
Get RTCC counter value. | |
__STATIC_INLINE void | RTCC_CounterSet (uint32_t value) |
Set RTCC CNT counter. | |
void | RTCC_Enable (bool enable) |
Enable/disable RTCC counting. | |
void | RTCC_Init (const RTCC_Init_TypeDef *init) |
Initialize RTCC. | |
__STATIC_INLINE void | RTCC_IntClear (uint32_t flags) |
Clear one or more pending RTCC interrupts. | |
__STATIC_INLINE void | RTCC_IntDisable (uint32_t flags) |
Disable one or more RTCC interrupts. | |
__STATIC_INLINE void | RTCC_IntEnable (uint32_t flags) |
Enable one or more RTCC interrupts. | |
__STATIC_INLINE uint32_t | RTCC_IntGet (void) |
Get pending RTCC interrupt flags. | |
__STATIC_INLINE uint32_t | RTCC_IntGetEnabled (void) |
Get enabled and pending RTCC interrupt flags. | |
__STATIC_INLINE void | RTCC_IntSet (uint32_t flags) |
Set one or more pending RTCC interrupts from SW. | |
__STATIC_INLINE void | RTCC_Lock (void) |
Lock RTCC registers. | |
__STATIC_INLINE uint32_t | RTCC_PreCounterGet (void) |
Get RTCC pre-counter value. | |
__STATIC_INLINE void | RTCC_PreCounterSet (uint32_t preCntVal) |
Set RTCC pre-counter value. | |
void | RTCC_Reset (void) |
Restore RTCC to its reset state. | |
__STATIC_INLINE void | RTCC_Start (void) |
Start RTCC counter. | |
void | RTCC_StatusClear (void) |
Clear the STATUS register. | |
__STATIC_INLINE uint32_t | RTCC_StatusGet (void) |
Get STATUS register value. | |
__STATIC_INLINE void | RTCC_Stop (void) |
Stop the RTCC counter. | |
__STATIC_INLINE void | RTCC_SyncWait (void) |
Wait for the RTCC to complete all synchronization of register changes and commands. | |
__STATIC_INLINE void | RTCC_Unlock (void) |
Unlock RTCC registers. | |
Macro Definition Documentation
#define RTCC_CH_INIT_CAPTURE_DEFAULT |
Default RTCC channel input capture initialization structure.
Definition at line 345
of file em_rtcc.h
.
#define RTCC_CH_INIT_COMPARE_DEFAULT |
Default RTCC channel output compare initialization structure.
Definition at line 335
of file em_rtcc.h
.
#define RTCC_CH_VALID | ( | ch | ) | ((unsigned)(ch) < RTCC_CC_NUM) |
Number of RTCC capture/compare channels Validation of valid RTCC channel for assert statements.
Definition at line 388
of file em_rtcc.h
.
Referenced by RTCC_ChannelCaptureValueGet(), RTCC_ChannelCompareValueGet(), RTCC_ChannelCompareValueSet(), and RTCC_ChannelInit().
#define RTCC_INIT_DEFAULT |
Default RTCC initialization structure.
Definition at line 292
of file em_rtcc.h
.
Referenced by UDELAY_Calibrate().
#define rtccPRSCh0 0U |
Deprecated PRS channel values. New code should use an integer instead of using these deprecated enum values.
Definition at line 170
of file em_rtcc.h
.
Typedef Documentation
typedef uint8_t RTCC_PRSSel_TypeDef |
PRS channel number. This type is used when configuring input capture mode on a RTCC channel.
Definition at line 166
of file em_rtcc.h
.
Enumeration Type Documentation
Counter prescaler selection.
Definition at line 107
of file em_rtcc.h
.
Function Documentation
__STATIC_INLINE uint32_t RTCC_ChannelCaptureValueGet | ( | int | ch | ) |
Get RTCC input capture register value for selected channel.
- Parameters
-
[in] ch
Channel selector.
- Returns
- Capture register value.
Definition at line 444
of file em_rtcc.h
.
References RTCC_CH_VALID.
__STATIC_INLINE uint32_t RTCC_ChannelCCVGet | ( | int | ch | ) |
Get RTCC capture/compare register value for selected channel. For parts with separate capture compare value registers, this function returns the compare value.
- Parameters
-
[in] ch
Channel selector.
- Returns
- Capture/compare register value.
Definition at line 466
of file em_rtcc.h
.
References RTCC_ChannelCompareValueGet().
__STATIC_INLINE void RTCC_ChannelCCVSet | ( | int | ch, |
uint32_t | value |
||
) |
Set RTCC capture/compare register value for selected channel. For parts with separate capture compare value registers, this function sets the compare value.
- Parameters
-
[in] ch
Channel selector. [in] value
Capture/compare register value
Definition at line 483
of file em_rtcc.h
.
References RTCC_ChannelCompareValueSet().
__STATIC_INLINE uint32_t RTCC_ChannelCompareValueGet | ( | int | ch | ) |
Get RTCC compare register value for selected channel.
- Parameters
-
[in] ch
Channel selector.
- Returns
- Compare register value.
Definition at line 404
of file em_rtcc.h
.
References RTCC_CH_VALID.
Referenced by RTCC_ChannelCCVGet().
__STATIC_INLINE void RTCC_ChannelCompareValueSet | ( | int | ch, |
uint32_t | value |
||
) |
Set RTCC compare register value for selected channel.
- Parameters
-
[in] ch
Channel selector. [in] value
Compare register value
Definition at line 424
of file em_rtcc.h
.
References RTCC_CH_VALID.
Referenced by RTCC_ChannelCCVSet().
void RTCC_ChannelInit | ( | int | ch, |
RTCC_CCChConf_TypeDef const * | confPtr |
||
) |
Configure the selected capture/compare channel of the RTCC.
Use this function to configure an RTCC channel. Select capture/compare mode, match output action, overflow output action, and PRS input configuration. See the configuration structure RTCC_CCChConf_TypeDef for more details.
- Parameters
-
[in] ch
A channel selector. [in] confPtr
A pointer to the configuration structure.
Configure the selected capture/compare channel.
Definition at line 79
of file em_rtcc.c
.
References RTCC_CCChConf_TypeDef::chMode, RTCC_CCChConf_TypeDef::compBase, RTCC_CCChConf_TypeDef::compMatchOutAction, RTCC_CCChConf_TypeDef::inputEdgeSel, RTCC_CCChConf_TypeDef::prsSel, RTCC_CH_VALID, and rtccCapComChModeCapture.
Referenced by RTCDRV_Init().
__STATIC_INLINE uint32_t RTCC_CombinedCounterGet | ( | void |
| ) |
Get combined CNT/PRECNT register content.
- Returns
- CNT/PRECNT register value.
Definition at line 561
of file em_rtcc.h
.
__STATIC_INLINE uint32_t RTCC_CounterGet | ( | void |
| ) |
Get RTCC counter value.
- Returns
- Current RTCC counter value.
Definition at line 578
of file em_rtcc.h
.
__STATIC_INLINE void RTCC_CounterSet | ( | uint32_t | value | ) |
Set RTCC CNT counter.
- Parameters
-
[in] value
CNT value.
Definition at line 595
of file em_rtcc.h
.
void RTCC_Enable | ( | bool | enable | ) |
Enable/disable RTCC counting.
- Parameters
-
[in] enable
True to enable RTCC counting, false to disable counting.
Definition at line 117
of file em_rtcc.c
.
References BUS_RegBitWrite(), RTCC_Start(), RTCC_Stop(), and RTCC_SyncWait().
Referenced by RTCDRV_DeInit(), and UDELAY_Calibrate().
void RTCC_Init | ( | const RTCC_Init_TypeDef * | init | ) |
Initialize RTCC.
Note that the compare values must be set separately with RTCC_CompareSet(), which should probably be done prior to the use of this function if configuring the RTCC to start when initialization is completed.
- Parameters
-
[in] init
A pointer to the RTCC initialization structure.
Definition at line 157
of file em_rtcc.c
.
References RTCC_Init_TypeDef::cntWrapOnCCV1, RTCC_Init_TypeDef::debugRun, RTCC_Init_TypeDef::enable, RTCC_Init_TypeDef::precntWrapOnCCV0, RTCC_Init_TypeDef::presc, RTCC_Init_TypeDef::prescMode, and RTCC_SyncWait().
Referenced by RTCDRV_Init(), and UDELAY_Calibrate().
__STATIC_INLINE void RTCC_IntClear | ( | uint32_t | flags | ) |
Clear one or more pending RTCC interrupts.
- Parameters
-
[in] flags
RTCC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources.
Definition at line 664
of file em_rtcc.h
.
Referenced by RTCC_IRQHandler(), and RTCC_Reset().
__STATIC_INLINE void RTCC_IntDisable | ( | uint32_t | flags | ) |
Disable one or more RTCC interrupts.
- Parameters
-
[in] flags
RTCC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt.
Definition at line 681
of file em_rtcc.h
.
__STATIC_INLINE void RTCC_IntEnable | ( | uint32_t | flags | ) |
Enable one or more RTCC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using RTCC_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] flags
RTCC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt.
Definition at line 699
of file em_rtcc.h
.
__STATIC_INLINE uint32_t RTCC_IntGet | ( | void |
| ) |
Get pending RTCC interrupt flags.
- Note
- Event bits are not cleared by using this function.
- Returns
- Pending RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.
Definition at line 715
of file em_rtcc.h
.
Referenced by RTCC_IRQHandler().
__STATIC_INLINE uint32_t RTCC_IntGetEnabled | ( | void |
| ) |
Get enabled and pending RTCC interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Returns
- Pending and enabled RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.
Definition at line 731
of file em_rtcc.h
.
__STATIC_INLINE void RTCC_IntSet | ( | uint32_t | flags | ) |
Set one or more pending RTCC interrupts from SW.
- Parameters
-
[in] flags
RTCC interrupt sources to set to pending. Use a set of interrupt flags (RTCC_IFS_nnn).
Definition at line 749
of file em_rtcc.h
.
__STATIC_INLINE void RTCC_Lock | ( | void |
| ) |
Lock RTCC registers.
- Note
- When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.
Definition at line 767
of file em_rtcc.h
.
__STATIC_INLINE uint32_t RTCC_PreCounterGet | ( | void |
| ) |
Get RTCC pre-counter value.
- Returns
- Current RTCC pre-counter value.
Definition at line 796
of file em_rtcc.h
.
__STATIC_INLINE void RTCC_PreCounterSet | ( | uint32_t | preCntVal | ) |
Set RTCC pre-counter value.
- Parameters
-
[in] preCntVal
RTCC pre-counter value to be set.
Definition at line 813
of file em_rtcc.h
.
__STATIC_INLINE void RTCC_Start | ( | void |
| ) |
Start RTCC counter.
This function will send a start command to the RTCC peripheral. The RTCC peripheral will use some LF clock ticks before the command is executed. The RTCC_SyncWait() function can be used to wait for the start command to be executed.
- Note
- This function requires the RTCC to be enabled.
Definition at line 893
of file em_rtcc.h
.
References RTCC_SyncWait().
Referenced by RTCC_Enable().
__STATIC_INLINE uint32_t RTCC_StatusGet | ( | void |
| ) |
Get STATUS register value.
- Returns
- Current STATUS register value.
Definition at line 853
of file em_rtcc.h
.
__STATIC_INLINE void RTCC_Stop | ( | void |
| ) |
Stop the RTCC counter.
This function will send a stop command to the RTCC peripheral. The RTCC peripheral will use some LF clock ticks before the command is executed. The RTCC_SyncWait() function can be used to wait for the stop command to be executed.
- Note
- This function requires the RTCC to be enabled.
Definition at line 912
of file em_rtcc.h
.
References RTCC_SyncWait().
Referenced by RTCC_Enable(), and RTCC_Reset().
__STATIC_INLINE void RTCC_Unlock | ( | void |
| ) |
Unlock RTCC registers.
- Note
- When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.
Definition at line 954
of file em_rtcc.h
.
Referenced by RTCC_Reset().