TOUCH_Config_TypeDef Struct Reference
Touch configuration structure
Definition at line 69
of file touch.h
.
#include <
touch.h
>
Data Fields | |
uint32_t | frequency |
uint8_t | ignore |
ADC_OvsRateSel_TypeDef | oversampling |
Field Documentation
uint32_t TOUCH_Config_TypeDef::frequency |
ADC frequency, min 32kHz, max 13MHz, typical 500kHz
Definition at line 70
of file touch.h
.
Referenced by TOUCH_Init().
uint8_t TOUCH_Config_TypeDef::ignore |
Ignore move if it has not at least defined pixels
Definition at line 71
of file touch.h
.
Referenced by TOUCH_Init().
ADC_OvsRateSel_TypeDef TOUCH_Config_TypeDef::oversampling |
ADC oversampling used during touch reading
Definition at line 72
of file touch.h
.
Referenced by TOUCH_Init().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/hardware/kit/common/drivers/
touch.h