Detailed Description

Driver for SSD2119 TFT in Direct Drive or Adress Mapped mode.

Functions

void SPI_TFT_Init (void)
 Initialize SPI interface to TFT-LCD SSD2119 controller.
 
void SPI_TFT_WriteRegister (uint8_t reg, uint16_t data)
 Write registers to SSD2119 controller.
 
bool TFT_AddressMappedInit (void)
 TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
 
void TFT_DirectGPIOConfig (void)
 GPIO configuration for TFT direct drive.
 
bool TFT_DirectInit (const EBI_TFTInit_TypeDef *tftInit)
 TFT initialization funxction. Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
 

Variables

static const USART_InitSync_TypeDef inittft
 
static bool runOnce = true
 
static bool runOnce = true
 

Function Documentation

void SPI_TFT_Init ( void  )

Initialize SPI interface to TFT-LCD SSD2119 controller.

Note
To enable access, be sure to call the function BSP_PeripheralAccess() before using this interface.

Definition at line 69 of file tftspi.c.

References CMU_ClockEnable(), cmuClock_GPIO, cmuClock_HFPER, cmuClock_USART1, GPIO_PinModeSet(), gpioModeInput, gpioModePushPull, USART_InitSync(), and USART_Reset().

void SPI_TFT_WriteRegister ( uint8_t  reg,
uint16_t  data 
)

Write registers to SSD2119 controller.

Parameters
[in]regRegister to write to
[in]data16-bit data to write into register
Note
It is not possible to read back register value through SSD2119 SPI interface.

Definition at line 104 of file tftspi.c.

References GPIO_PinOutClear(), GPIO_PinOutSet(), USART_Rx(), and USART_Tx().

bool TFT_AddressMappedInit ( void  )

TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)

Returns
true if we should redraw into buffer, false if BC has control over display

Definition at line 61 of file tftamapped.c.

References BC_ARB_CTRL_EBI, BC_REGISTER, BC_SPI_DEMUX_SLAVE_AUDIO, BC_SPI_DEMUX_SLAVE_DISPLAY, BC_SSD2119_BASE, BC_UIF_AEM_EFM, BSP_Display_EBI, BSP_Display_Mode8080, BSP_Display_PowerDisable, BSP_Display_PowerEnable, BSP_Display_ResetAssert, BSP_Display_ResetRelease, BSP_DisplayControl(), BSP_RegisterRead(), BSP_RegisterWrite(), runOnce, and SystemCoreClockGet().

bool TFT_DirectInit ( const EBI_TFTInit_TypeDef *  tftInit)

TFT initialization funxction. Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)

Parameters
[in]tftInitPointer to EBI TFT initialization structure
Returns
true if we should redraw into buffer, false if BC has control over display

Definition at line 77 of file tftdirect.c.

References BC_ARB_CTRL_EBI, BC_REGISTER, BC_UIF_AEM_EFM, BSP_Display_EBI, BSP_Display_ModeGeneric, BSP_Display_PowerDisable, BSP_Display_PowerEnable, BSP_Display_ResetAssert, BSP_Display_ResetRelease, BSP_DisplayControl(), BSP_PeripheralAccess(), BSP_RegisterRead(), BSP_TFT, runOnce, SystemCoreClockGet(), and TFT_DirectGPIOConfig().

Variable Documentation

const USART_InitSync_TypeDef inittft
static
Initial value:
= {
48000000,
1000000,
true,
true,
false,
usartPrsRxCh0,
false,
false
}
Definition: em_usart.h:130
Definition: em_usart.h:185
Definition: em_usart.h:108

Set default values for tft synchronous mode init structure

Definition at line 50 of file tftspi.c.

bool runOnce = true
static

Flag to indicate that we need to initialize once if starting up in

Definition at line 51 of file tftdirect.c.

Referenced by TFT_DirectInit().

bool runOnce = true
static

Flag to indicate that we need to initialize once if starting up in

Definition at line 52 of file tftamapped.c.

Referenced by TFT_AddressMappedInit().