EMU_VmonHystInit_TypeDef Struct Reference

VMON Hysteresis initialization structure.

Definition at line 881 of file em_emu.h.

#include <em_emu.h>

Data Fields

EMU_VmonChannel_TypeDef channel
 
bool enable
 
int fallThreshold
 
bool fallWakeup
 
int riseThreshold
 
bool riseWakeup
 

Field Documentation

EMU_VmonChannel_TypeDef EMU_VmonHystInit_TypeDef::channel

VMON channel to configure.

Definition at line 882 of file em_emu.h.

Referenced by EMU_VmonHystInit().

bool EMU_VmonHystInit_TypeDef::enable

Enable VMON channel.

Definition at line 887 of file em_emu.h.

Referenced by EMU_VmonHystInit().

int EMU_VmonHystInit_TypeDef::fallThreshold

Falling threshold (mV).

Definition at line 884 of file em_emu.h.

Referenced by EMU_VmonHystInit().

bool EMU_VmonHystInit_TypeDef::fallWakeup

Wake up from EM4H on falling edge.

Definition at line 886 of file em_emu.h.

Referenced by EMU_VmonHystInit().

int EMU_VmonHystInit_TypeDef::riseThreshold

Rising threshold (mV).

Definition at line 883 of file em_emu.h.

Referenced by EMU_VmonHystInit().

bool EMU_VmonHystInit_TypeDef::riseWakeup

Wake up from EM4H on rising edge.

Definition at line 885 of file em_emu.h.

Referenced by EMU_VmonHystInit().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/em_emu.h