Detailed Description

Reset Management Unit (RMU) Peripheral API.

This module contains functions to control the RMU peripheral of Silicon Labs 32-bit MCUs and SoCs. RMU ensures correct reset operation and is responsible for connecting the different reset sources to the reset lines of the MCU or SoC.

Macros

#define RMU_LockupResetDisable (A) RMU_ResetControl ( rmuResetLockUp , A)

Enumerations

enum RMU_Reset_TypeDef {
rmuResetLockUp = _RMU_CTRL_LOCKUPRMODE_MASK,
rmuResetWdog = _RMU_CTRL_WDOGRMODE_MASK,
rmuResetCoreLockup = _RMU_CTRL_LOCKUPRMODE_MASK,
rmuResetSys = _RMU_CTRL_SYSRMODE_MASK,
rmuResetPin = _RMU_CTRL_PINRMODE_MASK
}
enum RMU_ResetMode_TypeDef {
rmuResetModeDisabled = _RMU_CTRL_PINRMODE_DISABLED,
rmuResetModeLimited = _RMU_CTRL_PINRMODE_LIMITED,
rmuResetModeExtended = _RMU_CTRL_PINRMODE_EXTENDED,
rmuResetModeFull = _RMU_CTRL_PINRMODE_FULL
}

Functions

void RMU_ResetCauseClear (void)
Clear the reset cause register.
uint32_t RMU_ResetCauseGet (void)
Get the cause of the last reset.
void RMU_ResetControl ( RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode)
Disable/enable reset for various peripherals and signal sources.
__STATIC_INLINE uint32_t RMU_UserResetStateGet (void)
Get user reset state. Reset only by a Power-on-reset and a pin reset.
__STATIC_INLINE void RMU_UserResetStateSet (uint32_t userState)
Set user reset state. Reset only by a Power-on-reset and a pin reset.

Macro Definition Documentation

#define RMU_LockupResetDisable ( A ) RMU_ResetControl ( rmuResetLockUp , A)

RMU_LockupResetDisable kept for backwards compatibility.

Definition at line 131 of file em_rmu.h .

Enumeration Type Documentation

RMU controlled peripheral reset control and reset source control.

Enumerator
rmuResetLockUp

Cortex lockup reset select.

rmuResetWdog

WDOG reset select.

rmuResetCoreLockup

Cortex lockup reset select.

rmuResetSys

SYSRESET select.

rmuResetPin

Pin reset select.

Definition at line 75 of file em_rmu.h .

RMU reset modes.

Definition at line 59 of file em_rmu.h .

Function Documentation

void RMU_ResetCauseClear ( void )

Clear the reset cause register.

This function clears all the reset cause bits of the RSTCAUSE register. The reset cause bits must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseGet() .

Definition at line 273 of file em_rmu.c .

References BUS_RegBitWrite() , EMU_Lock() , and EMU_Unlock() .

Referenced by SLEEP_Init() .

uint32_t RMU_ResetCauseGet ( void )

Get the cause of the last reset.

To be useful, the reset cause must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseClear() . This function call will return the main cause for reset, which can be a bit mask (several causes) and clear away "noise".

Returns
A reset cause mask. See the reference manual for a description of the reset cause mask.

Definition at line 316 of file em_rmu.c .

Referenced by SLEEP_Init() .

void RMU_ResetControl ( RMU_Reset_TypeDef reset,
RMU_ResetMode_TypeDef mode
)

Disable/enable reset for various peripherals and signal sources.

Parameters
[in] reset Reset types to enable/disable.s
[in] mode Reset mode.

Definition at line 245 of file em_rmu.c .

References BUS_RegBitWrite() , and SL_CTZ() .

__STATIC_INLINE uint32_t RMU_UserResetStateGet ( void )

Get user reset state. Reset only by a Power-on-reset and a pin reset.

Returns
Reset surviving user state.

Definition at line 159 of file em_rmu.h .

__STATIC_INLINE void RMU_UserResetStateSet ( uint32_t userState )

Set user reset state. Reset only by a Power-on-reset and a pin reset.

Parameters
[in] userState User state to set

Definition at line 144 of file em_rmu.h .