Data Structures

struct  sl_slist_node
 

Macros

#define container_of(ptr, type, member)   (type *)((uintptr_t)(ptr) - ((uintptr_t)(&((type *)0)->member)))
 
#define SL_SLIST_ENTRY   container_of
 
#define SL_SLIST_FOR_EACH(list_head, iterator)    for ((iterator) = (list_head); (iterator) != NULL; (iterator) = (iterator)->node)
 
#define SL_SLIST_FOR_EACH_ENTRY(list_head, entry, type, member)
 

Typedefs

typedef struct sl_slist_node sl_slist_node_t
 

Functions

void sl_slist_init (sl_slist_node_t **head)
 
void sl_slist_insert (sl_slist_node_t *item, sl_slist_node_t *pos)
 
sl_slist_node_tsl_slist_pop (sl_slist_node_t **head)
 
void sl_slist_push (sl_slist_node_t **head, sl_slist_node_t *item)
 
void sl_slist_push_back (sl_slist_node_t **head, sl_slist_node_t *item)
 
void sl_slist_remove (sl_slist_node_t **head, sl_slist_node_t *item)
 
void sl_slist_sort (sl_slist_node_t **head, bool(*cmp_fnct)(sl_slist_node_t *item_l, sl_slist_node_t *item_r))
 

Macro Definition Documentation

#define SL_SLIST_FOR_EACH_ENTRY (   list_head,
  entry,
  type,
  member 
)
Value:
for ( (entry) = SL_SLIST_ENTRY(list_head, type, member); \
&((entry)->member) != NULL; \
(entry) = SL_SLIST_ENTRY((entry)->member.node, type, member))

Definition at line 54 of file sl_slist.h.

Function Documentation

void sl_slist_init ( sl_slist_node_t **  head)

Initializes a singly-linked list.

Parameters
headPointer to pointer of head element of list.

Initializes a singly-linked list.

Definition at line 32 of file sl_slist.c.

void sl_slist_insert ( sl_slist_node_t item,
sl_slist_node_t pos 
)

Insert item after given item.

Parameters
itemPointer to item to add.
posPointer to item after which the item to add will be inserted.

Insert item after given item.

Definition at line 85 of file sl_slist.c.

sl_slist_node_t* sl_slist_pop ( sl_slist_node_t **  head)

Removes and returns first element of list.

Parameters
headPointer to pointer of head element of list.
Returns
Pointer to item that was at top of the list.

Removes and returns first element of list.

Definition at line 66 of file sl_slist.c.

void sl_slist_push ( sl_slist_node_t **  head,
sl_slist_node_t item 
)

Add given item at beginning of list.

Parameters
headPointer to pointer of head element of list.
itemPointer to item to add.

Add given item at beginning of list.

Definition at line 40 of file sl_slist.c.

void sl_slist_push_back ( sl_slist_node_t **  head,
sl_slist_node_t item 
)

Add item at end of list.

Parameters
headPointer to pointer of head element of list.
itemPointer to item to add.

Add item at end of list.

Definition at line 50 of file sl_slist.c.

void sl_slist_remove ( sl_slist_node_t **  head,
sl_slist_node_t item 
)

Remove item from list.

Parameters
headPointer to pointer of head element of list.
itemPointer to item to remove.
Note
(1) An EFM_ASSERT is thrown if the item is not found within the list.

Remove item from list.

Definition at line 95 of file sl_slist.c.

void sl_slist_sort ( sl_slist_node_t **  head,
bool(*)(sl_slist_node_t *item_l, sl_slist_node_t *item_r)  cmp_fnct 
)

Sorts list items.

Parameters
headPointer to pointer of head element of list.
cmp_fnctPointer to function to use for sorting the list. item_l Pointer to left item. item_r Pointer to right item. Returns whether the two items are ordered (true) or not (false).

Sorts list items.

Definition at line 113 of file sl_slist.c.