OPAMP

Detailed Description

Operational Amplifier (OPAMP) peripheral API.

This module contains functions to:

All OPAMP functions assume that the VDAC clock is running. If VDAC is not used, the clock can be turned off when the OPAMPs are configured.

If the available gain values don't suit the application at hand, the resistor ladders can be disabled and external gain programming resistors used.

A number of predefined OPAMP setup macros are available for configuration of the most common OPAMP topologies (see figures below).

Note
The terms POSPAD and NEGPAD in the figures are used to indicate that these pads should be connected to a suitable signal ground.


Unity gain voltage follower.
Use predefined macro OPA_INIT_UNITY_GAIN .

                    |\
         ___________|+\
                    |  \_______
                 ___|_ /    |
                |   | /     |
                |   |/      |
                |___________|


Non-inverting amplifier.
Use predefined macro OPA_INIT_NON_INVERTING .

                    |\
         ___________|+\
                    |  \_______
                 ___|_ /    |
                |   | /     |
                |   |/      |
                |_____R2____|
                |
                R1
                |
              NEGPAD 


Inverting amplifier.
Use predefined macro OPA_INIT_INVERTING .

                 _____R2____
                |           |
                |   |\      |
         ____R1_|___|_\     |
                    |  \____|___
                 ___|  /
                |   |+/
                |   |/
                |
              POSPAD 


Cascaded non-inverting amplifiers.
Use predefined macros OPA_INIT_CASCADED_NON_INVERTING_OPA0 , OPA_INIT_CASCADED_NON_INVERTING_OPA1 and OPA_INIT_CASCADED_NON_INVERTING_OPA2 .

                    |\                       |\                       |\
         ___________|+\ OPA0      ___________|+\ OPA1      ___________|+\ OPA2
                    |  \_________|           |  \_________|           |  \_______
                 ___|_ /    |             ___|_ /    |             ___|_ /    |
                |   | /     |            |   | /     |            |   | /     |
                |   |/      |            |   |/      |            |   |/      |
                |_____R2____|            |_____R2____|            |_____R2____|
                |                        |                        |
                R1                       R1                       R1
                |                        |                        |
              NEGPAD                   NEGPAD                   NEGPAD 


Cascaded inverting amplifiers.
Use predefined macros OPA_INIT_CASCADED_INVERTING_OPA0 , OPA_INIT_CASCADED_INVERTING_OPA1 and OPA_INIT_CASCADED_INVERTING_OPA2 .

                 _____R2____              _____R2____              _____R2____
                |           |            |           |            |           |
                |   |\      |            |   |\      |            |   |\      |
         ____R1_|___|_\     |     ____R1_|___|_\     |     ____R1_|___|_\     |
                    |  \____|____|           |  \____|___|            |  \____|__
                 ___|  /                  ___|  /                  ___|  /
                |   |+/ OPA0             |   |+/ OPA1             |   |+/ OPA2
                |   |/                   |   |/                   |   |/
                |                        |                        |
              POSPAD                   POSPAD                   POSPAD 


Differential driver with two opamp's.
Use predefined macros OPA_INIT_DIFF_DRIVER_OPA0 and OPA_INIT_DIFF_DRIVER_OPA1 .

                                  __________________________
                                 |                          +
                                 |        _____R2____
                    |\           |       |           |
         ___________|+\ OPA0     |       |   |\ OPA1 |
                    |  \_________|____R1_|___|_\     |      _
                 ___|_ /         |           |  \____|______
                |   | /          |        ___|  /
                |   |/           |       |   |+/
                |________________|       |   |/
                                         |
                                       POSPAD 


Differential receiver with three opamp's.
Use predefined macros OPA_INIT_DIFF_RECEIVER_OPA0 , OPA_INIT_DIFF_RECEIVER_OPA1 and OPA_INIT_DIFF_RECEIVER_OPA2 .

                    |\
          __________|+\ OPA1
         _          |  \_________
                 ___|_ /    |    |        _____R2____
                |   | /     |    |       |           |
                |   |/      |    |       |   |\      |
                |___________|    |____R1_|___|_\     |
                                             |  \____|___
                    |\            ____R1_ ___|  /
         +__________|+\ OPA0     |       |   |+/ OPA2
                    |  \_________|       |   |/
                 ___|_ /    |            R2
                |   | /     |            |
                |   |/      |          NEGPAD OPA0
                |___________|


Instrumentation amplifier.
Use predefined macros OPA_INIT_INSTR_AMP_OPA0 and OPA_INIT_INSTR_AMP_OPA1 .

                    |\
          __________|+\ OPA1
                    |  \______________
                 ___|_ /     |
                |   | /      |
                |   |/       R2
                |____________|
                             |
                             R1
                             |
                             R1
                 ____________|
                |            |
                |            R2
                |   |\       |
                |___|+\ OPA0 |
                    |  \_____|________
          __________|_ /
                    | /
                    |/

Data Structures

struct OPAMP_Init_TypeDef

Macros

#define OPA_INIT_CASCADED_INVERTING_OPA0
#define OPA_INIT_CASCADED_INVERTING_OPA1
#define OPA_INIT_CASCADED_INVERTING_OPA2
#define OPA_INIT_CASCADED_INVERTING_OPA3
#define OPA_INIT_CASCADED_NON_INVERTING_OPA0
#define OPA_INIT_CASCADED_NON_INVERTING_OPA1
#define OPA_INIT_CASCADED_NON_INVERTING_OPA2
#define OPA_INIT_CASCADED_NON_INVERTING_OPA3
#define OPA_INIT_DIFF_DRIVER_OPA0
#define OPA_INIT_DIFF_DRIVER_OPA1
#define OPA_INIT_DIFF_RECEIVER_OPA0
#define OPA_INIT_DIFF_RECEIVER_OPA1
#define OPA_INIT_DIFF_RECEIVER_OPA2
#define OPA_INIT_DIFF_RECEIVER_OPA3
#define OPA_INIT_INSTR_AMP_OPA0
#define OPA_INIT_INSTR_AMP_OPA1
#define OPA_INIT_INVERTING
#define OPA_INIT_NON_INVERTING
#define OPA_INIT_UNITY_GAIN

Enumerations

enum OPAMP_DrvStr_Typedef {
opaDrvStrDefault = VDAC_OPA_CTRL_DRIVESTRENGTH_DEFAULT,
opaDrvStrLowerAccLowStr = (0 << _VDAC_OPA_CTRL_DRIVESTRENGTH_SHIFT),
opaDrvStrLowAccLowStr = (1 << _VDAC_OPA_CTRL_DRIVESTRENGTH_SHIFT),
opaDrvStrHighAccHighStr = (2 << _VDAC_OPA_CTRL_DRIVESTRENGTH_SHIFT),
opaDrvStrHigherAccHighStr = (3 << _VDAC_OPA_CTRL_DRIVESTRENGTH_SHIFT)
}
enum OPAMP_NegSel_TypeDef {
opaNegSelAPORT1YCH1 = VDAC_OPA_MUX_NEGSEL_APORT1YCH1,
opaNegSelAPORT1YCH3 = VDAC_OPA_MUX_NEGSEL_APORT1YCH3,
opaNegSelAPORT1YCH5 = VDAC_OPA_MUX_NEGSEL_APORT1YCH5,
opaNegSelAPORT1YCH7 = VDAC_OPA_MUX_NEGSEL_APORT1YCH7,
opaNegSelAPORT1YCH9 = VDAC_OPA_MUX_NEGSEL_APORT1YCH9,
opaNegSelAPORT1YCH11 = VDAC_OPA_MUX_NEGSEL_APORT1YCH11,
opaNegSelAPORT1YCH13 = VDAC_OPA_MUX_NEGSEL_APORT1YCH13,
opaNegSelAPORT1YCH15 = VDAC_OPA_MUX_NEGSEL_APORT1YCH15,
opaNegSelAPORT1YCH17 = VDAC_OPA_MUX_NEGSEL_APORT1YCH17,
opaNegSelAPORT1YCH19 = VDAC_OPA_MUX_NEGSEL_APORT1YCH19,
opaNegSelAPORT1YCH21 = VDAC_OPA_MUX_NEGSEL_APORT1YCH21,
opaNegSelAPORT1YCH23 = VDAC_OPA_MUX_NEGSEL_APORT1YCH23,
opaNegSelAPORT1YCH25 = VDAC_OPA_MUX_NEGSEL_APORT1YCH25,
opaNegSelAPORT1YCH27 = VDAC_OPA_MUX_NEGSEL_APORT1YCH27,
opaNegSelAPORT1YCH29 = VDAC_OPA_MUX_NEGSEL_APORT1YCH29,
opaNegSelAPORT1YCH31 = VDAC_OPA_MUX_NEGSEL_APORT1YCH31,
opaNegSelAPORT2YCH0 = VDAC_OPA_MUX_NEGSEL_APORT2YCH0,
opaNegSelAPORT2YCH2 = VDAC_OPA_MUX_NEGSEL_APORT2YCH2,
opaNegSelAPORT2YCH4 = VDAC_OPA_MUX_NEGSEL_APORT2YCH4,
opaNegSelAPORT2YCH6 = VDAC_OPA_MUX_NEGSEL_APORT2YCH6,
opaNegSelAPORT2YCH8 = VDAC_OPA_MUX_NEGSEL_APORT2YCH8,
opaNegSelAPORT2YCH10 = VDAC_OPA_MUX_NEGSEL_APORT2YCH10,
opaNegSelAPORT2YCH12 = VDAC_OPA_MUX_NEGSEL_APORT2YCH12,
opaNegSelAPORT2YCH14 = VDAC_OPA_MUX_NEGSEL_APORT2YCH14,
opaNegSelAPORT2YCH16 = VDAC_OPA_MUX_NEGSEL_APORT2YCH16,
opaNegSelAPORT2YCH18 = VDAC_OPA_MUX_NEGSEL_APORT2YCH18,
opaNegSelAPORT2YCH20 = VDAC_OPA_MUX_NEGSEL_APORT2YCH20,
opaNegSelAPORT2YCH22 = VDAC_OPA_MUX_NEGSEL_APORT2YCH22,
opaNegSelAPORT2YCH24 = VDAC_OPA_MUX_NEGSEL_APORT2YCH24,
opaNegSelAPORT2YCH26 = VDAC_OPA_MUX_NEGSEL_APORT2YCH26,
opaNegSelAPORT2YCH28 = VDAC_OPA_MUX_NEGSEL_APORT2YCH28,
opaNegSelAPORT2YCH30 = VDAC_OPA_MUX_NEGSEL_APORT2YCH30,
opaNegSelAPORT3YCH1 = VDAC_OPA_MUX_NEGSEL_APORT3YCH1,
opaNegSelAPORT3YCH3 = VDAC_OPA_MUX_NEGSEL_APORT3YCH3,
opaNegSelAPORT3YCH5 = VDAC_OPA_MUX_NEGSEL_APORT3YCH5,
opaNegSelAPORT3YCH7 = VDAC_OPA_MUX_NEGSEL_APORT3YCH7,
opaNegSelAPORT3YCH9 = VDAC_OPA_MUX_NEGSEL_APORT3YCH9,
opaNegSelAPORT3YCH11 = VDAC_OPA_MUX_NEGSEL_APORT3YCH11,
opaNegSelAPORT3YCH13 = VDAC_OPA_MUX_NEGSEL_APORT3YCH13,
opaNegSelAPORT3YCH15 = VDAC_OPA_MUX_NEGSEL_APORT3YCH15,
opaNegSelAPORT3YCH17 = VDAC_OPA_MUX_NEGSEL_APORT3YCH17,
opaNegSelAPORT3YCH19 = VDAC_OPA_MUX_NEGSEL_APORT3YCH19,
opaNegSelAPORT3YCH21 = VDAC_OPA_MUX_NEGSEL_APORT3YCH21,
opaNegSelAPORT3YCH23 = VDAC_OPA_MUX_NEGSEL_APORT3YCH23,
opaNegSelAPORT3YCH25 = VDAC_OPA_MUX_NEGSEL_APORT3YCH25,
opaNegSelAPORT3YCH27 = VDAC_OPA_MUX_NEGSEL_APORT3YCH27,
opaNegSelAPORT3YCH29 = VDAC_OPA_MUX_NEGSEL_APORT3YCH29,
opaNegSelAPORT3YCH31 = VDAC_OPA_MUX_NEGSEL_APORT3YCH31,
opaNegSelAPORT4YCH0 = VDAC_OPA_MUX_NEGSEL_APORT4YCH0,
opaNegSelAPORT4YCH2 = VDAC_OPA_MUX_NEGSEL_APORT4YCH2,
opaNegSelAPORT4YCH4 = VDAC_OPA_MUX_NEGSEL_APORT4YCH4,
opaNegSelAPORT4YCH6 = VDAC_OPA_MUX_NEGSEL_APORT4YCH6,
opaNegSelAPORT4YCH8 = VDAC_OPA_MUX_NEGSEL_APORT4YCH8,
opaNegSelAPORT4YCH10 = VDAC_OPA_MUX_NEGSEL_APORT4YCH10,
opaNegSelAPORT4YCH12 = VDAC_OPA_MUX_NEGSEL_APORT4YCH12,
opaNegSelAPORT4YCH14 = VDAC_OPA_MUX_NEGSEL_APORT4YCH14,
opaNegSelAPORT4YCH16 = VDAC_OPA_MUX_NEGSEL_APORT4YCH16,
opaNegSelAPORT4YCH18 = VDAC_OPA_MUX_NEGSEL_APORT4YCH18,
opaNegSelAPORT4YCH20 = VDAC_OPA_MUX_NEGSEL_APORT4YCH20,
opaNegSelAPORT4YCH22 = VDAC_OPA_MUX_NEGSEL_APORT4YCH22,
opaNegSelAPORT4YCH24 = VDAC_OPA_MUX_NEGSEL_APORT4YCH24,
opaNegSelAPORT4YCH26 = VDAC_OPA_MUX_NEGSEL_APORT4YCH26,
opaNegSelAPORT4YCH28 = VDAC_OPA_MUX_NEGSEL_APORT4YCH28,
opaNegSelAPORT4YCH30 = VDAC_OPA_MUX_NEGSEL_APORT4YCH30,
opaNegSelDisable = VDAC_OPA_MUX_NEGSEL_DISABLE,
opaNegSelUnityGain = VDAC_OPA_MUX_NEGSEL_UG,
opaNegSelResTap = VDAC_OPA_MUX_NEGSEL_OPATAP,
opaNegSelNegPad = VDAC_OPA_MUX_NEGSEL_NEGPAD
}
enum OPAMP_OutMode_TypeDef {
opaOutModeDisable = 0,
opaOutModeMain = VDAC_OPA_OUT_MAINOUTEN,
opaOutModeAlt = VDAC_OPA_OUT_ALTOUTEN,
opaOutModeAll = VDAC_OPA_OUT_SHORT,
opaOutModeAPORT1YCH1 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH1),
opaOutModeAPORT1YCH3 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH3),
opaOutModeAPORT1YCH5 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH5),
opaOutModeAPORT1YCH7 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH7),
opaOutModeAPORT1YCH9 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH9),
opaOutModeAPORT1YCH11 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH11),
opaOutModeAPORT1YCH13 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH13),
opaOutModeAPORT1YCH15 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH15),
opaOutModeAPORT1YCH17 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH17),
opaOutModeAPORT1YCH19 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH19),
opaOutModeAPORT1YCH21 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH21),
opaOutModeAPORT1YCH23 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH23),
opaOutModeAPORT1YCH25 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH25),
opaOutModeAPORT1YCH27 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH27),
opaOutModeAPORT1YCH29 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH29),
opaOutModeAPORT1YCH31 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT1YCH31),
opaOutModeAPORT2YCH0 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH0),
opaOutModeAPORT2YCH2 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH2),
opaOutModeAPORT2YCH4 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH4),
opaOutModeAPORT2YCH6 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH6),
opaOutModeAPORT2YCH8 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH8),
opaOutModeAPORT2YCH10 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH10),
opaOutModeAPORT2YCH12 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH12),
opaOutModeAPORT2YCH14 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH14),
opaOutModeAPORT2YCH16 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH16),
opaOutModeAPORT2YCH18 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH18),
opaOutModeAPORT2YCH20 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH20),
opaOutModeAPORT2YCH22 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH22),
opaOutModeAPORT2YCH24 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH24),
opaOutModeAPORT2YCH26 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH26),
opaOutModeAPORT2YCH28 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH28),
opaOutModeAPORT2YCH30 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT2YCH30),
opaOutModeAPORT3YCH1 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH1),
opaOutModeAPORT3YCH3 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH3),
opaOutModeAPORT3YCH5 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH5),
opaOutModeAPORT3YCH7 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH7),
opaOutModeAPORT3YCH9 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH9),
opaOutModeAPORT3YCH11 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH11),
opaOutModeAPORT3YCH13 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH13),
opaOutModeAPORT3YCH15 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH15),
opaOutModeAPORT3YCH17 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH17),
opaOutModeAPORT3YCH19 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH19),
opaOutModeAPORT3YCH21 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH21),
opaOutModeAPORT3YCH23 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH23),
opaOutModeAPORT3YCH25 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH25),
opaOutModeAPORT3YCH27 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH27),
opaOutModeAPORT3YCH29 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH29),
opaOutModeAPORT3YCH31 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT3YCH31),
opaOutModeAPORT4YCH0 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH0),
opaOutModeAPORT4YCH2 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH2),
opaOutModeAPORT4YCH4 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH4),
opaOutModeAPORT4YCH6 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH6),
opaOutModeAPORT4YCH8 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH8),
opaOutModeAPORT4YCH10 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH10),
opaOutModeAPORT4YCH12 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH12),
opaOutModeAPORT4YCH14 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH14),
opaOutModeAPORT4YCH16 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH16),
opaOutModeAPORT4YCH18 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH18),
opaOutModeAPORT4YCH20 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH20),
opaOutModeAPORT4YCH22 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH22),
opaOutModeAPORT4YCH24 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH24),
opaOutModeAPORT4YCH26 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH26),
opaOutModeAPORT4YCH28 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH28),
opaOutModeAPORT4YCH30 = (VDAC_OPA_OUT_APORTOUTEN | VDAC_OPA_OUT_APORTOUTSEL_APORT4YCH30)
}
enum OPAMP_OutScale_Typedef {
opaOutScaleDefault = VDAC_OPA_CTRL_OUTSCALE_DEFAULT,
opaOutScaleFull = VDAC_OPA_CTRL_OUTSCALE_FULL,
opaOutSacleHalf = VDAC_OPA_CTRL_OUTSCALE_HALF
}
enum OPAMP_PosSel_TypeDef {
opaPosSelAPORT1XCH0 = VDAC_OPA_MUX_POSSEL_APORT1XCH0,
opaPosSelAPORT1XCH2 = VDAC_OPA_MUX_POSSEL_APORT1XCH2,
opaPosSelAPORT1XCH4 = VDAC_OPA_MUX_POSSEL_APORT1XCH4,
opaPosSelAPORT1XCH6 = VDAC_OPA_MUX_POSSEL_APORT1XCH6,
opaPosSelAPORT1XCH8 = VDAC_OPA_MUX_POSSEL_APORT1XCH8,
opaPosSelAPORT1XCH10 = VDAC_OPA_MUX_POSSEL_APORT1XCH10,
opaPosSelAPORT1XCH12 = VDAC_OPA_MUX_POSSEL_APORT1XCH12,
opaPosSelAPORT1XCH14 = VDAC_OPA_MUX_POSSEL_APORT1XCH14,
opaPosSelAPORT1XCH16 = VDAC_OPA_MUX_POSSEL_APORT1XCH16,
opaPosSelAPORT1XCH18 = VDAC_OPA_MUX_POSSEL_APORT1XCH18,
opaPosSelAPORT1XCH20 = VDAC_OPA_MUX_POSSEL_APORT1XCH20,
opaPosSelAPORT1XCH22 = VDAC_OPA_MUX_POSSEL_APORT1XCH22,
opaPosSelAPORT1XCH24 = VDAC_OPA_MUX_POSSEL_APORT1XCH24,
opaPosSelAPORT1XCH26 = VDAC_OPA_MUX_POSSEL_APORT1XCH26,
opaPosSelAPORT1XCH28 = VDAC_OPA_MUX_POSSEL_APORT1XCH28,
opaPosSelAPORT1XCH30 = VDAC_OPA_MUX_POSSEL_APORT1XCH30,
opaPosSelAPORT2XCH1 = VDAC_OPA_MUX_POSSEL_APORT2XCH1,
opaPosSelAPORT2XCH3 = VDAC_OPA_MUX_POSSEL_APORT2XCH3,
opaPosSelAPORT2XCH5 = VDAC_OPA_MUX_POSSEL_APORT2XCH5,
opaPosSelAPORT2XCH7 = VDAC_OPA_MUX_POSSEL_APORT2XCH7,
opaPosSelAPORT2XCH9 = VDAC_OPA_MUX_POSSEL_APORT2XCH9,
opaPosSelAPORT2XCH11 = VDAC_OPA_MUX_POSSEL_APORT2XCH11,
opaPosSelAPORT2XCH13 = VDAC_OPA_MUX_POSSEL_APORT2XCH13,
opaPosSelAPORT2XCH15 = VDAC_OPA_MUX_POSSEL_APORT2XCH15,
opaPosSelAPORT2XCH17 = VDAC_OPA_MUX_POSSEL_APORT2XCH17,
opaPosSelAPORT2XCH19 = VDAC_OPA_MUX_POSSEL_APORT2XCH19,
opaPosSelAPORT2XCH21 = VDAC_OPA_MUX_POSSEL_APORT2XCH21,
opaPosSelAPORT2XCH23 = VDAC_OPA_MUX_POSSEL_APORT2XCH23,
opaPosSelAPORT2XCH25 = VDAC_OPA_MUX_POSSEL_APORT2XCH25,
opaPosSelAPORT2XCH27 = VDAC_OPA_MUX_POSSEL_APORT2XCH27,
opaPosSelAPORT2XCH29 = VDAC_OPA_MUX_POSSEL_APORT2XCH29,
opaPosSelAPORT2XCH31 = VDAC_OPA_MUX_POSSEL_APORT2XCH31,
opaPosSelAPORT3XCH0 = VDAC_OPA_MUX_POSSEL_APORT3XCH0,
opaPosSelAPORT3XCH2 = VDAC_OPA_MUX_POSSEL_APORT3XCH2,
opaPosSelAPORT3XCH4 = VDAC_OPA_MUX_POSSEL_APORT3XCH4,
opaPosSelAPORT3XCH6 = VDAC_OPA_MUX_POSSEL_APORT3XCH6,
opaPosSelAPORT3XCH8 = VDAC_OPA_MUX_POSSEL_APORT3XCH8,
opaPosSelAPORT3XCH10 = VDAC_OPA_MUX_POSSEL_APORT3XCH10,
opaPosSelAPORT3XCH12 = VDAC_OPA_MUX_POSSEL_APORT3XCH12,
opaPosSelAPORT3XCH14 = VDAC_OPA_MUX_POSSEL_APORT3XCH14,
opaPosSelAPORT3XCH16 = VDAC_OPA_MUX_POSSEL_APORT3XCH16,
opaPosSelAPORT3XCH18 = VDAC_OPA_MUX_POSSEL_APORT3XCH18,
opaPosSelAPORT3XCH20 = VDAC_OPA_MUX_POSSEL_APORT3XCH20,
opaPosSelAPORT3XCH22 = VDAC_OPA_MUX_POSSEL_APORT3XCH22,
opaPosSelAPORT3XCH24 = VDAC_OPA_MUX_POSSEL_APORT3XCH24,
opaPosSelAPORT3XCH26 = VDAC_OPA_MUX_POSSEL_APORT3XCH26,
opaPosSelAPORT3XCH28 = VDAC_OPA_MUX_POSSEL_APORT3XCH28,
opaPosSelAPORT3XCH30 = VDAC_OPA_MUX_POSSEL_APORT3XCH30,
opaPosSelAPORT4XCH1 = VDAC_OPA_MUX_POSSEL_APORT4XCH1,
opaPosSelAPORT4XCH3 = VDAC_OPA_MUX_POSSEL_APORT4XCH3,
opaPosSelAPORT4XCH5 = VDAC_OPA_MUX_POSSEL_APORT4XCH5,
opaPosSelAPORT4XCH7 = VDAC_OPA_MUX_POSSEL_APORT4XCH7,
opaPosSelAPORT4XCH9 = VDAC_OPA_MUX_POSSEL_APORT4XCH9,
opaPosSelAPORT4XCH11 = VDAC_OPA_MUX_POSSEL_APORT4XCH11,
opaPosSelAPORT4XCH13 = VDAC_OPA_MUX_POSSEL_APORT4XCH13,
opaPosSelAPORT4XCH15 = VDAC_OPA_MUX_POSSEL_APORT4XCH15,
opaPosSelAPORT4XCH17 = VDAC_OPA_MUX_POSSEL_APORT4XCH17,
opaPosSelAPORT4XCH19 = VDAC_OPA_MUX_POSSEL_APORT4XCH19,
opaPosSelAPORT4XCH21 = VDAC_OPA_MUX_POSSEL_APORT4XCH21,
opaPosSelAPORT4XCH23 = VDAC_OPA_MUX_POSSEL_APORT4XCH23,
opaPosSelAPORT4XCH25 = VDAC_OPA_MUX_POSSEL_APORT4XCH25,
opaPosSelAPORT4XCH27 = VDAC_OPA_MUX_POSSEL_APORT4XCH27,
opaPosSelAPORT4XCH29 = VDAC_OPA_MUX_POSSEL_APORT4XCH29,
opaPosSelAPORT4XCH31 = VDAC_OPA_MUX_POSSEL_APORT4XCH31,
opaPosSelDisable = VDAC_OPA_MUX_POSSEL_DISABLE,
opaPosSelDac = VDAC_OPA_MUX_POSSEL_DAC,
opaPosSelPosPad = VDAC_OPA_MUX_POSSEL_POSPAD,
opaPosSelOpaIn = VDAC_OPA_MUX_POSSEL_OPANEXT,
opaPosSelResTap = VDAC_OPA_MUX_POSSEL_OPATAP
}
enum OPAMP_PrsMode_TypeDef {
opaPrsModeDefault = VDAC_OPA_CTRL_PRSMODE_DEFAULT,
opaPrsModePulsed = VDAC_OPA_CTRL_PRSMODE_PULSED,
opaPrsModeTimed = VDAC_OPA_CTRL_PRSMODE_TIMED
}
enum OPAMP_PrsOut_TypeDef {
opaPrsOutDefault = VDAC_OPA_CTRL_PRSOUTMODE_DEFAULT,
opaPrsOutWarm = VDAC_OPA_CTRL_PRSOUTMODE_WARM,
opaPrsOutOutValid = VDAC_OPA_CTRL_PRSOUTMODE_OUTVALID
}
enum OPAMP_PrsSel_TypeDef {
opaPrsSelDefault = VDAC_OPA_CTRL_PRSSEL_DEFAULT,
opaPrsSelCh0 = VDAC_OPA_CTRL_PRSSEL_PRSCH0,
opaPrsSelCh1 = VDAC_OPA_CTRL_PRSSEL_PRSCH1,
opaPrsSelCh2 = VDAC_OPA_CTRL_PRSSEL_PRSCH2,
opaPrsSelCh3 = VDAC_OPA_CTRL_PRSSEL_PRSCH3,
opaPrsSelCh4 = VDAC_OPA_CTRL_PRSSEL_PRSCH4,
opaPrsSelCh5 = VDAC_OPA_CTRL_PRSSEL_PRSCH5,
opaPrsSelCh6 = VDAC_OPA_CTRL_PRSSEL_PRSCH6,
opaPrsSelCh7 = VDAC_OPA_CTRL_PRSSEL_PRSCH7,
opaPrsSelCh8 = VDAC_OPA_CTRL_PRSSEL_PRSCH8,
opaPrsSelCh9 = VDAC_OPA_CTRL_PRSSEL_PRSCH9,
opaPrsSelCh10 = VDAC_OPA_CTRL_PRSSEL_PRSCH10,
opaPrsSelCh11 = VDAC_OPA_CTRL_PRSSEL_PRSCH11
}
enum OPAMP_ResInMux_TypeDef {
opaResInMuxDisable = VDAC_OPA_MUX_RESINMUX_DISABLE,
opaResInMuxOpaIn = VDAC_OPA_MUX_RESINMUX_OPANEXT,
opaResInMuxNegPad = VDAC_OPA_MUX_RESINMUX_NEGPAD,
opaResInMuxPosPad = VDAC_OPA_MUX_RESINMUX_POSPAD,
opaResInMuxComPad = VDAC_OPA_MUX_RESINMUX_COMPAD,
opaResInMuxCenter = VDAC_OPA_MUX_RESINMUX_CENTER,
opaResInMuxVss = VDAC_OPA_MUX_RESINMUX_VSS
}
enum OPAMP_ResSel_TypeDef {
opaResSelDefault = VDAC_OPA_MUX_RESSEL_DEFAULT,
opaResSelR2eq0_33R1 = VDAC_OPA_MUX_RESSEL_RES0,
opaResSelR2eqR1 = VDAC_OPA_MUX_RESSEL_RES1,
opaResSelR1eq1_67R1 = VDAC_OPA_MUX_RESSEL_RES2,
opaResSelR2eq2_2R1 = VDAC_OPA_MUX_RESSEL_RES3,
opaResSelR2eq3R1 = VDAC_OPA_MUX_RESSEL_RES4,
opaResSelR2eq4_33R1 = VDAC_OPA_MUX_RESSEL_RES5,
opaResSelR2eq7R1 = VDAC_OPA_MUX_RESSEL_RES6,
opaResSelR2eq15R1 = VDAC_OPA_MUX_RESSEL_RES7
}
enum OPAMP_TypeDef {
OPA0 = 0,
OPA1 = 1
}

Functions

void OPAMP_Disable (VDAC_TypeDef *dac, OPAMP_TypeDef opa)
Disable an Operational Amplifier.
void OPAMP_Enable (VDAC_TypeDef *dac, OPAMP_TypeDef opa, const OPAMP_Init_TypeDef *init)
Configure and enable an Operational Amplifier.

Macro Definition Documentation

#define OPA_INIT_CASCADED_INVERTING_OPA0
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxNegPad, /* Resistor ladder input from negative pad. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA0 in cascaded inverting amplifier mode.

Definition at line 1101 of file em_opamp.h .

#define OPA_INIT_CASCADED_INVERTING_OPA1
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxOpaIn, /* Resistor ladder input from OPA0. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA1 in cascaded inverting amplifier mode.

Definition at line 1129 of file em_opamp.h .

#define OPA_INIT_CASCADED_INVERTING_OPA2
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxOpaIn, /* Resistor ladder input from OPA1. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA2 in cascaded inverting amplifier mode.

Definition at line 1157 of file em_opamp.h .

#define OPA_INIT_CASCADED_INVERTING_OPA3
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxOpaIn, /* Resistor ladder input from OPA2. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA3 in cascaded inverting amplifier mode.

Definition at line 1185 of file em_opamp.h .

#define OPA_INIT_CASCADED_NON_INVERTING_OPA0
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eq0_33R1, /* R2 = 1/3 R1 */ \
opaResInMuxNegPad, /* Resistor ladder input from negative pad. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA0 in cascaded non-inverting amplifier mode.

Definition at line 989 of file em_opamp.h .

#define OPA_INIT_CASCADED_NON_INVERTING_OPA1
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelOpaIn, /* Positive input from OPA0 output. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eq0_33R1, /* R2 = 1/3 R1 */ \
opaResInMuxNegPad, /* Resistor ladder input from negative pad. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA1 in cascaded non-inverting amplifier mode.

Definition at line 1017 of file em_opamp.h .

#define OPA_INIT_CASCADED_NON_INVERTING_OPA2
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelOpaIn, /* Positive input from OPA1 output. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eq0_33R1, /* R2 = 1/3 R1 */ \
opaResInMuxNegPad, /* Resistor ladder input from negative pad. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA2 in cascaded non-inverting amplifier mode.

Definition at line 1045 of file em_opamp.h .

#define OPA_INIT_CASCADED_NON_INVERTING_OPA3
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelOpaIn, /* Positive input from OPA2NEXT output. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eq0_33R1, /* R2 = 1/3 R1 */ \
opaResInMuxNegPad, /* Resistor ladder input from negative pad. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA3 in cascaded non-inverting amplifier mode.

Definition at line 1073 of file em_opamp.h .

#define OPA_INIT_DIFF_DRIVER_OPA0
Value:
{ \
opaNegSelUnityGain, /* Unity gain. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelDefault, /* Resistor ladder is not used. */ \
opaResInMuxDisable, /* Resistor ladder disabled. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA0 in two-opamp differential driver mode.

Definition at line 1213 of file em_opamp.h .

#define OPA_INIT_DIFF_DRIVER_OPA1
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxOpaIn, /* Resistor ladder input from OPA0. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA1 in two-opamp differential driver mode.

Definition at line 1241 of file em_opamp.h .

#define OPA_INIT_DIFF_RECEIVER_OPA0
Value:
{ \
opaNegSelUnityGain, /* Unity gain. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxNegPad, /* Resistor ladder input from negative pad. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA0 in three-opamp differential receiver mode.

Definition at line 1269 of file em_opamp.h .

#define OPA_INIT_DIFF_RECEIVER_OPA1
Value:
{ \
opaNegSelUnityGain, /* Unity gain. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelDefault, /* Resistor ladder is not used. */ \
opaResInMuxDisable, /* Disable resistor ladder. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA1 in three-opamp differential receiver mode.

Definition at line 1297 of file em_opamp.h .

#define OPA_INIT_DIFF_RECEIVER_OPA2
Value:
{ \
opaNegSelResTap, /* Input from resistor ladder tap. */ \
opaPosSelResTap, /* Input from OPA0 resistor ladder tap. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxOpaIn, /* Resistor ladder input from OPA1. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA2 in three-opamp differential receiver mode.

Definition at line 1325 of file em_opamp.h .

#define OPA_INIT_DIFF_RECEIVER_OPA3
Value:
{ \
opaNegSelResTap, /* Input from resistor ladder tap. */ \
opaPosSelResTap, /* Input from OPA2 resistor ladder tap. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxOpaIn, /* Resistor ladder input from OPA2. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA3 in three+one opamp differential receiver mode. In this configuration, OPA3 is a second single-ended output amplifier.

Definition at line 1354 of file em_opamp.h .

#define OPA_INIT_INSTR_AMP_OPA0
Value:
{ \
opaNegSelResTap, /* Input from resistor ladder tap. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxCenter, /* OPA0/OPA1 resistor ladders connected. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA0 in two-opamp instrumentation amplifier mode.

Definition at line 1382 of file em_opamp.h .

#define OPA_INIT_INSTR_AMP_OPA1
Value:
{ \
opaNegSelNegPad, /* Negative input from pad. */ \
opaPosSelResTap, /* Input from resistor ladder tap. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxCenter, /* OPA0/OPA1 resistor ladders connected. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA1 in two-opamp instrumentation amplifier mode.

Definition at line 1410 of file em_opamp.h .

#define OPA_INIT_INVERTING
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eqR1, /* R2 = R1 */ \
opaResInMuxNegPad, /* Resistor ladder input from negative pad. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA in inverting amplifier mode.

Definition at line 961 of file em_opamp.h .

#define OPA_INIT_NON_INVERTING
Value:
{ \
opaNegSelResTap, /* Negative input from resistor ladder tap. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelR2eq0_33R1, /* R2 = 1/3 R1 */ \
opaResInMuxNegPad, /* Resistor ladder input from negative pad. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA in non-inverting amplifier mode.

Definition at line 933 of file em_opamp.h .

#define OPA_INIT_UNITY_GAIN
Value:
{ \
opaNegSelUnityGain, /* Unity gain. */ \
opaPosSelPosPad, /* Positive input from pad. */ \
opaOutModeMain, /* Main output enabled. */ \
opaResSelDefault, /* Resistor ladder is not used. */ \
opaResInMuxDisable, /* Resistor ladder disabled. */ \
0, /* No alternate outputs enabled. */ \
opaDrvStrDefault, /* Default opamp operation mode. */ \
false, /* Disable 3x gain setting. */ \
false, /* Use full output drive strength. */ \
false, /* Disable unity-gain bandwidth scaling. */ \
false, /* Opamp triggered by OPAxEN. */ \
opaPrsModeDefault, /* PRS is not used to trigger opamp. */ \
opaPrsSelDefault, /* PRS is not used to trigger opamp. */ \
opaPrsOutDefault, /* Default PRS output setting. */ \
false, /* Bus mastering enabled on APORTX. */ \
false, /* Bus mastering enabled on APORTY. */ \
3, /* 3 us settle time with default DrvStr. */ \
0, /* No startup delay. */ \
false, /* Rail-to-rail input enabled. */ \
true, /* Use calibrated inverting offset. */ \
0, /* Opamp offset value (not used). */ \
true, /* Use calibrated non-inverting offset. */ \
0 /* Opamp offset value (not used). */ \
}

Configuration of OPA in unity gain voltage follower mode.

Definition at line 905 of file em_opamp.h .

Enumeration Type Documentation

Enumerator
opaDrvStrDefault

Default value.

opaDrvStrLowerAccLowStr

Lower accuracy with low drive strength.

opaDrvStrLowAccLowStr

Low accuracy with low drive strength.

opaDrvStrHighAccHighStr

High accuracy with high drive strength.

opaDrvStrHigherAccHighStr

Higher accuracy with high drive strength.

Definition at line 426 of file em_opamp.h .

OPAMP negative terminal input selection values.

Enumerator
opaNegSelAPORT1YCH1

APORT1YCH1

opaNegSelAPORT1YCH3

APORT1YCH3

opaNegSelAPORT1YCH5

APORT1YCH5

opaNegSelAPORT1YCH7

APORT1YCH7

opaNegSelAPORT1YCH9

APORT1YCH9

opaNegSelAPORT1YCH11

APORT1YCH11

opaNegSelAPORT1YCH13

APORT1YCH13

opaNegSelAPORT1YCH15

APORT1YCH15

opaNegSelAPORT1YCH17

APORT1YCH17

opaNegSelAPORT1YCH19

APORT1YCH19

opaNegSelAPORT1YCH21

APORT1YCH21

opaNegSelAPORT1YCH23

APORT1YCH23

opaNegSelAPORT1YCH25

APORT1YCH25

opaNegSelAPORT1YCH27

APORT1YCH27

opaNegSelAPORT1YCH29

APORT1YCH29

opaNegSelAPORT1YCH31

APORT1YCH31

opaNegSelAPORT2YCH0

APORT2YCH0

opaNegSelAPORT2YCH2

APORT2YCH2

opaNegSelAPORT2YCH4

APORT2YCH4

opaNegSelAPORT2YCH6

APORT2YCH6

opaNegSelAPORT2YCH8

APORT2YCH8

opaNegSelAPORT2YCH10

APORT2YCH10

opaNegSelAPORT2YCH12

APORT2YCH12

opaNegSelAPORT2YCH14

APORT2YCH14

opaNegSelAPORT2YCH16

APORT2YCH16

opaNegSelAPORT2YCH18

APORT2YCH18

opaNegSelAPORT2YCH20

APORT2YCH20

opaNegSelAPORT2YCH22

APORT2YCH22

opaNegSelAPORT2YCH24

APORT2YCH24

opaNegSelAPORT2YCH26

APORT2YCH26

opaNegSelAPORT2YCH28

APORT2YCH28

opaNegSelAPORT2YCH30

APORT2YCH30

opaNegSelAPORT3YCH1

APORT3YCH1

opaNegSelAPORT3YCH3

APORT3YCH3

opaNegSelAPORT3YCH5

APORT3YCH5

opaNegSelAPORT3YCH7

APORT3YCH7

opaNegSelAPORT3YCH9

APORT3YCH9

opaNegSelAPORT3YCH11

APORT3YCH11

opaNegSelAPORT3YCH13

APORT3YCH13

opaNegSelAPORT3YCH15

APORT3YCH15

opaNegSelAPORT3YCH17

APORT3YCH17

opaNegSelAPORT3YCH19

APORT3YCH19

opaNegSelAPORT3YCH21

APORT3YCH21

opaNegSelAPORT3YCH23

APORT3YCH23

opaNegSelAPORT3YCH25

APORT3YCH25

opaNegSelAPORT3YCH27

APORT3YCH27

opaNegSelAPORT3YCH29

APORT3YCH29

opaNegSelAPORT3YCH31

APORT3YCH31

opaNegSelAPORT4YCH0

APORT4YCH0

opaNegSelAPORT4YCH2

APORT4YCH2

opaNegSelAPORT4YCH4

APORT4YCH4

opaNegSelAPORT4YCH6

APORT4YCH6

opaNegSelAPORT4YCH8

APORT4YCH8

opaNegSelAPORT4YCH10

APORT4YCH10

opaNegSelAPORT4YCH12

APORT4YCH12

opaNegSelAPORT4YCH14

APORT4YCH14

opaNegSelAPORT4YCH16

APORT4YCH16

opaNegSelAPORT4YCH18

APORT4YCH18

opaNegSelAPORT4YCH20

APORT4YCH20

opaNegSelAPORT4YCH22

APORT4YCH22

opaNegSelAPORT4YCH24

APORT4YCH24

opaNegSelAPORT4YCH26

APORT4YCH26

opaNegSelAPORT4YCH28

APORT4YCH28

opaNegSelAPORT4YCH30

APORT4YCH30

opaNegSelDisable

Input disabled.

opaNegSelUnityGain

Unity gain feedback path.

opaNegSelResTap

Feedback resistor ladder tap.

opaNegSelNegPad

Negative pad as input.

Definition at line 101 of file em_opamp.h .

OPAMP output terminal selection values.

Enumerator
opaOutModeDisable

OPA output disabled.

opaOutModeMain

Main output to pin enabled.

opaOutModeAlt

Alternate output(s) enabled (not OPA2).

opaOutModeAll

Both main and alternate enabled (not OPA2).

opaOutModeAPORT1YCH1

APORT output to APORT1YCH1 pin enabled.

opaOutModeAPORT1YCH3

APORT output to APORT1YCH3 pin enabled.

opaOutModeAPORT1YCH5

APORT output to APORT1YCH5 pin enabled.

opaOutModeAPORT1YCH7

APORT output to APORT1YCH7 pin enabled.

opaOutModeAPORT1YCH9

APORT output to APORT1YCH9 pin enabled.

opaOutModeAPORT1YCH11

APORT output to APORT1YCH11 pin enabled.

opaOutModeAPORT1YCH13

APORT output to APORT1YCH13 pin enabled.

opaOutModeAPORT1YCH15

APORT output to APORT1YCH15 pin enabled.

opaOutModeAPORT1YCH17

APORT output to APORT1YCH17 pin enabled.

opaOutModeAPORT1YCH19

APORT output to APORT1YCH19 pin enabled.

opaOutModeAPORT1YCH21

APORT output to APORT1YCH21 pin enabled.

opaOutModeAPORT1YCH23

APORT output to APORT1YCH23 pin enabled.

opaOutModeAPORT1YCH25

APORT output to APORT1YCH25 pin enabled.

opaOutModeAPORT1YCH27

APORT output to APORT1YCH27 pin enabled.

opaOutModeAPORT1YCH29

APORT output to APORT1YCH29 pin enabled.

opaOutModeAPORT1YCH31

APORT output to APORT1YCH31 pin enabled.

opaOutModeAPORT2YCH0

APORT output to APORT2YCH0 pin enabled.

opaOutModeAPORT2YCH2

APORT output to APORT2YCH2 pin enabled.

opaOutModeAPORT2YCH4

APORT output to APORT2YCH4 pin enabled.

opaOutModeAPORT2YCH6

APORT output to APORT2YCH6 pin enabled.

opaOutModeAPORT2YCH8

APORT output to APORT2YCH8 pin enabled.

opaOutModeAPORT2YCH10

APORT output to APORT2YCH10 pin enabled.

opaOutModeAPORT2YCH12

APORT output to APORT2YCH12 pin enabled.

opaOutModeAPORT2YCH14

APORT output to APORT2YCH14 pin enabled.

opaOutModeAPORT2YCH16

APORT output to APORT2YCH16 pin enabled.

opaOutModeAPORT2YCH18

APORT output to APORT2YCH18 pin enabled.

opaOutModeAPORT2YCH20

APORT output to APORT2YCH20 pin enabled.

opaOutModeAPORT2YCH22

APORT output to APORT2YCH22 pin enabled.

opaOutModeAPORT2YCH24

APORT output to APORT2YCH24 pin enabled.

opaOutModeAPORT2YCH26

APORT output to APORT2YCH26 pin enabled.

opaOutModeAPORT2YCH28

APORT output to APORT2YCH28 pin enabled.

opaOutModeAPORT2YCH30

APORT output to APORT2YCH30 pin enabled.

opaOutModeAPORT3YCH1

APORT output to APORT3YCH1 pin enabled.

opaOutModeAPORT3YCH3

APORT output to APORT3YCH3 pin enabled.

opaOutModeAPORT3YCH5

APORT output to APORT3YCH5 pin enabled.

opaOutModeAPORT3YCH7

APORT output to APORT3YCH7 pin enabled.

opaOutModeAPORT3YCH9

APORT output to APORT3YCH9 pin enabled.

opaOutModeAPORT3YCH11

APORT output to APORT3YCH11 pin enabled.

opaOutModeAPORT3YCH13

APORT output to APORT3YCH13 pin enabled.

opaOutModeAPORT3YCH15

APORT output to APORT3YCH15 pin enabled.

opaOutModeAPORT3YCH17

APORT output to APORT3YCH17 pin enabled.

opaOutModeAPORT3YCH19

APORT output to APORT3YCH19 pin enabled.

opaOutModeAPORT3YCH21

APORT output to APORT3YCH21 pin enabled.

opaOutModeAPORT3YCH23

APORT output to APORT3YCH23 pin enabled.

opaOutModeAPORT3YCH25

APORT output to APORT3YCH25 pin enabled.

opaOutModeAPORT3YCH27

APORT output to APORT3YCH27 pin enabled.

opaOutModeAPORT3YCH29

APORT output to APORT3YCH29 pin enabled.

opaOutModeAPORT3YCH31

APORT output to APORT3YCH31 pin enabled.

opaOutModeAPORT4YCH0

APORT output to APORT4YCH0 pin enabled.

opaOutModeAPORT4YCH2

APORT output to APORT4YCH2 pin enabled.

opaOutModeAPORT4YCH4

APORT output to APORT4YCH4 pin enabled.

opaOutModeAPORT4YCH6

APORT output to APORT4YCH6 pin enabled.

opaOutModeAPORT4YCH8

APORT output to APORT4YCH8 pin enabled.

opaOutModeAPORT4YCH10

APORT output to APORT4YCH10 pin enabled.

opaOutModeAPORT4YCH12

APORT output to APORT4YCH12 pin enabled.

opaOutModeAPORT4YCH14

APORT output to APORT4YCH14 pin enabled.

opaOutModeAPORT4YCH16

APORT output to APORT4YCH16 pin enabled.

opaOutModeAPORT4YCH18

APORT output to APORT4YCH18 pin enabled.

opaOutModeAPORT4YCH20

APORT output to APORT4YCH20 pin enabled.

opaOutModeAPORT4YCH22

APORT output to APORT4YCH22 pin enabled.

opaOutModeAPORT4YCH24

APORT output to APORT4YCH24 pin enabled.

opaOutModeAPORT4YCH26

APORT output to APORT4YCH26 pin enabled.

opaOutModeAPORT4YCH28

APORT output to APORT4YCH28 pin enabled.

opaOutModeAPORT4YCH30

APORT output to APORT4YCH30 pin enabled.

Definition at line 261 of file em_opamp.h .

Enumerator
opaOutScaleDefault

Default OPAM output drive strength.

opaOutScaleFull

OPAMP uses full output drive strength.

opaOutSacleHalf

OPAMP uses half output drive strength.

Definition at line 420 of file em_opamp.h .

OPAMP positive terminal input selection values.

Enumerator
opaPosSelAPORT1XCH0

APORT1XCH0

opaPosSelAPORT1XCH2

APORT1XCH2

opaPosSelAPORT1XCH4

APORT1XCH4

opaPosSelAPORT1XCH6

APORT1XCH6

opaPosSelAPORT1XCH8

APORT1XCH8

opaPosSelAPORT1XCH10

APORT1XCH10

opaPosSelAPORT1XCH12

APORT1XCH12

opaPosSelAPORT1XCH14

APORT1XCH14

opaPosSelAPORT1XCH16

APORT1XCH16

opaPosSelAPORT1XCH18

APORT1XCH18

opaPosSelAPORT1XCH20

APORT1XCH20

opaPosSelAPORT1XCH22

APORT1XCH22

opaPosSelAPORT1XCH24

APORT1XCH24

opaPosSelAPORT1XCH26

APORT1XCH26

opaPosSelAPORT1XCH28

APORT1XCH28

opaPosSelAPORT1XCH30

APORT1XCH30

opaPosSelAPORT2XCH1

APORT2XCH1

opaPosSelAPORT2XCH3

APORT2XCH3

opaPosSelAPORT2XCH5

APORT2XCH5

opaPosSelAPORT2XCH7

APORT2XCH7

opaPosSelAPORT2XCH9

APORT2XCH9

opaPosSelAPORT2XCH11

APORT2XCH11

opaPosSelAPORT2XCH13

APORT2XCH13

opaPosSelAPORT2XCH15

APORT2XCH15

opaPosSelAPORT2XCH17

APORT2XCH17

opaPosSelAPORT2XCH19

APORT2XCH19

opaPosSelAPORT2XCH21

APORT2XCH21

opaPosSelAPORT2XCH23

APORT2XCH23

opaPosSelAPORT2XCH25

APORT2XCH25

opaPosSelAPORT2XCH27

APORT2XCH27

opaPosSelAPORT2XCH29

APORT2XCH29

opaPosSelAPORT2XCH31

APORT2XCH31

opaPosSelAPORT3XCH0

APORT3XCH0

opaPosSelAPORT3XCH2

APORT3XCH2

opaPosSelAPORT3XCH4

APORT3XCH4

opaPosSelAPORT3XCH6

APORT3XCH6

opaPosSelAPORT3XCH8

APORT3XCH8

opaPosSelAPORT3XCH10

APORT3XCH10

opaPosSelAPORT3XCH12

APORT3XCH12

opaPosSelAPORT3XCH14

APORT3XCH14

opaPosSelAPORT3XCH16

APORT3XCH16

opaPosSelAPORT3XCH18

APORT3XCH18

opaPosSelAPORT3XCH20

APORT3XCH20

opaPosSelAPORT3XCH22

APORT3XCH22

opaPosSelAPORT3XCH24

APORT3XCH24

opaPosSelAPORT3XCH26

APORT3XCH26

opaPosSelAPORT3XCH28

APORT3XCH28

opaPosSelAPORT3XCH30

APORT3XCH30

opaPosSelAPORT4XCH1

APORT4XCH1

opaPosSelAPORT4XCH3

APORT4XCH3

opaPosSelAPORT4XCH5

APORT4XCH5

opaPosSelAPORT4XCH7

APORT4XCH7

opaPosSelAPORT4XCH9

APORT4XCH9

opaPosSelAPORT4XCH11

APORT4XCH11

opaPosSelAPORT4XCH13

APORT4XCH13

opaPosSelAPORT4XCH15

APORT4XCH15

opaPosSelAPORT4XCH17

APORT4XCH17

opaPosSelAPORT4XCH19

APORT4XCH19

opaPosSelAPORT4XCH21

APORT4XCH21

opaPosSelAPORT4XCH23

APORT4XCH23

opaPosSelAPORT4XCH25

APORT4XCH25

opaPosSelAPORT4XCH27

APORT4XCH27

opaPosSelAPORT4XCH29

APORT4XCH29

opaPosSelAPORT4XCH31

APORT4XCH31

opaPosSelDisable

Input disabled.

opaPosSelDac

DAC as input (not OPA2).

opaPosSelPosPad

Positive pad as input.

opaPosSelOpaIn

Input from OPAx.

opaPosSelResTap

Feedback resistor ladder tap.

Definition at line 180 of file em_opamp.h .

Enumerator
opaPrsModeDefault

Default value when PRS is not the trigger.

opaPrsModePulsed

PRS trigger is a pulse that starts the OPAMP warmup sequence. The end of the warmup sequence is controlled by timeout settings in OPAxTIMER.

opaPrsModeTimed

PRS trigger is a pulse long enough to provide the OPAMP warmup sequence. The end of the warmup sequence is controlled by the edge of the pulse.

Definition at line 386 of file em_opamp.h .

Enumerator
opaPrsOutDefault

Default value.

opaPrsOutWarm

Warm status available on PRS.

opaPrsOutOutValid

Outvalid status available on PRS.

Definition at line 414 of file em_opamp.h .

Enumerator
opaPrsSelDefault

Default value when PRS is not the trigger.

opaPrsSelCh0

PRS channel 0 triggers OPAMP.

opaPrsSelCh1

PRS channel 1 triggers OPAMP.

opaPrsSelCh2

PRS channel 2 triggers OPAMP.

opaPrsSelCh3

PRS channel 3 triggers OPAMP.

opaPrsSelCh4

PRS channel 4 triggers OPAMP.

opaPrsSelCh5

PRS channel 5 triggers OPAMP.

opaPrsSelCh6

PRS channel 6 triggers OPAMP.

opaPrsSelCh7

PRS channel 7 triggers OPAMP.

opaPrsSelCh8

PRS channel 8 triggers OPAMP.

opaPrsSelCh9

PRS channel 9 triggers OPAMP.

opaPrsSelCh10

PRS channel 10 triggers OPAMP.

opaPrsSelCh11

PRS channel 11 triggers OPAMP.

Definition at line 396 of file em_opamp.h .

OPAMP resistor ladder input selector values.

Enumerator
opaResInMuxDisable

Resistor ladder disabled.

opaResInMuxOpaIn

Input from OPAx.

opaResInMuxNegPad

Input from negative pad.

opaResInMuxPosPad

Input from positive pad.

opaResInMuxComPad

Input from negative pad of OPA0. Direct input to support common reference.

opaResInMuxCenter

OPA0 and OPA1 Resmux connected to form fully differential instrumentation amplifier.

opaResInMuxVss

Input connected to Vss.

Definition at line 365 of file em_opamp.h .

OPAMP gain values.

Enumerator
opaResSelDefault

Default value when resistor ladder is unused.

opaResSelR2eq0_33R1

R2 = 0.33 * R1

opaResSelR2eqR1

R2 = R1

opaResSelR1eq1_67R1

R2 = 1.67 R1

opaResSelR2eq2_2R1

R2 = 2.2 * R1

opaResSelR2eq3R1

R2 = 3 * R1

opaResSelR2eq4_33R1

R2 = 4.33 * R1

opaResSelR2eq7R1

R2 = 7 * R1

opaResSelR2eq15R1

R2 = 15 * R1

Definition at line 340 of file em_opamp.h .

OPAMP selector values.

Enumerator
OPA0

Select OPA0.

OPA1

Select OPA1.

Definition at line 85 of file em_opamp.h .

Function Documentation

void OPAMP_Disable ( VDAC_TypeDef * dac,
OPAMP_TypeDef opa
)

Disable an Operational Amplifier.

Parameters
[in] dac A pointer to the VDAC peripheral register block.
[in] opa Selects an OPA, valid values are OPA0 , OPA1 , and OPA2.

Definition at line 258 of file em_opamp.c .

References OPA0 , and OPA1 .

Referenced by OPAMP_Enable() .

void OPAMP_Enable ( VDAC_TypeDef * dac,
OPAMP_TypeDef opa,
const OPAMP_Init_TypeDef * init
)

Configure and enable an Operational Amplifier.

Note
The value of the alternate output enable bit mask in the OPAMP_Init_TypeDef structure should consist of one or more of the VDAC_OPA_OUT_ALTOUTPADEN_OUT[output#] flags (defined in <part_name>_vdac.h) OR'ed together.

  • VDAC_OPA_OUT_ALTOUTPADEN_OUT0
  • VDAC_OPA_OUT_ALTOUTPADEN_OUT1
  • VDAC_OPA_OUT_ALTOUTPADEN_OUT2
  • VDAC_OPA_OUT_ALTOUTPADEN_OUT3
  • VDAC_OPA_OUT_ALTOUTPADEN_OUT4
For example:
init.outPen = VDAC_OPA_OUT_ALTOUTPADEN_OUT0 | VDAC_OPA_OUT_ALTOUTPADEN_OUT4;
Parameters
[in] dac A pointer to the VDAC peripheral register block.
[in] opa Selects an OPA, valid values are OPA0 , OPA1 , and OPA2.
[in] init A pointer to a structure containing OPAMP initialization information.

Definition at line 369 of file em_opamp.c .

References OPAMP_Init_TypeDef::aportXMasterDisable , OPAMP_Init_TypeDef::aportYMasterDisable , OPAMP_Init_TypeDef::defaultOffsetN , OPAMP_Init_TypeDef::defaultOffsetP , OPAMP_Init_TypeDef::drvStr , OPAMP_Init_TypeDef::gain3xEn , OPAMP_Init_TypeDef::halfDrvStr , OPAMP_Init_TypeDef::hcmDisable , OPAMP_Init_TypeDef::negSel , OPAMP_Init_TypeDef::offsetN , OPAMP_Init_TypeDef::offsetP , OPA0 , OPA1 , opaDrvStrHighAccHighStr , opaDrvStrHigherAccHighStr , opaDrvStrLowAccLowStr , opaDrvStrLowerAccLowStr , OPAMP_Disable() , opaNegSelResTap , opaPosSelResTap , OPAMP_Init_TypeDef::outMode , OPAMP_Init_TypeDef::outPen , OPAMP_Init_TypeDef::posSel , OPAMP_Init_TypeDef::prsEn , OPAMP_Init_TypeDef::prsMode , OPAMP_Init_TypeDef::prsOutSel , OPAMP_Init_TypeDef::prsSel , OPAMP_Init_TypeDef::resInMux , OPAMP_Init_TypeDef::resSel , OPAMP_Init_TypeDef::settleTime , OPAMP_Init_TypeDef::startupDly , SYSTEM_GetCalibrationValue() , and OPAMP_Init_TypeDef::ugBwScale .