VddCheck

Detailed Description

VDD Voltage Check using EMLIB Voltage Comparator (VCOMP) API.

Functions

void VDDCHECK_Disable (void)
VCMP deinitialization routine.
void VDDCHECK_Init (void)
VCMP initialization routine.
bool VDDCHECK_LowVoltage (float vdd)
Check if voltage is higher than indicated.

Function Documentation

bool VDDCHECK_LowVoltage ( float vdd )

Check if voltage is higher than indicated.

Parameters
vdd The voltage level to compare against.
Returns
Returns true if voltage is lower, false otherwise

Definition at line 81 of file vddcheck.c .