VDAC channel initialization structure.
Definition at line 207
of file em_vdac.h
.
#include <
em_vdac.h
>
Data Fields | |
bool | enable |
bool | prsAsync |
VDAC_PrsSel_TypeDef | prsSel |
bool | sampleOffMode |
VDAC_TrigMode_TypeDef | trigMode |
Field Documentation
bool VDAC_InitChannel_TypeDef::enable |
bool VDAC_InitChannel_TypeDef::prsAsync |
Treat the PRS signal asynchronously.
Definition at line 217
of file em_vdac.h
.
Referenced by VDAC_InitChannel().
VDAC_PrsSel_TypeDef VDAC_InitChannel_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if trigMode
is set to vdacTrigModePrs
or vdacTrigModeSwPrs
.
Definition at line 214
of file em_vdac.h
.
Referenced by VDAC_InitChannel().
bool VDAC_InitChannel_TypeDef::sampleOffMode |
Set channel conversion mode to sample/shut-off mode. Default is continuous.
Definition at line 224
of file em_vdac.h
.
Referenced by VDAC_InitChannel().
VDAC_TrigMode_TypeDef VDAC_InitChannel_TypeDef::trigMode |
Channel conversion trigger mode.
Definition at line 220
of file em_vdac.h
.
Referenced by VDAC_InitChannel().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_vdac.h