sl_mpu.c File Reference
MPU API implementation.
- Version
- 1.0.0
License
(C) Copyright 2018 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file sl_mpu.c
.
#include "em_device.h"
#include "em_common.h
"
#include "em_core.h
"
#include "sl_mpu.h
"
#include <stdlib.h>
#include <math.h>
Functions | |
static void | mpu_compute_region_data (uint32_t section_begin, uint32_t section_end, uint32_t section_size, uint32_t *mpu_region_begin, uint32_t *mpu_region_end, uint32_t *mpu_region_size) |
static uint8_t | mpu_region_size_encode (uint32_t region_size) |
static uint32_t | mpu_round_up_next_pwr2 (uint32_t nbr) |
void | sl_mpu_disable_execute (uint32_t address_begin, uint32_t address_end, uint32_t size) |
void | sl_mpu_disable_execute_from_ram (void) |
Variables | |
uint32_t | __ram_func_section_end |
uint32_t | __ram_func_section_start |
static uint32_t | region_nbr = 0 |
Function Documentation
|
static |
Compute region size.
- Parameters
-
section_begin
Section begin address. section_end
Section end address. section_size
Size of section. mpu_region_begin
Pointer to a region begin variable. mpu_region_end
Pointer to a region end variable. mpu_region_size
Pointer to a region size variable.
Definition at line 299
of file sl_mpu.c
.
References mpu_round_up_next_pwr2().
Referenced by sl_mpu_disable_execute(), and sl_mpu_disable_execute_from_ram().
|
static |
Encode region size in RASR register REGION size field format.
- Parameters
-
region_size
Size of region.
Definition at line 277
of file sl_mpu.c
.
Referenced by sl_mpu_disable_execute(), and sl_mpu_disable_execute_from_ram().
|
static |
Rounds up given number to next power of 2.
- Parameters
-
nbr
Number to round-up to next power of 2.
Definition at line 257
of file sl_mpu.c
.
Referenced by mpu_compute_region_data().