Measurement mode initialization structure.
Definition at line 392
of file em_csen.h
.
#include <
em_csen.h
>
Data Fields | |
CSEN_AccMode_TypeDef | accMode |
bool | autoGnd |
CSEN_CmpMode_TypeDef | cmpMode |
uint16_t | cmpThr |
CSEN_ConvSel_TypeDef | convSel |
uint8_t | dmCycles |
uint8_t | dmDelta |
bool | dmFixedDelta |
uint8_t | dmIterPerCycle |
CSEN_DMRes_TypeDef | dmRes |
CSEN_DriveSel_TypeDef | driveSel |
CSEN_EMASample_TypeDef | emaSample |
bool | enableDma |
CSEN_GainSel_TypeDef | gainSel |
uint32_t | inputMask0 |
uint32_t | inputMask1 |
CSEN_ResetPhaseSel_TypeDef | resetPhase |
CSEN_SampleMode_TypeDef | sampleMode |
CSEN_SARRes_TypeDef | sarRes |
CSEN_SingleSel_TypeDef | singleSel |
bool | sumOnly |
CSEN_TrigSel_TypeDef | trigSel |
Field Documentation
CSEN_AccMode_TypeDef CSEN_InitMode_TypeDef::accMode |
Selects the number of samples to accumulate per conversion.
Definition at line 406
of file em_csen.h
.
Referenced by CSEN_InitMode().
bool CSEN_InitMode_TypeDef::autoGnd |
Ground inactive inputs during a conversion.
Definition at line 433
of file em_csen.h
.
Referenced by CSEN_InitMode().
CSEN_CmpMode_TypeDef CSEN_InitMode_TypeDef::cmpMode |
Enables the comparator and selects the comparison type.
Definition at line 412
of file em_csen.h
.
Referenced by CSEN_InitMode().
uint16_t CSEN_InitMode_TypeDef::cmpThr |
Comparator threshold value. Meaning depends on cmpMode
.
Definition at line 415
of file em_csen.h
.
Referenced by CSEN_InitMode().
CSEN_ConvSel_TypeDef CSEN_InitMode_TypeDef::convSel |
Selects the converter type.
Definition at line 436
of file em_csen.h
.
Referenced by CSEN_InitMode().
uint8_t CSEN_InitMode_TypeDef::dmCycles |
Sets number of DM converter cycles. Only applies to the Delta Modulation converter.
Definition at line 450
of file em_csen.h
.
Referenced by CSEN_InitMode().
uint8_t CSEN_InitMode_TypeDef::dmDelta |
Sets the DM converter initial delta value. Only applies to the Delta Modulation converter.
Definition at line 454
of file em_csen.h
.
Referenced by CSEN_InitMode().
bool CSEN_InitMode_TypeDef::dmFixedDelta |
Disables DM automatic delta size reduction per cycle. Only applies to the Delta Modulation converter.
Definition at line 458
of file em_csen.h
.
Referenced by CSEN_InitMode().
uint8_t CSEN_InitMode_TypeDef::dmIterPerCycle |
Sets the number of DM iterations (comparisons) per cycle. Only applies to the Delta Modulation converter.
Definition at line 446
of file em_csen.h
.
Referenced by CSEN_InitMode().
CSEN_DMRes_TypeDef CSEN_InitMode_TypeDef::dmRes |
Selects the Delta Modulation (DM) converter resolution.
Definition at line 442
of file em_csen.h
.
Referenced by CSEN_InitMode().
CSEN_DriveSel_TypeDef CSEN_InitMode_TypeDef::driveSel |
Selects the output drive strength. Most measurements should use the default value. See reference manual for details on when to adjust.
Definition at line 466
of file em_csen.h
.
Referenced by CSEN_InitMode().
CSEN_EMASample_TypeDef CSEN_InitMode_TypeDef::emaSample |
Selects the Exponential Moving Average sample weighting.
Definition at line 409
of file em_csen.h
.
Referenced by CSEN_InitMode().
bool CSEN_InitMode_TypeDef::enableDma |
CSEN_GainSel_TypeDef CSEN_InitMode_TypeDef::gainSel |
Selects the converter gain.
Definition at line 469
of file em_csen.h
.
Referenced by CSEN_InitMode().
uint32_t CSEN_InitMode_TypeDef::inputMask0 |
Mask selects inputs 0 to 31. Effect depends on sampleMode
. If sample mode is bonded, then mask selects inputs to short together. If sample mode is scan, then mask selects which inputs will be scanned. If sample mode is single and auto-ground is on (autoGnd
is true), mask selects which pins are grounded.
Definition at line 427
of file em_csen.h
.
Referenced by CSEN_InitMode().
uint32_t CSEN_InitMode_TypeDef::inputMask1 |
Mask selects inputs 32 to 63. See inputMask0
for more information.
Definition at line 430
of file em_csen.h
.
Referenced by CSEN_InitMode().
CSEN_ResetPhaseSel_TypeDef CSEN_InitMode_TypeDef::resetPhase |
Selects the reset phase timing. Most measurements should use the default value. See reference manual for details on when to adjust.
Definition at line 462
of file em_csen.h
.
Referenced by CSEN_InitMode().
CSEN_SampleMode_TypeDef CSEN_InitMode_TypeDef::sampleMode |
Selects the conversion sample mode.
Definition at line 394
of file em_csen.h
.
Referenced by CSEN_InitMode().
CSEN_SARRes_TypeDef CSEN_InitMode_TypeDef::sarRes |
Selects the Successive Approximation (SAR) converter resolution.
Definition at line 439
of file em_csen.h
.
Referenced by CSEN_InitMode().
CSEN_SingleSel_TypeDef CSEN_InitMode_TypeDef::singleSel |
Selects an APORT channel for a single conversion.
Definition at line 418
of file em_csen.h
.
Referenced by CSEN_InitMode().
bool CSEN_InitMode_TypeDef::sumOnly |
Disables dividing the accumulated result.
Definition at line 403
of file em_csen.h
.
Referenced by CSEN_InitMode().
CSEN_TrigSel_TypeDef CSEN_InitMode_TypeDef::trigSel |
Selects the conversion trigger source.
Definition at line 397
of file em_csen.h
.
Referenced by CSEN_InitMode().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_csen.h