VMON Hysteresis initialization structure.
       Definition at line
       
        881
       
       of file
       
        em_emu.h
       
       .
      
      
       #include <
       
     
        em_emu.h
       
       >
      
         Data Fields | 
       |
| EMU_VmonChannel_TypeDef | channel | 
| bool | enable | 
| int | fallThreshold | 
| bool | fallWakeup | 
| int | riseThreshold | 
| bool | riseWakeup | 
Field Documentation
| EMU_VmonChannel_TypeDef EMU_VmonHystInit_TypeDef::channel | 
VMON channel to configure.
        Definition at line
        
         882
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_VmonHystInit() .
| bool EMU_VmonHystInit_TypeDef::enable | 
| int EMU_VmonHystInit_TypeDef::fallThreshold | 
Falling threshold (mV).
        Definition at line
        
         884
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_VmonHystInit() .
| bool EMU_VmonHystInit_TypeDef::fallWakeup | 
Wake up from EM4H on falling edge.
        Definition at line
        
         886
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_VmonHystInit() .
| int EMU_VmonHystInit_TypeDef::riseThreshold | 
| bool EMU_VmonHystInit_TypeDef::riseWakeup | 
Wake up from EM4H on rising edge.
        Definition at line
        
         885
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_VmonHystInit() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_emu.h