ARRAY_TypeDef Struct Reference
Defines segment COM and BIT fields for array.
Definition at line 136
of file segmentlcd.c
.
Data Fields | |
uint8_t | bit [35] |
uint8_t | com [35] |
Field Documentation
uint8_t ARRAY_TypeDef::bit[35] |
LCD bit number
Definition at line 138
of file segmentlcd.c
.
uint8_t ARRAY_TypeDef::com[35] |
LCD COM line (for multiplexing)
Definition at line 137
of file segmentlcd.c
.
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/hardware/kit/common/drivers/
segmentlcd.c