EM_TypeDef Struct Reference
Defines segment COM and BIT fields for Energy Modes on display.
Definition at line 112
of file segmentlcd.c
.
Data Fields | |
uint8_t | bit [5] |
uint8_t | com [5] |
Field Documentation
uint8_t EM_TypeDef::bit[5] |
LCD bit number
Definition at line 114
of file segmentlcd.c
.
uint8_t EM_TypeDef::com[5] |
LCD COM line (for multiplexing)
Definition at line 113
of file segmentlcd.c
.
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/hardware/kit/common/drivers/
segmentlcd.c