Building the Bluetooth Hosts Locally#
This page describes how to configure and build the Bluetooth Host applications on a Raspberry pi 4B or a similar ARM host platform.
Prerequisites#
Clone the Silicon Labs SDK source code on the Raspberry Pi:
git clone https://github.com/SiliconLabs/simplicity_sdk.git
Bluetooth Host Configuration for Multiprotocol NCP#
The default Bluetooth NCP host application (bt_host_empty) is configured to communicate with the NCP target using BGAPI via UART. In order to enable CPC, the application needs to be built with the following command line option:
make CPC=1
The makefile for bt_host_empty is in the following SiSDK directory: <path_to_sdk>/app/bluetooth/example_host/bt_host_empty.
Note: CPCd must first be installed on the system before building the host application.
Bluetooth Host Configuration for Multiprotocol RCP#
BlueZ - Official Linux Bluetooth Stack#
In newer versions of Raspberry Pi OS, BlueZ is already installed by default and the bluetooth service is enabled.
Check the BlueZ stack version using the command
bluetoothd --versionand if not the latest, download the latest version from https://www.kernel.org/pub/linux/bluetooth/ and follow the instructions in the README file.The bluetooth service status can be checked with the command
systemctl status bluetooth, which should give the following output:
● bluetooth.service - Bluetooth service Loaded: loaded (/lib/systemd/system/bluetooth.service; enabled; vendor preset: enabled) Active: active (running) since Tue 2024-10-15 20:24:27 BST; 4 weeks 2 days ago Docs: man:bluetoothd(8) Main PID: 932 (bluetoothd) Status: "Running" Tasks: 1 (limit: 3933) CPU: 5.179s CGroup: /system.slice/bluetooth.service └─932 /usr/libexec/bluetooth/bluetoothd
If the bluetooth service is disabled, manually start the service by running systemctl start bluetooth.
*As of Nov 2024, the latest BlueZ version is 5.79.
CPC HCI Bridge#
The CPC-HCI bridge application connects to the CPCd and exposes a virtual serial device on the Linux host in /dev/pts. The source code and makefile are located in the SiSDK at <path_to_sdk>/app/bluetooth/example/example_host/bt_host_cpc_hci_bridge. Go to the bt_host_cpc_hci_bridge folder and run the following command to build the CPC-HCI bridge application:
make