Running CPCd, Zigbeed, Z3Gateway, OTBR Concurrently on Raspbian#
The purpose of this guide is to provide a hands-on example of running the previously discussed multiprotocol processes concurrently. This guide aims to demonstrate the process of setting up and configuring the Co-Processor Communication Daemon (CPCd), Zigbee Daemon (zigbeed), Zigbee Host application (Z3Gateway), and the OpenThread Border Router (OTBR). This guide assumes that the previous sections: Building CPCd on Raspbian, Building zigbeed and Z3Gateway on Raspbian (UART), Building Zigbee host, and Building OTBR on Raspbian have been completed.
Running CPCd#
This step must be done before before running the Zigbee or OpenThread processes. CPCd can either be run from systemd or via the binary in the build folder, this guide will cover both. Note that by default CPCd encryption is turned on. This means you will have an additional CPCd binding step. The steps below have disabled CPC Security on both CPCd and the RCP.
Running CPCd from the Binary#
This method runs the CPCd binary directly in the terminal. If logging is enabled, debug logs will appear as shown below. The log level can be adjusted in the cpcd.conf file.
From the cpcd/build/debug/out folder: ./cpcd -c [/path_to_cpcd_conf] -[options] or cpcd/build/debug/out/cpcd -c [/path_to_cpcd_conf] -[options]
If you are running CPCd with security enabled you will first need to run:
./cpcd -c cpcd.conf --bind ecdh
Running CPCd as a Service in the Background#
If you chose to run CPCd as a service in the background, you can create a cpcd.service file and move it to the following location: /etc/systemd/system. Now with this file installed, you can simply start CPCd by running the following command:
systemctl start cpcd
To view the status of this process:
systemctl status cpcd
Should yield an output like the following:
● cpcd.service - Cpcd service Loaded: loaded (/etc/systemd/system/cpcd.service; disabled; vendor preset: enabled) Active: active (running) since Tue 2024-09-23 20:31:18 UTC; 4s ago Main PID: 1170 (cpcd) Tasks: 6 (limit: 9238) CPU: 32ms CGroup: /system.slice/cpcd.service └─1170 /usr/local/bin/cpcd
CPCd Log Example#
[2024-09-20T19:28:38.039762Z] Info : [CPCd v4.5.0.0] [Library API v3] [RCP Protocol v5] [2024-09-20T19:28:38.040027Z] Info : Git commit: f7cb761e18f338f09b4a59f07f6458aefb0a0f05 / branch: refs/heads/main [2024-09-20T19:28:38.040047Z] Info : Reading cli arguments [2024-09-20T19:28:38.040067Z] Info : ./cpcd [2024-09-20T19:28:38.040999Z] Info : Reading configuration [2024-09-20T19:28:38.041019Z] Info : file_path = /usr/local/etc/cpcd.conf [2024-09-20T19:28:38.041029Z] Info : instance_name = cpcd_0 [2024-09-20T19:28:38.041038Z] Info : socket_folder = /dev/shm [2024-09-20T19:28:38.041048Z] Info : operation_mode = MODE_NORMAL [2024-09-20T19:28:38.041057Z] Info : use_encryption = false [2024-09-20T19:28:38.041066Z] Info : binding_key_file = /home/orkevlar/.cpcd/binding.key [2024-09-20T19:28:38.041075Z] Info : stdout_tracing = false [2024-09-20T19:28:38.041084Z] Info : file_tracing = false [2024-09-20T19:28:38.041092Z] Info : lttng_tracing = false [2024-09-20T19:28:38.041100Z] Info : enable_frame_trace = false [2024-09-20T19:28:38.041108Z] Info : traces_folder = /dev/shm/cpcd-traces [2024-09-20T19:28:38.041117Z] Info : bus = UART [2024-09-20T19:28:38.041125Z] Info : uart_baudrate = 115200 [2024-09-20T19:28:38.041134Z] Info : uart_hardflow = true [2024-09-20T19:28:38.041142Z] Info : uart_file = /dev/ttyACM0 [2024-09-20T19:28:38.041151Z] Info : fwu_recovery_pins_enabled = false [2024-09-20T19:28:38.041160Z] Info : fwu_connect_to_bootloader = false [2024-09-20T19:28:38.041168Z] Info : fwu_enter_bootloader = false [2024-09-20T19:28:38.041177Z] Info : restart_cpcd = false [2024-09-20T19:28:38.041185Z] Info : application_version_validation = false [2024-09-20T19:28:38.041194Z] Info : print_secondary_versions_and_exit = false [2024-09-20T19:28:38.041202Z] Info : use_noop_keep_alive = false [2024-09-20T19:28:38.041210Z] Info : reset_sequence = true [2024-09-20T19:28:38.041218Z] Info : stats_interval = 0 [2024-09-20T19:28:38.041226Z] Info : rlimit_nofile = 2000 [2024-09-20T19:28:38.041236Z] Info : ENCRYPTION IS DISABLED [2024-09-20T19:28:38.052580Z] Info : Starting daemon in normal mode [2024-09-20T19:28:38.063960Z] Info : Connecting to Secondary... [2024-09-20T19:28:38.230299Z] Info : RX capability is 256 bytes [2024-09-20T19:28:38.230329Z] Info : Connected to Secondary [2024-09-20T19:28:38.236297Z] Info : Secondary Protocol v5 [2024-09-20T19:28:38.249294Z] Info : Secondary CPC v4.5.0 [2024-09-20T19:28:38.261343Z] Info : Secondary bus bitrate is 115200 [2024-09-20T19:28:38.273286Z] Info : Secondary APP vUNDEFINED [2024-09-20T19:28:38.273546Z] Info : Daemon startup was successful. Waiting for client connections
When either the otbr-agent or zigbeed are connected to cpcd, the following will appear in the cpcd logs:
[2024-09-23T18:09:26.299013Z] Info : New client connection using library v4.5.2.0 [2024-09-23T18:09:26.305764Z] Info : Opened connection socket for ep#12 [2024-09-23T18:09:26.313604Z] Info : Endpoint socket #12: Client connected. 1 connection(s)
When both are connected, the logs will show:
[2024-09-23T20:01:07.851455Z] Info : New client connection using library v4.5.2.0 [2024-09-23T20:01:07.858154Z] Info : Endpoint socket #12: Client connected. 2 connection(s)
When the CPC-HCI bridge is connected to CPCd, the log will show:
[2024-11-15T20:43:46.043660Z] Info : New client connection using library v4.5.2.0 [2024-11-15T20:43:46.056109Z] Info : Opened connection socket for ep#14 [2024-11-15T20:43:46.065940Z] Info : Endpoint socket #14: Client connected. 1 connection(s)
Running Zigbeed#
This must be done after CPCd is running.
Running Socat#
You can run Socat from the command line by following this command:
socat -x -v pty,link=/dev/ttyZigbeeNCP pty,link=/tmp/ttyZigbeeNCP
This command creates a virtual serial port for Zigbee Communication.
Running Socat as a Service in the Background#
Similarly, Socat can be run as a service with systemd.
This service requires the zigbeed-socat.service file to be created and copied into the /etc/systemd/system/.. directory. Now you can start zigbeed-socat with:
sudo systemctl start zigbeed-socat
To view the status of this process:
systemctl status zigbeed-socat
Should yield an output like the following:
● zigbeed-socat.service - Zigbeed socat helper service Loaded: loaded (/etc/systemd/system/zigbeed-socat.service; disabled; vendor preset: enabled) Active: active (running) since Tue 2024-09-23 20:31:18 UTC; 4s ago Main PID: 1171 (socat) Tasks: 1 (limit: 9238) CPU: 14ms CGroup: /system.slice/zigbeed-socat.service └─1171 /usr/bin/socat -v pty,link=/dev/ttyZigbeeNCP pty,link=/tmp/ttyZigbeeNCP
Running Zigbeed from the Binary#
This method runs the Zigbeed binary directly in the terminal. If logging is enabled, debug logs will appear as shown below. The log level can be adjusted in the zigbeed.conf file.
From the zigbeed/build/debug/out folder: ./zigbeed -[options] or zigbeed/build/debug/out/zigbeed -[options]
The zigbeed logs will appear in the terminal as shown below:
By using this software, you are agreeing to the Silicon Labs MSLA found at https://www.silabs.com/about-us/legal/master-software-license-agreement. zigbeed[5479]: [D] P-SpinelDrive-: Received spinel frame, flg:0x2, iid:0, tid:0, cmd:PROP_VALUE_IS, key:LAST_STATUS, status:RESET_SOFTWARE zigbeed[5479]: [I] P-SpinelDrive-: co-processor reset: RESET_SOFTWARE zigbeed[5479]: [D] P-SpinelDrive-: Sent spinel frame, flg:0x2, iid:1, tid:0, cmd:RESET zigbeed[5479]: [D] P-SpinelDrive-: Waiting response: key=0 zigbeed[5479]: [C] P-SpinelDrive-: Software reset co-processor successfully zigbeed[5479]: [D] P-SpinelDrive-: Waiting response: key=1 zigbeed[5479]: [D] P-SpinelDrive-: Received spinel frame, flg:0x2, iid:1, tid:1, cmd:PROP_VALUE_IS, key:PROTOCOL_VERSION, major:4, minor:3 zigbeed[5479]: [D] P-SpinelDrive-: Received spinel frame, flg:0x2, iid:0, tid:0, cmd:PROP_VALUE_IS, key:LAST_STATUS, status:RESET_SOFTWARE zigbeed[5479]: [I] P-SpinelDrive-: co-processor reset: RESET_SOFTWARE zigbeed[5479]: [D] P-SpinelDrive-: Waiting response: key=2 zigbeed[5479]: [D] P-SpinelDrive-: Received spinel frame, flg:0x2, iid:1, tid:1, cmd:PROP_VALUE_IS, key:NCP_VERSION, version:SL-OPENTHREAD/2.5.1.0_GitHub-1fceb225b; zigbeed[5479]: [D] P-SpinelDrive-: Waiting response: key=5 zigbeed[5479]: [D] P-SpinelDrive-: Received spinel frame, flg:0x2, iid:1, tid:1, cmd:PROP_VALUE_IS, key:CAPS, caps:COUNTERS UNSOL_UPDATE_FILTER 802_15_4_2450MHZ_OQP zigbeed[5479]: [D] Platform------: instance init:0xcd178 - iid = 1 zigbeed[5479]: [D] P-RadioSpinel-: Wait response: tid=1 key=8 zigbeed[5479]: [D] P-SpinelDrive-: Received spinel frame, flg:0x2, iid:1, tid:1, cmd:PROP_VALUE_IS, key:HWADDR, eui64:90395efffee405e1 zigbeed[5479]: [D] P-RadioSpinel-: RCP supports crash dump logging. Requesting crash dump. zigbeed[5479]: [D] P-RadioSpinel-: Wait response: tid=2 key=178 zigbeed[5479]: [D] P-SpinelDrive-: Received spinel frame, flg:0x2, iid:1, tid:2, cmd:PROP_VALUE_IS, key:LAST_STATUS, status:OK zigbeed[5479]: [D] P-RadioSpinel-: Wait response: tid=3 key=176 zigbeed[5479]: [D] P-SpinelDrive-: Received spinel frame, flg:0x2, iid:1, tid:3, cmd:PROP_VALUE_IS, key:RCP_API_VERSION, version:10 zigbeed[5479]: [D] P-RadioSpinel-: Wait response: tid=4 key=4619 zigbeed[5479]: [D] P-SpinelDrive-: Received spinel frame, flg:0x2, iid:1, tid:4, cmd:PROP_VALUE_IS, key:RADIO_CAPS, caps:255 zigbeed[5479]: Zigbeed started zigbeed[5479]: RCP version: SL-OPENTHREAD/2.5.1.0_GitHub-1fceb225b; EFR32; Sep 20 2024 15:27:16 zigbeed[5479]: Zigbeed Version: GSDK 8.0.1 - Jul 22 2024 - 21:58:48
To record the zigbeed logs to a file, you can use a command like this:
./zigbeed 2>&1 | sudo tee [path-to-out-file]
Running Zigbeed as a Service in the Background#
Again, running Zigbeed as a service in the background will require you to install the zigbeed.service file into /etc/systemd/system directory.
systemctl start zigbeed
To view the status of this process:
systemctl status zigbeed
Should yield an output like the following:
● zigbeed.service - Zigbeed service Loaded: loaded (/etc/systemd/system/zigbeed.service; disabled; vendor preset: enabled) Active: active (running) since Tue 2024-09-23 20:31:18 UTC; 4s ago Main PID: 1173 (zigbeed) Tasks: 1 (limit: 9238) CPU: 17ms CGroup: /system.slice/zigbeed.service └─1173 /usr/local/bin/zigbeed
Running the Zigbee Host Application#
This must be done after Zigbeed has been started. The Zigbee Host application is run directly in the terminal via the binary in the build folder.
From the zigbee_z3_gateway/build/debug/out folder: ./zigbee_z3_gateway -n 0 -p /dev/ttyZigbeeNCP or zigbee_z3_gateway/build/debug/out/z3gateway -n 0 -p /dev/ttyZigbeeNCP
Z3Gateway CLI
Reset info: 11 (SOFTWARE) ezsp ver 0x0E stack type 0x02 stack ver. [8.0.1 GA build 270] Ezsp Config: set address table size to 0x0002:Success: set Ezsp Config: set TC addr cache to 0x0002:Success: set Ezsp Config: set MAC indirect TX timeout to 0x1E00:Success: set Ezsp Config: set max hops to 0x001E:Success: set Ezsp Config: set tx power mode to 0x8000:Success: set Ezsp Config: set supported networks to 0x0001:Success: set Ezsp Config: set stack profile to 0x0002:Success: set Ezsp Config: set security level to 0x0005:Success: set Ezsp Value : set end device keep alive support mode to 0x00000003:Success: set Ezsp Policy: set binding modify to "allow for valid endpoints & clusters only":Success: set Ezsp Policy: set message content in msgSent to "return":Success: set Ezsp Value : set maximum incoming transfer size to 0x00000052:Success: set Ezsp Value : set maximum outgoing transfer size to 0x00000052:Success: set Ezsp Value : set default timeout for transient device table to 0x00002710:Success: set Ezsp Config: set binding table size to 0x0002:Success: set Ezsp Config: set key table size to 0x0004:Success: set Ezsp Config: set max end device children to 0x0006:Success: set Ezsp Config: set aps unicast message count to 0x000A:Success: set Ezsp Config: set broadcast table size to 0x000F:Success: set Ezsp Config: set neighbor table size to 0x0010:Success: set Ezsp Config: set end device poll timeout to 0x0008:Success: set Ezsp Config: set zll group addresses to 0x0000:Success: set Ezsp Config: set zll rssi threshold to 0xFFD8:Success: set Ezsp Config: set transient key timeout to 0x012C:Success: set Ezsp Config: set retry size to 0x0010:Success: set Ezsp Endpoint 1 added, profile 0x0104, in clusters: 8, out clusters 17 Ezsp Endpoint 242 added, profile 0xA1E0, in clusters: 0, out clusters 1 Starting identifying on endpoint 0x01, identify time is 0 sec Stopping identifying on endpoint 0x01 No endpoints identifying; stopping identification feedback. Found 0 files zigbee_z3_gateway>
Running the OTBR#
In the Multiprotocol context, this must be done after CPCd is running. The otbr-agent can be run as a service with systemd or directly in the terminal via the binary.
Running the otbr-agent Binary#
The binary is located in: ~/simplicity_sdk/util/third_party/ot-br-posix/build/otbr/src/agent. The following command will start the otbr-agent, and logs will appear in the terminal window.
sudo ./otbr-agent -d 6 -v -I wpan0 -B eth0 'spinel+cpc://cpcd_0?iid=2&iid-list=0'
If the Radio URL is not configured properly, the OTBR will respond with the following error message:
Aug 14 14:18:21 raspberrypi otbr-agent[8037]: 49d.19:21:57.018 [C] Platform------: Init() at radio.cpp:107: InvalidArgument Aug 14 14:18:21 raspberrypi systemd[1]: otbr-agent.service: Main process exited, code=exited, status=2/INVALIDARGUMENT
The OTBR logs will appear similar to the following if it is running properly:
otbr-agent[1892]: [NOTE]-AGENT---: Running 0.3.0-v2024.6.1-0-1-g36e12f01 otbr-agent[1892]: [NOTE]-AGENT---: Thread version: 1.4 otbr-agent[1892]: [NOTE]-AGENT---: Thread interface: wpan0 otbr-agent[1892]: [NOTE]-AGENT---: Radio URL: spinel+cpc://cpcd_0?iid=2&iid-list=0 otbr-agent[1892]: [NOTE]-ILS-----: Infra link selected: eth0 otbr-agent[1892]: [INFO]-NCP-----: OpenThread log level changed to 4 otbr-agent[1892]: 49d.17:11:58.417 [I] P-SpinelDrive-: co-processor reset: RESET_SOFTWARE otbr-agent[1892]: 49d.17:12:00.447 [C] P-SpinelDrive-: Software reset co-processor successfully otbr-agent[1892]: 49d.17:12:00.504 [I] P-Netif-------: Sent request#1 to set addr_gen_mode to 1 otbr-agent[1892]: 00:00:00.087 [I] ChildSupervsn-: Timeout: 0 -> 190 otbr-agent[1892]: 00:00:00.088 [I] TrelInterface-: Enabled interface, local port:60358 otbr-agent[1892]: 00:00:00.088 [I] RoutingManager: Initializing - InfraIfIndex:2 otbr-agent[1892]: 00:00:00.089 [I] InfraIf-------: Init infra netif 2 otbr-agent[1892]: 00:00:00.089 [I] Settings------: Read BrUlaPrefix fd8b:b68:2457::/48 otbr-agent[1892]: 00:00:00.089 [N] RoutingManager: BR ULA prefix: fd8b:b68:2457::/48 (loaded) otbr-agent[1892]: 00:00:00.089 [I] RoutingManager: Generated local OMR prefix: fd8b:b68:2457:1::/64 otbr-agent[1892]: 00:00:00.089 [I] RoutingManager: Generated local NAT64 prefix: fd8b:b68:2457:2:0:0::/96 otbr-agent[1892]: 00:00:00.089 [N] RoutingManager: Local on-link prefix: fdde:ad00:beef:cafe::/64 otbr-agent[1892]: 00:00:00.089 [I] InfraIf-------: State changed: NOT RUNNING -> RUNNING otbr-agent[1892]: 00:00:00.089 [I] RoutingManager: Enabling otbr-agent[1892]: 00:00:00.089 [I] Nat64---------: IPv4 CIDR for NAT64: 192.168.255.0/24 (actual address pool: 192.168.255.1 - 192.168.255.254, 254 addresses) otbr-agent[1892]: 00:00:00.089 [I] Nat64---------: NAT64 translator is now Disabled otbr-agent[1892]: 00:00:00.090 [I] P-Resolver----: Got nameserver #0: 192.168.0.1 otbr-agent[1892]: [INFO]-UTILS---: Set state callback: OK otbr-agent[1892]: 00:00:00.090 [I] Nat64---------: NAT64 translator is now NotRunning otbr-agent[1892]: [INFO]-BA------: Start Thread Border Agent otbr-agent[1892]: [INFO]-BA------: Publish meshcop service OpenThread BorderRouter #102C._meshcop._udp.local. otbr-agent[1892]: 00:00:00.091 [I] Settings------: Read BorderAgentId {id:27497e430c9fd5c4b52cb337e06f77a7} otbr-agent[1892]: [INFO]-MDNS----: Registering service OpenThread BorderRouter #102C._meshcop._udp otbr-agent[1892]: 00:00:00.097 [I] BbrLocal------: Add Domain Prefix: ::/0, NotFound otbr-agent[1892]: 00:00:00.098 [I] BbrLocal------: Add BBR Service: seqno (73), delay (5s), timeout (3600s), InvalidState otbr-agent[1892]: [INFO]-ADPROXY-: Started otbr-agent[1892]: [INFO]-DPROXY--: Started otbr-agent[1892]: [INFO]-APP-----: Thread Border Router started on AIL eth0. otbr-agent[1892]: 00:00:00.108 [I] Notifier------: StateChanged (0x42038210) [MLAddr NetData PanId NetName ExtPanId BbrState Nat64] otbr-agent[1892]: 00:00:00.108 [I] Bbr-----------: Start listening on port 61631 otbr-agent[1892]: 00:00:00.108 [I] Bbr-----------: Backbone TMF subscribes ff32:40:fdde:ad00:beef:0:0:3: OK otbr-agent[1892]: 00:00:00.109 [I] BbrManager----: Start Backbone TMF agent: OK otbr-agent[1892]: 00:00:00.114 [I] Platform------: Execute command `ipset flush otbr-ingress-allow-dst-swap` = 0 otbr-agent[1892]: 00:00:00.118 [I] Platform------: Execute command `ipset flush otbr-ingress-deny-src-swap` = 0 otbr-agent[1892]: 00:00:00.122 [I] Platform------: Execute command `ipset add otbr-ingress-deny-src-swap fdde:ad00:beef:0::/64 -exist` = 0 otbr-agent[1892]: 00:00:00.130 [I] Platform------: Execute command `ipset swap otbr-ingress-deny-src-swap otbr-ingress-deny-src` = 0 otbr-agent[1892]: 00:00:00.134 [I] Platform------: Execute command `ipset swap otbr-ingress-allow-dst-swap otbr-ingress-allow-dst` = 0 otbr-agent[1892]: 00:00:00.134 [I] P-Netif-------: NAT64 CIDR updated to 192.168.255.0/24. otbr-agent[1892]: 00:00:00.135 [I] P-Netif-------: Deleting route for NAT64 otbr-agent[1892]: 00:00:00.135 [I] P-McastRtMgr--: Disable: OK otbr-agent[1892]: [INFO]-BA------: Publish meshcop service OpenThread BorderRouter #102C._meshcop._udp.local. otbr-agent[1892]: 00:00:00.135 [I] RouterTable---: Route table otbr-agent[1892]: 00:00:00.135 [I] TrelInterface-: Registering DNS-SD service: port:60358, txt:"xa=f2385e307513102c, xp=dead00beef00cafe" otbr-agent[1892]: 00:00:00.142 [I] P-Netif-------: Host netif is down otbr-agent[1892]: 00:00:00.143 [I] P-Netif-------: Succeeded to process request#1 otbr-agent[1892]: 00:00:00.143 [W] P-Netif-------: Failed to process request#2: No such process otbr-agent[1892]: [INFO]-MDNS----: Successfully registered service OpenThread BorderRouter #102C._meshcop._udp otbr-agent[1892]: [INFO]-BA------: Result of publish meshcop service OpenThread BorderRouter #102C._meshcop._udp.local: OK otbr-agent[1892]: [INFO]-BA------: Result of publish meshcop service OpenThread BorderRouter #102C._meshcop._udp.local: OK
You should now be able to interact with the OT CLI:
sudo ot-ctl state enabled
Running the OTBR as a Service#
OTBR Service can be started as by calling:
sudo systemctl start otbr-agent
Running the Bluetooth Host Applications#
For both multiprotocol RCP and NCP architectures, CPCd must be started before running the Bluetooth host applications.
Bluetooth Host Applications for Multiprotocol RCP#
Follow the steps below after CPCd starts up successfully.
Run the CPC-HCI bridge application (bt_host_cpc_hci_bridge). It connects to CPCd using the standard instance name cpcd_0, opens a CPC endpoint to the BLE RCP running on the EFR, and creates a numbered virtual serial device on the host, for example
/dev/pts/2. The actual number may vary. For convenience,bt_host_cpc_hci_bridgealso creates a symlink to the device frompts_hciin the working directory.[I] Silicon Labs | CPC-HCI bridge [I] CPC successfully initialized with 'cpcd_0' [I] CPC Bluetooth endpoint opened [I] PTY device file opened at '/dev/pts/6'Use the following command to attach the Bluetooth stack to the newly created virtual serial device, where <device> is the name of the virtual serial device:
sudo btattach -B <device> -S 115200Run
sudo bluetoothctlto start the Bluetooth CLI utility and use commands to control the Bluetooth controller device.A utility that comes with the standard Bluetooth tools, called
btmon, can be used to view the HCI traffic between the Bluetooth host and the controller.To view the HCI traces for live debugging, run
sudo btmon &.To save the HCI traces and debug later using tools such as Wireshark, run
sudo btmon --write ~/hcitrace.snoop.
Bluetooth Host Application for Multiprotocol NCP#
Run the example Bluetooth host application bt_host_empty with the following command:
./bt_host_empty -C cpcd_0
The -C option is used to specify the CPC instance name (ex: -C cpcd_0).