You are viewing documentation for version:
This structure represents an IPv6 network interface unicast address.
Public Attributes#
The IPv6 unicast address.
uint8_t
The Prefix length (in bits).
bool
TRUE if the address is preferred, FALSE otherwise.
bool
TRUE if the address is valid, FALSE otherwise.
bool
TRUE if the mScopeOverride value is valid, FALSE otherwise.
unsigned int
The IPv6 scope of this address.
bool
TRUE if the address is an RLOC, FALSE otherwise.
A pointer to the next network interface address.
Public Attribute Documentation#
mAddress#
otIp6Address otNetifAddress::mAddress
The IPv6 unicast address.
mPrefixLength#
uint8_t otNetifAddress::mPrefixLength
The Prefix length (in bits).
mAddressOrigin#
uint8_t otNetifAddress::mAddressOrigin
The IPv6 address origin.
mPreferred#
bool otNetifAddress::mPreferred
TRUE if the address is preferred, FALSE otherwise.
mValid#
bool otNetifAddress::mValid
TRUE if the address is valid, FALSE otherwise.
mScopeOverrideValid#
bool otNetifAddress::mScopeOverrideValid
TRUE if the mScopeOverride value is valid, FALSE otherwise.
mScopeOverride#
unsigned int otNetifAddress::mScopeOverride
The IPv6 scope of this address.
mRloc#
bool otNetifAddress::mRloc
TRUE if the address is an RLOC, FALSE otherwise.
mNext#
struct otNetifAddress* otNetifAddress::mNext
A pointer to the next network interface address.