Border Agent#

This module includes functions for the Thread Border Agent role.

Modules#

otBorderAgentId

Enumerations#

enum
OT_BORDER_AGENT_STATE_STOPPED = 0
OT_BORDER_AGENT_STATE_STARTED = 1
OT_BORDER_AGENT_STATE_ACTIVE = 2
}

Defines the Border Agent state.

Typedefs#

typedef enum otBorderAgentState

Defines the Border Agent state.

Functions#

otBorderAgentGetState(otInstance *aInstance)

Gets the otBorderAgentState of the Thread Border Agent role.

uint16_t
otBorderAgentGetUdpPort(otInstance *aInstance)

Gets the UDP port of the Thread Border Agent service.

otBorderAgentGetId(otInstance *aInstance, otBorderAgentId *aId)

Gets the randomly generated Border Agent ID.

otBorderAgentSetId(otInstance *aInstance, const otBorderAgentId *aId)

Sets the Border Agent ID.

Macros#

#define

The length of Border Agent/Router ID in bytes.

Enumeration Documentation#

otBorderAgentState#

otBorderAgentState

Defines the Border Agent state.

Enumerator
OT_BORDER_AGENT_STATE_STOPPED

Border agent role is disabled.

OT_BORDER_AGENT_STATE_STARTED

Border agent is started.

OT_BORDER_AGENT_STATE_ACTIVE

Border agent is connected with external commissioner.


Typedef Documentation#

otBorderAgentState#

typedef enum otBorderAgentState otBorderAgentState

Defines the Border Agent state.


Variable Documentation#

OT_TOOL_PACKED_END#

OT_TOOL_PACKED_BEGIN struct otBorderAgentId OT_TOOL_PACKED_END

Function Documentation#

otBorderAgentGetState#

otBorderAgentState otBorderAgentGetState (otInstance * aInstance)

Gets the otBorderAgentState of the Thread Border Agent role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns


otBorderAgentGetUdpPort#

uint16_t otBorderAgentGetUdpPort (otInstance * aInstance)

Gets the UDP port of the Thread Border Agent service.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • UDP port of the Border Agent.


otBorderAgentGetId#

otError otBorderAgentGetId (otInstance * aInstance, otBorderAgentId * aId)

Gets the randomly generated Border Agent ID.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otBorderAgentId *[out]aId

A pointer to buffer to receive the ID.

The ID is saved in persistent storage and survives reboots. The typical use case of the ID is to be published in the MeshCoP mDNS service as the id TXT value for the client to identify this Border Router/Agent device.

See Also


otBorderAgentSetId#

otError otBorderAgentSetId (otInstance * aInstance, const otBorderAgentId * aId)

Sets the Border Agent ID.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otBorderAgentId *[out]aId

A pointer to the Border Agent ID.

The Border Agent ID will be saved in persistent storage and survive reboots. It's required to set the ID only once after factory reset. If the ID has never been set by calling this function, a random ID will be generated and returned when otBorderAgentGetId is called.

See Also


Macro Definition Documentation#

OT_BORDER_AGENT_ID_LENGTH#

#define OT_BORDER_AGENT_ID_LENGTH
Value:
(16)

The length of Border Agent/Router ID in bytes.