Represents the message buffer information for different queues used by OpenThread stack.

Public Attributes#

uint16_t

The total number of buffers in the messages pool (0xffff if unknown).

uint16_t

The number of free buffers (0xffff if unknown).

uint16_t

The maximum number of used buffers at the same time since OT stack initialization or last call to otMessageResetBufferInfo().

Info about 6LoWPAN send queue.

Info about 6LoWPAN reassembly queue.

Info about IPv6 send queue.

Info about MPL send queue.

Info about MLE delayed message queue.

Info about CoAP/TMF send queue.

Info about CoAP secure send queue.

Info about application CoAP send queue.

Public Attribute Documentation#

mTotalBuffers#

uint16_t otBufferInfo::mTotalBuffers

The total number of buffers in the messages pool (0xffff if unknown).


Definition at line 290 of file include/openthread/message.h

mFreeBuffers#

uint16_t otBufferInfo::mFreeBuffers

The number of free buffers (0xffff if unknown).


Definition at line 291 of file include/openthread/message.h

mMaxUsedBuffers#

uint16_t otBufferInfo::mMaxUsedBuffers

The maximum number of used buffers at the same time since OT stack initialization or last call to otMessageResetBufferInfo().


Definition at line 298 of file include/openthread/message.h

m6loSendQueue#

otMessageQueueInfo otBufferInfo::m6loSendQueue

Info about 6LoWPAN send queue.


Definition at line 300 of file include/openthread/message.h

m6loReassemblyQueue#

otMessageQueueInfo otBufferInfo::m6loReassemblyQueue

Info about 6LoWPAN reassembly queue.


Definition at line 301 of file include/openthread/message.h

mIp6Queue#

otMessageQueueInfo otBufferInfo::mIp6Queue

Info about IPv6 send queue.


Definition at line 302 of file include/openthread/message.h

mMplQueue#

otMessageQueueInfo otBufferInfo::mMplQueue

Info about MPL send queue.


Definition at line 303 of file include/openthread/message.h

mMleQueue#

otMessageQueueInfo otBufferInfo::mMleQueue

Info about MLE delayed message queue.


Definition at line 304 of file include/openthread/message.h

mCoapQueue#

otMessageQueueInfo otBufferInfo::mCoapQueue

Info about CoAP/TMF send queue.


Definition at line 305 of file include/openthread/message.h

mCoapSecureQueue#

otMessageQueueInfo otBufferInfo::mCoapSecureQueue

Info about CoAP secure send queue.


Definition at line 306 of file include/openthread/message.h

mApplicationCoapQueue#

otMessageQueueInfo otBufferInfo::mApplicationCoapQueue

Info about application CoAP send queue.


Definition at line 307 of file include/openthread/message.h