Represents a TCP listener.
A TCP listener is used to listen for and accept incoming TCP connections.
The application should not inspect the fields of this structure directly; it should only interact with it via the TCP API functions whose signatures are provided in this file.
Public Attributes#
uint8_t
void *
union otTcpListener::@27
struct otTcpListener *
A pointer to the next TCP listener (internal use only)
void *
A pointer to application-specific context.
"Accept ready" callback function
"Accept done" callback function
Public Attribute Documentation#
mSize#
uint8_t otTcpListener::mSize[OT_TCP_LISTENER_TCB_SIZE_BASE+OT_TCP_LISTENER_TCB_NUM_PTR *sizeof(void *)]
Definition at line
672
of file include/openthread/tcp.h
mTcbListen#
union otTcpListener::@27 otTcpListener::mTcbListen
Definition at line
674
of file include/openthread/tcp.h
mNext#
struct otTcpListener* otTcpListener::mNext
A pointer to the next TCP listener (internal use only)
Definition at line
676
of file include/openthread/tcp.h
mContext#
void* otTcpListener::mContext
A pointer to application-specific context.
Definition at line
677
of file include/openthread/tcp.h
mAcceptReadyCallback#
otTcpAcceptReady otTcpListener::mAcceptReadyCallback
"Accept ready" callback function
Definition at line
679
of file include/openthread/tcp.h
mAcceptDoneCallback#
otTcpAcceptDone otTcpListener::mAcceptDoneCallback
"Accept done" callback function
Definition at line
680
of file include/openthread/tcp.h