SPI Slave#

This module includes the platform abstraction for SPI slave communication.

Typedefs#

typedef bool(*
otPlatSpiSlaveTransactionCompleteCallback)(void *aContext, uint8_t *aOutputBuf, uint16_t aOutputBufLen, uint8_t *aInputBuf, uint16_t aInputBufLen, uint16_t aTransactionLength)

Indicates that a SPI transaction has completed with the given length.

typedef void(*

Invoked after a transaction complete callback is called and returns TRUE to do any further processing required.

Functions#

otPlatSpiSlaveEnable(otPlatSpiSlaveTransactionCompleteCallback aCompleteCallback, otPlatSpiSlaveTransactionProcessCallback aProcessCallback,