Represents a ping request configuration.

Public Attributes#

Source address of the ping.

Destination address to ping.

Callback function to report replies (can be NULL if not needed).

Callback function to report statistics (can be NULL if not needed).

void *

A pointer to the callback application-specific context.

uint16_t

Data size (# of bytes) excludes IPv6/ICMPv6 header. Zero for default.

uint16_t

Number of ping messages to send. Zero to use default.

uint32_t

Ping tx interval in milliseconds. Zero to use default.

uint16_t

Time in milliseconds to wait for final reply after sending final request.

uint8_t

Hop limit (used if mAllowZeroHopLimit is false). Zero for default.

bool

Indicates whether hop limit is zero.

bool

Allow looping back pings to multicast address that device is subscribed to.

Public Attribute Documentation#

mSource#

otIp6Address otPingSenderConfig::mSource

Source address of the ping.


mDestination#

otIp6Address otPingSenderConfig::mDestination

Destination address to ping.


mReplyCallback#

otPingSenderReplyCallback otPingSenderConfig::mReplyCallback

Callback function to report replies (can be NULL if not needed).


mStatisticsCallback#

otPingSenderStatisticsCallback otPingSenderConfig::mStatisticsCallback

Callback function to report statistics (can be NULL if not needed).


mCallbackContext#

void* otPingSenderConfig::mCallbackContext

A pointer to the callback application-specific context.


mSize#

uint16_t otPingSenderConfig::mSize

Data size (# of bytes) excludes IPv6/ICMPv6 header. Zero for default.


mCount#

uint16_t otPingSenderConfig::mCount

Number of ping messages to send. Zero to use default.


mInterval#

uint32_t otPingSenderConfig::mInterval

Ping tx interval in milliseconds. Zero to use default.


mTimeout#

uint16_t otPingSenderConfig::mTimeout

Time in milliseconds to wait for final reply after sending final request.

Zero to use default.


mHopLimit#

uint8_t otPingSenderConfig::mHopLimit

Hop limit (used if mAllowZeroHopLimit is false). Zero for default.


mAllowZeroHopLimit#

bool otPingSenderConfig::mAllowZeroHopLimit

Indicates whether hop limit is zero.


mMulticastLoop#

bool otPingSenderConfig::mMulticastLoop

Allow looping back pings to multicast address that device is subscribed to.