RNG Cryptographic#

This module includes functions that generates cryptographic random numbers.

Functions#

otRandomCryptoFillBuffer(uint8_t *aBuffer, uint16_t aSize)

Fills a given buffer with cryptographically secure random bytes.

Function Documentation#

otRandomCryptoFillBuffer#

otError otRandomCryptoFillBuffer (uint8_t * aBuffer, uint16_t aSize)

Fills a given buffer with cryptographically secure random bytes.

Parameters
[out]aBuffer

A pointer to a buffer to fill with the random bytes.

[in]aSize

Size of buffer (number of bytes to fill).


Definition at line 63 of file include/openthread/random_crypto.h