Represents a Network Diagnostic Mac Counters value.

See RFC 2863 for definitions of member fields.

Public Attribute Documentation#

mIfInUnknownProtos#

uint32_t otNetworkDiagMacCounters::mIfInUnknownProtos

Definition at line 200 of file include/openthread/netdiag.h

mIfInErrors#

uint32_t otNetworkDiagMacCounters::mIfInErrors

Definition at line 201 of file include/openthread/netdiag.h

mIfOutErrors#

uint32_t otNetworkDiagMacCounters::mIfOutErrors

Definition at line 202 of file include/openthread/netdiag.h

mIfInUcastPkts#

uint32_t otNetworkDiagMacCounters::mIfInUcastPkts

Definition at line 203 of file include/openthread/netdiag.h

mIfInBroadcastPkts#

uint32_t otNetworkDiagMacCounters::mIfInBroadcastPkts

Definition at line 204 of file include/openthread/netdiag.h

mIfInDiscards#

uint32_t otNetworkDiagMacCounters::mIfInDiscards

Definition at line 205 of file include/openthread/netdiag.h

mIfOutUcastPkts#

uint32_t otNetworkDiagMacCounters::mIfOutUcastPkts

Definition at line 206 of file include/openthread/netdiag.h

mIfOutBroadcastPkts#

uint32_t otNetworkDiagMacCounters::mIfOutBroadcastPkts

Definition at line 207 of file include/openthread/netdiag.h

mIfOutDiscards#

uint32_t otNetworkDiagMacCounters::mIfOutDiscards

Definition at line 208 of file include/openthread/netdiag.h