Command Line Interface#

This module includes functions that control the Thread stack's execution.

Modules#

otCliCommand

Typedefs#

typedef int(*
otCliOutputCallback)(void *aContext, const char *aFormat, va_list aArguments)

Pointer is called to notify about Console output.

Functions#

void
otCliInit(otInstance *aInstance, otCliOutputCallback aCallback, void *aContext)

Initialize the CLI module.

void
otCliInputLine(char *aBuf)

Is called to feed in a console input line.

otCliSetUserCommands(const otCliCommand *aUserCommands, uint8_t aLength, void *aContext)

Set a user command table.

void
otCliOutputBytes(const uint8_t *aBytes, uint8_t aLength)

Write a number of bytes to the CLI console as a hex string.

void
otCliOutputFormat(const char *aFmt,...)

Write formatted string to the CLI console.

void
otCliAppendResult(otError aError)

Write error code to the CLI console.

void
otCliPlatLogv(otLogLevel aLogLevel, otLogRegion aLogRegion, const char *aFormat, va_list aArgs)

Callback to write the OpenThread Log to the CLI console.

void

Callback to allow vendor specific commands to be added to the user command table.

Typedef Documentation#

otCliOutputCallback#

typedef int(* otCliOutputCallback) (void *aContext, const char *aFormat, va_list aArguments) )(void *aContext, const char *aFormat, va_list aArguments)

Pointer is called to notify about Console output.

Parameters
TypeDirectionArgument NameDescription
[out]aContext

A user context pointer.

[in]aFormat

The format string.

[in]aArguments

The format string arguments.

Returns

  • Number of bytes written by the callback.


otCliCommand#

typedef struct otCliCommand otCliCommand

Function Documentation#

otCliInit#

void otCliInit (otInstance * aInstance, otCliOutputCallback aCallback, void * aContext)

Initialize the CLI module.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance structure.

otCliOutputCallback[in]aCallback

A callback method called to process CLI output.

void *[in]aContext

A user context pointer.


otCliInputLine#

void otCliInputLine (char * aBuf)

Is called to feed in a console input line.

Parameters
TypeDirectionArgument NameDescription
char *[in]aBuf

A pointer to a null-terminated string.


otCliSetUserCommands#

otError otCliSetUserCommands (const otCliCommand * aUserCommands, uint8_t aLength, void * aContext)

Set a user command table.

Parameters
TypeDirectionArgument NameDescription
const otCliCommand *[in]aUserCommands

A pointer to an array with user commands.

uint8_t[in]aLength

aUserCommands length.

void *[in]aContext

The context passed to the handler.


otCliOutputBytes#

void otCliOutputBytes (const uint8_t * aBytes, uint8_t aLength)

Write a number of bytes to the CLI console as a hex string.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]aBytes

A pointer to data which should be printed.

uint8_t[in]aLength

aBytes length.


otCliOutputFormat#

void otCliOutputFormat (const char * aFmt, ... )

Write formatted string to the CLI console.

Parameters
TypeDirectionArgument NameDescription
const char *[in]aFmt

A pointer to the format string.

...[in]

A matching list of arguments.


otCliAppendResult#

void otCliAppendResult (otError aError)

Write error code to the CLI console.

Parameters
TypeDirectionArgument NameDescription
otError[in]aError

Error code value.

If the aError is OT_ERROR_PENDING nothing will be outputted.


otCliPlatLogv#

void otCliPlatLogv (otLogLevel aLogLevel, otLogRegion aLogRegion, const char * aFormat, va_list aArgs)

Callback to write the OpenThread Log to the CLI console.

Parameters
TypeDirectionArgument NameDescription
otLogLevel[in]aLogLevel

The log level.

otLogRegion[in]aLogRegion

The log region.

const char *[in]aFormat

A pointer to the format string.

va_list[in]aArgs

va_list matching aFormat.


otCliVendorSetUserCommands#

void otCliVendorSetUserCommands (void )

Callback to allow vendor specific commands to be added to the user command table.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Available when OPENTHREAD_CONFIG_CLI_VENDOR_COMMANDS_ENABLE is enabled and OPENTHREAD_CONFIG_CLI_MAX_USER_CMD_ENTRIES is greater than 1.