You are viewing documentation for version:
Represents the IP level counters.
Public Attributes#
uint32_t
The number of IPv6 packets successfully transmitted.
uint32_t
The number of IPv6 packets successfully received.
uint32_t
The number of IPv6 packets failed to transmit.
uint32_t
The number of IPv6 packets failed to receive.
Public Attribute Documentation#
mTxSuccess#
uint32_t otIpCounters::mTxSuccess
The number of IPv6 packets successfully transmitted.
mRxSuccess#
uint32_t otIpCounters::mRxSuccess
The number of IPv6 packets successfully received.
mTxFailure#
uint32_t otIpCounters::mTxFailure
The number of IPv6 packets failed to transmit.
mRxFailure#
uint32_t otIpCounters::mRxFailure
The number of IPv6 packets failed to receive.