Represents information about a message queue.

Public Attributes#

uint16_t

Number of messages in the queue.

uint16_t

Number of data buffers used by messages in the queue.

uint32_t

Total number of bytes used by all messages in the queue.

Public Attribute Documentation#

mNumMessages#

uint16_t otMessageQueueInfo::mNumMessages

Number of messages in the queue.


Definition at line 329 of file include/openthread/message.h

mNumBuffers#

uint16_t otMessageQueueInfo::mNumBuffers

Number of data buffers used by messages in the queue.


Definition at line 330 of file include/openthread/message.h

mTotalBytes#

uint32_t otMessageQueueInfo::mTotalBytes

Total number of bytes used by all messages in the queue.


Definition at line 331 of file include/openthread/message.h