Represents an MLE Link Mode configuration.

Public Attributes#

bool

1, if the sender has its receiver on when not transmitting. 0, otherwise.

bool

1, if the sender is an FTD. 0, otherwise.

bool

1, if the sender requires the full Network Data. 0, otherwise.

Public Attribute Documentation#

mRxOnWhenIdle#

bool otLinkModeConfig::mRxOnWhenIdle

1, if the sender has its receiver on when not transmitting. 0, otherwise.


Definition at line 86 of file include/openthread/thread.h

mDeviceType#

bool otLinkModeConfig::mDeviceType

1, if the sender is an FTD. 0, otherwise.


Definition at line 87 of file include/openthread/thread.h

mNetworkData#

bool otLinkModeConfig::mNetworkData

1, if the sender requires the full Network Data. 0, otherwise.


Definition at line 88 of file include/openthread/thread.h