Represents a Network Diagnostic Route64 TLV value.
Public Attributes#
uint8_t
The sequence number associated with the set of Router ID assignments in mRouteData.
uint8_t
Number of routes.
Link Quality and Routing Cost data.
Public Attribute Documentation#
mIdSequence#
uint8_t otNetworkDiagRoute::mIdSequence
The sequence number associated with the set of Router ID assignments in mRouteData.
Sequence number for Router ID assignments.
Definition at line
126
of file include/openthread/netdiag.h
mRouteCount#
uint8_t otNetworkDiagRoute::mRouteCount
Number of routes.
Definition at line
127
of file include/openthread/netdiag.h
mRouteData#
otNetworkDiagRouteData otNetworkDiagRoute::mRouteData[OT_NETWORK_MAX_ROUTER_ID+1]
Link Quality and Routing Cost data.
Definition at line
128
of file include/openthread/netdiag.h