Represents a Network Diagnostic Connectivity value.

Public Attributes#

int8_t

The priority of the sender as a parent.

uint8_t

Number of neighbors with link of quality 3.

uint8_t

Number of neighbors with link of quality 2.

uint8_t

Number of neighbors with link of quality 1.

uint8_t

Cost to the Leader.

uint8_t

Most recent received ID seq number.

uint8_t

Number of active routers.

uint16_t

Buffer capacity in bytes for SEDs. Optional.

uint8_t

Queue capacity (number of IPv6 datagrams) per SED. Optional.

Public Attribute Documentation#

mParentPriority#

int8_t otNetworkDiagConnectivity::mParentPriority

The priority of the sender as a parent.


mLinkQuality3#

uint8_t otNetworkDiagConnectivity::mLinkQuality3

Number of neighbors with link of quality 3.


mLinkQuality2#

uint8_t otNetworkDiagConnectivity::mLinkQuality2

Number of neighbors with link of quality 2.


mLinkQuality1#

uint8_t otNetworkDiagConnectivity::mLinkQuality1

Number of neighbors with link of quality 1.


mLeaderCost#

uint8_t otNetworkDiagConnectivity::mLeaderCost

Cost to the Leader.


mIdSequence#

uint8_t otNetworkDiagConnectivity::mIdSequence

Most recent received ID seq number.


mActiveRouters#

uint8_t otNetworkDiagConnectivity::mActiveRouters

Number of active routers.


mSedBufferSize#

uint16_t otNetworkDiagConnectivity::mSedBufferSize

Buffer capacity in bytes for SEDs. Optional.


mSedDatagramCount#

uint8_t otNetworkDiagConnectivity::mSedDatagramCount

Queue capacity (number of IPv6 datagrams) per SED. Optional.