Radio Configuration#
This module includes the platform abstraction for radio configuration.
Functions#
Get the radio capabilities.
Get the radio version string.
Get the radio receive sensitivity value.
Gets the factory-assigned IEEE EUI-64 for this interface.
Set the PAN ID for address filtering.
Set the Extended Address for address filtering.
Set the Short Address for address filtering.
Set the alternate short address.
Get the radio's transmit power in dBm.
Set the radio's transmit power in dBm for all channels.
Get the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.
Set the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.
Gets the external FEM's Rx LNA gain in dBm.
Sets the external FEM's Rx LNA gain in dBm.
Get the status of promiscuous mode.
Enable or disable promiscuous mode.
Sets the rx-on-when-idle state to the radio platform.
Update MAC keys and key index.
Sets the current MAC frame counter value.
Sets the current MAC frame counter value only if the new given value is larger than the current value.
Get the current time in microseconds referenced to a continuous monotonic local radio clock (64 bits width).
Get the bus speed in bits/second between the host and the radio chip.
Get the bus latency in microseconds between the host and the radio chip.
Function Documentation#
otPlatRadioGetCaps#
otRadioCaps otPlatRadioGetCaps (otInstance * aInstance)
Get the radio capabilities.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
Returns
The radio capability bit vector (see
OT_RADIO_CAP_*
definitions).
otPlatRadioGetVersionString#
const char * otPlatRadioGetVersionString (otInstance * aInstance)
Get the radio version string.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
This is an optional radio driver platform function. If not provided by platform radio driver, OpenThread uses the OpenThread version instead (See Also
Returns
A pointer to the OpenThread radio version.
otPlatRadioGetReceiveSensitivity#
int8_t otPlatRadioGetReceiveSensitivity (otInstance * aInstance)
Get the radio receive sensitivity value.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
Returns
The radio receive sensitivity value in dBm.
otPlatRadioGetIeeeEui64#
void otPlatRadioGetIeeeEui64 (otInstance * aInstance, uint8_t * aIeeeEui64)
Gets the factory-assigned IEEE EUI-64 for this interface.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
uint8_t * | [out] | aIeeeEui64 | A pointer to the factory-assigned IEEE EUI-64. |
otPlatRadioSetPanId#
void otPlatRadioSetPanId (otInstance * aInstance, otPanId aPanId)
Set the PAN ID for address filtering.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
otPanId | [in] | aPanId | The IEEE 802.15.4 PAN ID. |
otPlatRadioSetExtendedAddress#
void otPlatRadioSetExtendedAddress (otInstance * aInstance, const otExtAddress * aExtAddress)
Set the Extended Address for address filtering.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
const otExtAddress * | [in] | aExtAddress | A pointer to the IEEE 802.15.4 Extended Address stored in little-endian byte order. |
otPlatRadioSetShortAddress#
void otPlatRadioSetShortAddress (otInstance * aInstance, otShortAddress aShortAddress)
Set the Short Address for address filtering.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
otShortAddress | [in] | aShortAddress | The IEEE 802.15.4 Short Address. |
otPlatRadioSetAlternateShortAddress#
void otPlatRadioSetAlternateShortAddress (otInstance * aInstance, otShortAddress aShortAddress)
Set the alternate short address.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
otShortAddress | [in] | aShortAddress | The alternate IEEE 802.15.4 short address. |
This is an optional radio platform API. The radio platform MUST indicate support for this API by including the capability OT_RADIO_CAPS_ALT_SHORT_ADDR
in otPlatRadioGetCaps()
.
When supported, the radio should accept received frames destined to the specified alternate short address in addition to the short address provided in otPlatRadioSetShortAddress()
.
The aShortAddress
can be set to OT_RADIO_INVALID_SHORT_ADDR
(0xfffe) to clear any previously set alternate short address.
This function is used by OpenThread stack during child-to-router role transitions, allowing the device to continue receiving frames addressed to its previous short address for a short period.
otPlatRadioGetTransmitPower#
otError otPlatRadioGetTransmitPower (otInstance * aInstance, int8_t * aPower)
Get the radio's transmit power in dBm.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
int8_t * | [out] | aPower | The transmit power in dBm. |
Note
The transmit power returned will be no larger than the power specified in the max power table for the current channel.
otPlatRadioSetTransmitPower#
otError otPlatRadioSetTransmitPower (otInstance * aInstance, int8_t aPower)
Set the radio's transmit power in dBm for all channels.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
int8_t | [in] | aPower | The transmit power in dBm. |
Note
The real transmit power will be no larger than the power specified in the max power table for the current channel that was configured by
otPlatRadioSetChannelMaxTransmitPower()
.
otPlatRadioGetCcaEnergyDetectThreshold#
otError otPlatRadioGetCcaEnergyDetectThreshold (otInstance * aInstance, int8_t * aThreshold)
Get the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
int8_t * | [out] | aThreshold | The CCA ED threshold in dBm. |
otPlatRadioSetCcaEnergyDetectThreshold#
otError otPlatRadioSetCcaEnergyDetectThreshold (otInstance * aInstance, int8_t aThreshold)
Set the radio's CCA ED threshold in dBm measured at antenna connector per IEEE 802.15.4 - 2015 section 10.1.4.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
int8_t | [in] | aThreshold | The CCA ED threshold in dBm. |
otPlatRadioGetFemLnaGain#
otError otPlatRadioGetFemLnaGain (otInstance * aInstance, int8_t * aGain)
Gets the external FEM's Rx LNA gain in dBm.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
int8_t * | [out] | aGain | The external FEM's Rx LNA gain in dBm. |
otPlatRadioSetFemLnaGain#
otError otPlatRadioSetFemLnaGain (otInstance * aInstance, int8_t aGain)
Sets the external FEM's Rx LNA gain in dBm.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
int8_t | [in] | aGain | The external FEM's Rx LNA gain in dBm. |
otPlatRadioGetPromiscuous#
bool otPlatRadioGetPromiscuous (otInstance * aInstance)
Get the status of promiscuous mode.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
otPlatRadioSetPromiscuous#
void otPlatRadioSetPromiscuous (otInstance * aInstance, bool aEnable)
Enable or disable promiscuous mode.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
bool | [in] | aEnable | TRUE to enable or FALSE to disable promiscuous mode. |
otPlatRadioSetRxOnWhenIdle#
void otPlatRadioSetRxOnWhenIdle (otInstance * aInstance, bool aEnable)
Sets the rx-on-when-idle state to the radio platform.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance structure. |
bool | [in] | aEnable | TRUE to keep radio in Receive state, FALSE to put to Sleep state during idle periods. |
There are a few situations that the radio can enter sleep state if the device is in rx-off-when-idle state but it's hard and costly for the SubMac to identify these situations and instruct the radio to enter sleep:
Finalization of a regular frame reception task, provided that:
The frame is received without errors and passes the filtering and it's not an spurious ACK.
ACK is not requested or transmission of ACK is not possible due to internal conditions.
Finalization of a frame transmission or transmission of an ACK frame, when ACK is not requested in the transmitted frame.
Finalization of the reception operation of a requested ACK due to:
ACK timeout expiration.
Reception of an invalid ACK or not an ACK frame.
Reception of the proper ACK, unless the transmitted frame was a Data Request Command and the frame pending bit on the received ACK is set to true. In this case the radio platform implementation SHOULD keep the receiver on until a determined timeout which triggers an idle period start.
OPENTHREAD_CONFIG_MAC_DATA_POLL_TIMEOUT
can be taken as a reference for this.
Finalization of a stand alone CCA task.
Finalization of a CCA operation with busy result during CSMA/CA procedure.
Finalization of an Energy Detection task.
Finalization of a radio reception window scheduled with
otPlatRadioReceiveAt
.
If a platform supports OT_RADIO_CAPS_RX_ON_WHEN_IDLE
it must also support OT_RADIO_CAPS_CSMA_BACKOFF
and handle idle periods after CCA as described above.
Upon the transition of the "RxOnWhenIdle" flag from TRUE to FALSE, the radio platform should enter sleep mode. If the radio is currently in receive mode, it should enter sleep mode immediately. Otherwise, it should enter sleep mode after the current operation is completed.
otPlatRadioSetMacKey#
void otPlatRadioSetMacKey (otInstance * aInstance, uint8_t aKeyIdMode, uint8_t aKeyId, const otMacKeyMaterial * aPrevKey, const otMacKeyMaterial * aCurrKey, const otMacKeyMaterial * aNextKey, otRadioKeyType aKeyType)
Update MAC keys and key index.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
uint8_t | [in] | aKeyIdMode | The key ID mode. |
uint8_t | [in] | aKeyId | Current MAC key index. |
const otMacKeyMaterial * | [in] | aPrevKey | A pointer to the previous MAC key. |
const otMacKeyMaterial * | [in] | aCurrKey | A pointer to the current MAC key. |
const otMacKeyMaterial * | [in] | aNextKey | A pointer to the next MAC key. |
otRadioKeyType | [in] | aKeyType | Key Type used. |
Is used when radio provides OT_RADIO_CAPS_TRANSMIT_SEC capability.
The radio platform should reset the current security MAC frame counter tracked by the radio on this call. While this is highly recommended, the OpenThread stack, as a safeguard, will also reset the frame counter using the otPlatRadioSetMacFrameCounter()
before calling this API.
otPlatRadioSetMacFrameCounter#
void otPlatRadioSetMacFrameCounter (otInstance * aInstance, uint32_t aMacFrameCounter)
Sets the current MAC frame counter value.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
uint32_t | [in] | aMacFrameCounter | The MAC frame counter value. |
Is used when radio provides OT_RADIO_CAPS_TRANSMIT_SEC
capability.
otPlatRadioSetMacFrameCounterIfLarger#
void otPlatRadioSetMacFrameCounterIfLarger (otInstance * aInstance, uint32_t aMacFrameCounter)
Sets the current MAC frame counter value only if the new given value is larger than the current value.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
uint32_t | [in] | aMacFrameCounter | The MAC frame counter value. |
Is used when radio provides OT_RADIO_CAPS_TRANSMIT_SEC
capability.
otPlatRadioGetNow#
uint64_t otPlatRadioGetNow (otInstance * aInstance)
Get the current time in microseconds referenced to a continuous monotonic local radio clock (64 bits width).
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
The radio clock SHALL NOT wrap during the device's uptime. Implementations SHALL therefore identify and compensate for internal counter overflows. The clock does not have a defined epoch and it SHALL NOT introduce any continuous or discontinuous adjustments (e.g. leap seconds). Implementations SHALL compensate for any sleep times of the device.
Implementations MAY choose to discipline the radio clock and compensate for sleep times by any means (e.g. by combining a high precision/low power RTC with a high resolution counter) as long as the exposed combined clock provides continuous monotonic microsecond resolution ticks within the accuracy limits announced by otPlatRadioGetCslAccuracy.
Returns
The current time in microseconds. UINT64_MAX when platform does not support or radio time is not ready.
otPlatRadioGetBusSpeed#
uint32_t otPlatRadioGetBusSpeed (otInstance * aInstance)
Get the bus speed in bits/second between the host and the radio chip.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
The bus speed in bits/second between the host and the radio chip. Return 0 when the MAC and above layer and Radio layer resides on the same chip.
otPlatRadioGetBusLatency#
uint32_t otPlatRadioGetBusLatency (otInstance * aInstance)
Get the bus latency in microseconds between the host and the radio chip.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
The bus latency in microseconds between the host and the radio chip. Return 0 when the MAC and above layer and Radio layer resides on the same chip.