Represents the result (value) for a Link Metrics query.
Public Attributes#
Specifies which metrics values are present/included.
uint32_t
The value of Pdu Count.
uint8_t
The value LQI.
uint8_t
The value of Link Margin.
int8_t
The value of Rssi.
Public Attribute Documentation#
mMetrics#
otLinkMetrics otLinkMetricsValues::mMetrics
Specifies which metrics values are present/included.
Definition at line
62
of file include/openthread/link_metrics.h
mPduCountValue#
uint32_t otLinkMetricsValues::mPduCountValue
The value of Pdu Count.
Definition at line
64
of file include/openthread/link_metrics.h
mLqiValue#
uint8_t otLinkMetricsValues::mLqiValue
The value LQI.
Definition at line
65
of file include/openthread/link_metrics.h
mLinkMarginValue#
uint8_t otLinkMetricsValues::mLinkMarginValue
The value of Link Margin.
Definition at line
66
of file include/openthread/link_metrics.h
mRssiValue#
int8_t otLinkMetricsValues::mRssiValue
The value of Rssi.
Definition at line
67
of file include/openthread/link_metrics.h