Logging - Platform#
This module includes the platform abstraction for the debug log service.
Enumerations#
Represents log regions.
Functions#
Outputs logs.
Handles OpenThread log level changes.
Macros#
Log level None.
Log level Critical.
Log level Warning.
Log level Notice.
Log level Informational.
Log level Debug.
Enumeration Documentation#
otLogRegion#
otLogRegion
Represents log regions.
The support for log region is removed and instead each core module can define its own name to appended to the logs. However, the otLogRegion enumeration is still defined as before to help with platforms which we may be using it in their otPlatLog() implementation. The OT core will always emit all logs with OT_LOG_REGION_CORE. 
| Enumerator | |
|---|---|
| OT_LOG_REGION_API | OpenThread API.  | 
| OT_LOG_REGION_MLE | MLE.  | 
| OT_LOG_REGION_ARP | EID-to-RLOC mapping.  | 
| OT_LOG_REGION_NET_DATA | Network Data.  | 
| OT_LOG_REGION_ICMP | ICMPv6.  | 
| OT_LOG_REGION_IP6 | IPv6.  | 
| OT_LOG_REGION_TCP | TCP.  | 
| OT_LOG_REGION_MAC | IEEE 802.15.4 MAC.  | 
| OT_LOG_REGION_MEM | Memory.  | 
| OT_LOG_REGION_NCP | NCP.  | 
| OT_LOG_REGION_MESH_COP | Mesh Commissioning Protocol.  | 
| OT_LOG_REGION_NET_DIAG | Network Diagnostic.  | 
| OT_LOG_REGION_PLATFORM | Platform.  | 
| OT_LOG_REGION_COAP | CoAP.  | 
| OT_LOG_REGION_CLI | CLI.  | 
| OT_LOG_REGION_CORE | OpenThread Core.  | 
| OT_LOG_REGION_UTIL | Utility module.  | 
| OT_LOG_REGION_BBR | Backbone Router (available since Thread 1.2)  | 
| OT_LOG_REGION_MLR | Multicast Listener Registration (available since Thread 1.2)  | 
| OT_LOG_REGION_DUA | Domain Unicast Address (available since Thread 1.2)  | 
| OT_LOG_REGION_BR | Border Router.  | 
| OT_LOG_REGION_SRP | Service Registration Protocol (SRP)  | 
| OT_LOG_REGION_DNS | DNS.  | 
Typedef Documentation#
otLogRegion#
typedef enum otLogRegion otLogRegion
Represents log regions.
The support for log region is removed and instead each core module can define its own name to appended to the logs. However, the otLogRegion enumeration is still defined as before to help with platforms which we may be using it in their otPlatLog() implementation. The OT core will always emit all logs with OT_LOG_REGION_CORE. 
Function Documentation#
otPlatLog#
void otPlatLog (otLogLevel aLogLevel, otLogRegion aLogRegion, const char * aFormat, ... )
Outputs logs.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otLogLevel | [in] | aLogLevel | The log level.  | 
| otLogRegion | [in] | aLogRegion | The log region.  | 
| const char * | [in] | aFormat | A pointer to the format string.  | 
| ... | [in] | Arguments for the format specification.  | 
Note that the support for log region is removed. The OT core will always emit all logs with OT_LOG_REGION_CORE as aLogRegion.
otPlatLogHandleLevelChanged#
void otPlatLogHandleLevelChanged (otLogLevel aLogLevel)
Handles OpenThread log level changes.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otLogLevel | [in] | aLogLevel | The new OpenThread log level.  | 
This platform function is called whenever the OpenThread log level changes. This platform function is optional since an empty weak implementation has been provided.
Note
Only applicable when
OPENTHREAD_CONFIG_LOG_LEVEL_DYNAMIC_ENABLE=1.