Defines Border Agent counters.
The mEpskc related counters require OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.
Public Attributes#
The number of ePSKc activations.
The number of ePSKc deactivations via API.
The number of ePSKc deactivations due to timeout.
The number of ePSKc deactivations due to reached max attempts.
The number of ePSKc deactivations due to commissioner disconnected.
The number of invalid border agent state errors at ePSKc activation.
The number of invalid args errors at ePSKc activation.
The number of start secure session errors at ePSKc activation.
The number of established secure sessions with ePSKc.
The number of failed secure sessions with ePSKc.
The number of successful commissioner petitions with ePSKc.
The number of established secure sessions with PSKc.
The number of failed secure sessions with PSKc.
The number of successful commissioner petitions with PSKc.
The number of MGMT_ACTIVE_GET.req sent over secure sessions.
The number of MGMT_PENDING_GET.req sent over secure sessions.
Public Attribute Documentation#
mEpskcDeactivationClears#
uint32_t otBorderAgentCounters::mEpskcDeactivationClears
The number of ePSKc deactivations via API.
mEpskcDeactivationTimeouts#
uint32_t otBorderAgentCounters::mEpskcDeactivationTimeouts
The number of ePSKc deactivations due to timeout.
mEpskcDeactivationMaxAttempts#
uint32_t otBorderAgentCounters::mEpskcDeactivationMaxAttempts
The number of ePSKc deactivations due to reached max attempts.
mEpskcDeactivationDisconnects#
uint32_t otBorderAgentCounters::mEpskcDeactivationDisconnects
The number of ePSKc deactivations due to commissioner disconnected.
mEpskcInvalidBaStateErrors#
uint32_t otBorderAgentCounters::mEpskcInvalidBaStateErrors
The number of invalid border agent state errors at ePSKc activation.
mEpskcInvalidArgsErrors#
uint32_t otBorderAgentCounters::mEpskcInvalidArgsErrors
The number of invalid args errors at ePSKc activation.
mEpskcStartSecureSessionErrors#
uint32_t otBorderAgentCounters::mEpskcStartSecureSessionErrors
The number of start secure session errors at ePSKc activation.
mEpskcSecureSessionSuccesses#
uint32_t otBorderAgentCounters::mEpskcSecureSessionSuccesses
The number of established secure sessions with ePSKc.
mEpskcSecureSessionFailures#
uint32_t otBorderAgentCounters::mEpskcSecureSessionFailures
The number of failed secure sessions with ePSKc.
mEpskcCommissionerPetitions#
uint32_t otBorderAgentCounters::mEpskcCommissionerPetitions
The number of successful commissioner petitions with ePSKc.
mPskcSecureSessionSuccesses#
uint32_t otBorderAgentCounters::mPskcSecureSessionSuccesses
The number of established secure sessions with PSKc.
mPskcSecureSessionFailures#
uint32_t otBorderAgentCounters::mPskcSecureSessionFailures
The number of failed secure sessions with PSKc.
mPskcCommissionerPetitions#
uint32_t otBorderAgentCounters::mPskcCommissionerPetitions
The number of successful commissioner petitions with PSKc.
mMgmtActiveGets#
uint32_t otBorderAgentCounters::mMgmtActiveGets
The number of MGMT_ACTIVE_GET.req sent over secure sessions.
mMgmtPendingGets#
uint32_t otBorderAgentCounters::mMgmtPendingGets
The number of MGMT_PENDING_GET.req sent over secure sessions.