Represents an entry from the discovered prefix table.
The entries in the discovered table track the Prefix/Route Info Options in the received Router Advertisement messages from other routers on the infrastructure link.
Public Attributes#
Information about the router advertising this prefix.
The discovered IPv6 prefix.
Indicates whether the prefix is on-link or route prefix.
Milliseconds since last update of this prefix.
Valid lifetime of the prefix (in seconds).
Route preference when mIsOnlink is false.
Preferred lifetime of the on-link prefix when mIsOnLink.
Public Attribute Documentation#
mRouter#
otBorderRoutingRouterEntry otBorderRoutingPrefixTableEntry::mRouter
Information about the router advertising this prefix.
mIsOnLink#
bool otBorderRoutingPrefixTableEntry::mIsOnLink
Indicates whether the prefix is on-link or route prefix.
mMsecSinceLastUpdate#
uint32_t otBorderRoutingPrefixTableEntry::mMsecSinceLastUpdate
Milliseconds since last update of this prefix.
mValidLifetime#
uint32_t otBorderRoutingPrefixTableEntry::mValidLifetime
Valid lifetime of the prefix (in seconds).
mRoutePreference#
otRoutePreference otBorderRoutingPrefixTableEntry::mRoutePreference
Route preference when mIsOnlink is false.
mPreferredLifetime#
uint32_t otBorderRoutingPrefixTableEntry::mPreferredLifetime
Preferred lifetime of the on-link prefix when mIsOnLink.